<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Internal ISP using in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Internal-ISP-using/m-p/1599782#M201570</link>
    <description>&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;Im designing a board with IMX8MP and want to use the CSI-2 inputs of the processor for camera inputs.&lt;/P&gt;&lt;P&gt;is there a list of supported vendors for the ISP ? i will use Hynix sensor (i know that only NXP &amp;amp; partners can access to the ISP)&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
    <pubDate>Wed, 15 Feb 2023 18:35:33 GMT</pubDate>
    <dc:creator>YoavBenita</dc:creator>
    <dc:date>2023-02-15T18:35:33Z</dc:date>
    <item>
      <title>Internal ISP using</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Internal-ISP-using/m-p/1599782#M201570</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;Im designing a board with IMX8MP and want to use the CSI-2 inputs of the processor for camera inputs.&lt;/P&gt;&lt;P&gt;is there a list of supported vendors for the ISP ? i will use Hynix sensor (i know that only NXP &amp;amp; partners can access to the ISP)&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
      <pubDate>Wed, 15 Feb 2023 18:35:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Internal-ISP-using/m-p/1599782#M201570</guid>
      <dc:creator>YoavBenita</dc:creator>
      <dc:date>2023-02-15T18:35:33Z</dc:date>
    </item>
  </channel>
</rss>