<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Not possible to compile the generated code on CM4 using Azure RTOS and uart driver in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Not-possible-to-compile-the-generated-code-on-CM4-using-Azure/m-p/1599781#M201569</link>
    <description>&lt;P&gt;Hello all,&lt;/P&gt;&lt;P&gt;I have bought&amp;nbsp;MIMXRT1160-EVK. So I am new with this EVK and MCUXpresso IDE.&lt;/P&gt;&lt;P&gt;I have created&amp;nbsp; a project with the SDK Wizard for CM7 composed of the Azure RTOS and the uart driver. I can compile the generated code and I can run it. Everything looks fine.&lt;/P&gt;&lt;P&gt;However, now, if I do exactly the same thing but I select CM4 as standalone. Then I compile the generated code, errors are displayed.&lt;/P&gt;&lt;P&gt;Could you tell me why I cannot compile the generated code with CM4? Thanks in advance!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 15 Feb 2023 18:30:09 GMT</pubDate>
    <dc:creator>Mc2023</dc:creator>
    <dc:date>2023-02-15T18:30:09Z</dc:date>
    <item>
      <title>Not possible to compile the generated code on CM4 using Azure RTOS and uart driver</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Not-possible-to-compile-the-generated-code-on-CM4-using-Azure/m-p/1599781#M201569</link>
      <description>&lt;P&gt;Hello all,&lt;/P&gt;&lt;P&gt;I have bought&amp;nbsp;MIMXRT1160-EVK. So I am new with this EVK and MCUXpresso IDE.&lt;/P&gt;&lt;P&gt;I have created&amp;nbsp; a project with the SDK Wizard for CM7 composed of the Azure RTOS and the uart driver. I can compile the generated code and I can run it. Everything looks fine.&lt;/P&gt;&lt;P&gt;However, now, if I do exactly the same thing but I select CM4 as standalone. Then I compile the generated code, errors are displayed.&lt;/P&gt;&lt;P&gt;Could you tell me why I cannot compile the generated code with CM4? Thanks in advance!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 15 Feb 2023 18:30:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Not-possible-to-compile-the-generated-code-on-CM4-using-Azure/m-p/1599781#M201569</guid>
      <dc:creator>Mc2023</dc:creator>
      <dc:date>2023-02-15T18:30:09Z</dc:date>
    </item>
    <item>
      <title>Re: Not possible to compile the generated code on CM4 using Azure RTOS and uart driver</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Not-possible-to-compile-the-generated-code-on-CM4-using-Azure/m-p/1606325#M202080</link>
      <description>&lt;P&gt;Hello, my name is Pavel, and I will be supporting your case, I review your questions, unfortunately, there is no information about that movement.&lt;/P&gt;
&lt;P&gt;This is the note app for move the applicacion maybe could help you to undesrtand.&lt;BR /&gt;&lt;A href="https://www.nxp.com/docs/en/application-note/AN13232.pdf" target="_blank"&gt;RT-Thread Board Port and Application Development (nxp.com)&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Then I recommend using the FreeRTOS examples of CM4 to review how this works and then you could try port again the CM7 azure example to the CM4.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Pavel_Hernandez_0-1677526302597.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/212526iE5EE7F8EEA96ABBC/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Pavel_Hernandez_0-1677526302597.png" alt="Pavel_Hernandez_0-1677526302597.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Pavel_Hernandez_0-1677526302597.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Pavel&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 27 Feb 2023 19:32:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Not-possible-to-compile-the-generated-code-on-CM4-using-Azure/m-p/1606325#M202080</guid>
      <dc:creator>Pavel_Hernandez</dc:creator>
      <dc:date>2023-02-27T19:32:11Z</dc:date>
    </item>
  </channel>
</rss>