<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: I need to communicate quectel module using usb protocol rt1170 for sending receiving AT commands in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/I-need-to-communicate-quectel-module-using-usb-protocol-rt1170/m-p/1596111#M201286</link>
    <description>&lt;P&gt;Hello, could you share the datasheet of the Q&lt;SPAN&gt;uectel or the pinout, maybe you need to use Uart to send the AT command through RX &amp;amp; TX, if that is the right protocol, you can use the example&amp;nbsp;from the SDK.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;Best&lt;SPAN&gt;&amp;nbsp;regards,&lt;BR /&gt;Pavel&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Thu, 09 Feb 2023 02:24:00 GMT</pubDate>
    <dc:creator>Pavel_Hernandez</dc:creator>
    <dc:date>2023-02-09T02:24:00Z</dc:date>
    <item>
      <title>I need to communicate quectel module using usb protocol rt1170 for sending receiving AT commands</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I-need-to-communicate-quectel-module-using-usb-protocol-rt1170/m-p/1593043#M201010</link>
      <description>&lt;P&gt;I need to communicate quectel module using usb protocol using rt1170 arm processor for sending receiving AT commands response, so for this i gone through the usb example but i couldn't able to understand what are parameters i need to change for this if any one knows what are thigs i need to know before starting modifications&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 03 Feb 2023 09:57:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I-need-to-communicate-quectel-module-using-usb-protocol-rt1170/m-p/1593043#M201010</guid>
      <dc:creator>Bharath_S</dc:creator>
      <dc:date>2023-02-03T09:57:29Z</dc:date>
    </item>
    <item>
      <title>Re: I need to communicate quectel module using usb protocol rt1170 for sending receiving AT commands</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I-need-to-communicate-quectel-module-using-usb-protocol-rt1170/m-p/1596111#M201286</link>
      <description>&lt;P&gt;Hello, could you share the datasheet of the Q&lt;SPAN&gt;uectel or the pinout, maybe you need to use Uart to send the AT command through RX &amp;amp; TX, if that is the right protocol, you can use the example&amp;nbsp;from the SDK.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;Best&lt;SPAN&gt;&amp;nbsp;regards,&lt;BR /&gt;Pavel&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 09 Feb 2023 02:24:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I-need-to-communicate-quectel-module-using-usb-protocol-rt1170/m-p/1596111#M201286</guid>
      <dc:creator>Pavel_Hernandez</dc:creator>
      <dc:date>2023-02-09T02:24:00Z</dc:date>
    </item>
  </channel>
</rss>