<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: imx8m plus - self boot in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx8m-plus-self-boot/m-p/1595997#M201276</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/211097"&gt;@YoavBenita&lt;/a&gt;,&lt;/P&gt;&lt;P&gt;It is right. Additionally, you will need to check the Security Reference Manual (NDA required) to work with the eFuses and change the boot mode.&lt;BR /&gt;Finally, if you want, you can use another source to change the default boot via software as a microcontroller connected to BOOT MODE pins.&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 08 Feb 2023 22:16:20 GMT</pubDate>
    <dc:creator>brian14</dc:creator>
    <dc:date>2023-02-08T22:16:20Z</dc:date>
    <item>
      <title>imx8m plus - self boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8m-plus-self-boot/m-p/1591405#M200910</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Is it possible for the IMX8M+ to control the boot ?&lt;/P&gt;&lt;P&gt;If i want to use the eMMC boot as default, but in the field be able to change the boot to be from USB without hardware changes.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 01 Feb 2023 15:08:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8m-plus-self-boot/m-p/1591405#M200910</guid>
      <dc:creator>YoavBenita</dc:creator>
      <dc:date>2023-02-01T15:08:35Z</dc:date>
    </item>
    <item>
      <title>Re: imx8m plus - self boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8m-plus-self-boot/m-p/1592744#M200988</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/211097"&gt;@YoavBenita&lt;/a&gt;,&lt;BR /&gt;&lt;BR /&gt;It is possible to change the boot source via software using the system controller in Linux and you can modify registers to change the boot mode.&lt;BR /&gt;For the first option, I suggest using the Linux iMX Reference Manual section 2.2 System Controller and for the second option, you will need to read iMX8M Plus Reference Manual section 6.5.2.6 Boot Mode Control.&lt;BR /&gt;&lt;BR /&gt;Link 1: &lt;A href="https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applications-processors:IMXLINUX" target="_self"&gt;Embedded Linux for i.MX Applications Processors | NXP Semiconductors&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;Link 2: &lt;A href="https://www.nxp.com/webapp/Download?colCode=IMX8MPRM" target="_self"&gt;https://www.nxp.com/webapp/Download?colCode=IMX8MPRM&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;I hope this information will be helpful.&lt;/P&gt;</description>
      <pubDate>Fri, 03 Feb 2023 02:53:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8m-plus-self-boot/m-p/1592744#M200988</guid>
      <dc:creator>brian14</dc:creator>
      <dc:date>2023-02-03T02:53:05Z</dc:date>
    </item>
    <item>
      <title>Re: imx8m plus - self boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8m-plus-self-boot/m-p/1592930#M201003</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Thank you for answer.&lt;/P&gt;&lt;P&gt;So, the BOOT can be changed by writing to registers and there is no need to connect some IO's to boot pins, right?&lt;/P&gt;&lt;P&gt;These registers do not change during programming/booting new image ?&lt;/P&gt;</description>
      <pubDate>Fri, 03 Feb 2023 08:12:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8m-plus-self-boot/m-p/1592930#M201003</guid>
      <dc:creator>YoavBenita</dc:creator>
      <dc:date>2023-02-03T08:12:17Z</dc:date>
    </item>
    <item>
      <title>Re: imx8m plus - self boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8m-plus-self-boot/m-p/1595997#M201276</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/211097"&gt;@YoavBenita&lt;/a&gt;,&lt;/P&gt;&lt;P&gt;It is right. Additionally, you will need to check the Security Reference Manual (NDA required) to work with the eFuses and change the boot mode.&lt;BR /&gt;Finally, if you want, you can use another source to change the default boot via software as a microcontroller connected to BOOT MODE pins.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 08 Feb 2023 22:16:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8m-plus-self-boot/m-p/1595997#M201276</guid>
      <dc:creator>brian14</dc:creator>
      <dc:date>2023-02-08T22:16:20Z</dc:date>
    </item>
    <item>
      <title>Re: imx8m plus - self boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8m-plus-self-boot/m-p/1597133#M201361</link>
      <description>&lt;P&gt;Thanks !&lt;/P&gt;</description>
      <pubDate>Fri, 10 Feb 2023 08:18:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8m-plus-self-boot/m-p/1597133#M201361</guid>
      <dc:creator>YoavBenita</dc:creator>
      <dc:date>2023-02-10T08:18:05Z</dc:date>
    </item>
  </channel>
</rss>