<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: iMX8MP + DDR4 : Why or why not?</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX8MP-DDR4-Why-or-why-not/m-p/1594728#M201150</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am in the process of defining the architecture of a new PCB using the iMX8MP.&lt;BR /&gt;&lt;BR /&gt;I have had the same observation as you regarding the lack of&amp;nbsp;iMX8MP + DDR4 designs from NXP and SoM designers. I also note that there is less detail in the application notes regarding a DDR4 based design. For example, the routing recommendations in the Hardware Design Guide appear to cover LPDDR4 only.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I also notice the following note in the HDG Table 3. "It is strongly suggested to use LPDDR4 if lower power consumption is required since DLL-off mode is not supported". This may help explain why there is a preference for LPDDR4.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Did you manage to resolve the issues you have faced?&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Tom&amp;nbsp;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 07 Feb 2023 12:10:37 GMT</pubDate>
    <dc:creator>Tperman_msi</dc:creator>
    <dc:date>2023-02-07T12:10:37Z</dc:date>
    <item>
      <title>iMX8MP + DDR4 : Why or why not?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8MP-DDR4-Why-or-why-not/m-p/1589960#M200798</link>
      <description>&lt;P&gt;Dear Experts,&lt;/P&gt;&lt;P&gt;While being stuck with the booting up from SD card of own custom board based on iMX8MP + DDR4, I would like to have your opinion about why there seems to be only iMX8MP + LPDDR4 from NXP partners and SOM makers? And for iMX8MP + DDR4 combination, there's only internal boards such as imx8mp-ddr4-evk or the &lt;A href="https://www.nxp.com/design/designs/ai-robot-platform-based-on-i-mx-8m-plus:AI-ROBOT-PLATFORM" target="_self"&gt;iMX8M Plus AI Robot&lt;/A&gt; which are only for internal use?&lt;/P&gt;&lt;P&gt;Anyway, the DDR4 training and initialization are successfully passed on our custom board. But u-Boot SPL is stuck at loading the ATF/BL31 as this later could not be found (magic word is incorrect).&lt;/P&gt;&lt;P&gt;Thanks in advance and best regards,&lt;BR /&gt;Khang&lt;/P&gt;</description>
      <pubDate>Mon, 30 Jan 2023 16:43:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8MP-DDR4-Why-or-why-not/m-p/1589960#M200798</guid>
      <dc:creator>khang_letruong</dc:creator>
      <dc:date>2023-01-30T16:43:38Z</dc:date>
    </item>
    <item>
      <title>Re: iMX8MP + DDR4 : Why or why not?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8MP-DDR4-Why-or-why-not/m-p/1594728#M201150</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am in the process of defining the architecture of a new PCB using the iMX8MP.&lt;BR /&gt;&lt;BR /&gt;I have had the same observation as you regarding the lack of&amp;nbsp;iMX8MP + DDR4 designs from NXP and SoM designers. I also note that there is less detail in the application notes regarding a DDR4 based design. For example, the routing recommendations in the Hardware Design Guide appear to cover LPDDR4 only.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I also notice the following note in the HDG Table 3. "It is strongly suggested to use LPDDR4 if lower power consumption is required since DLL-off mode is not supported". This may help explain why there is a preference for LPDDR4.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Did you manage to resolve the issues you have faced?&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Tom&amp;nbsp;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 07 Feb 2023 12:10:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8MP-DDR4-Why-or-why-not/m-p/1594728#M201150</guid>
      <dc:creator>Tperman_msi</dc:creator>
      <dc:date>2023-02-07T12:10:37Z</dc:date>
    </item>
    <item>
      <title>Re: iMX8MP + DDR4 : Why or why not?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8MP-DDR4-Why-or-why-not/m-p/1594742#M201153</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/212274"&gt;@Tperman_msi&lt;/a&gt; ,&lt;/P&gt;&lt;P&gt;I am in the process of bringing up a custom iMX8MP + DDR4 based board, inspired from imx8mp-ddr4-evk. Currently we are receiving the help from NXP technical support but there's not been important progress in resolving the issue yet.&lt;/P&gt;&lt;P&gt;Regards,&lt;BR /&gt;K.&lt;/P&gt;</description>
      <pubDate>Tue, 07 Feb 2023 12:36:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8MP-DDR4-Why-or-why-not/m-p/1594742#M201153</guid>
      <dc:creator>khang_letruong</dc:creator>
      <dc:date>2023-02-07T12:36:56Z</dc:date>
    </item>
    <item>
      <title>Re: iMX8MP + DDR4 : Why or why not?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8MP-DDR4-Why-or-why-not/m-p/1599395#M201525</link>
      <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/147542"&gt;@khang_letruong&lt;/a&gt; How is the status in your side?&lt;/P&gt;</description>
      <pubDate>Wed, 15 Feb 2023 07:56:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8MP-DDR4-Why-or-why-not/m-p/1599395#M201525</guid>
      <dc:creator>Rita_Wang</dc:creator>
      <dc:date>2023-02-15T07:56:31Z</dc:date>
    </item>
    <item>
      <title>Re: iMX8MP + DDR4 : Why or why not?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8MP-DDR4-Why-or-why-not/m-p/1599552#M201548</link>
      <description>&lt;P&gt;Dear &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/57740"&gt;@Rita_Wang&lt;/a&gt; ,&lt;/P&gt;&lt;P&gt;Unfortunately we are still being blocked due to ATF (BL31) not found. We are also being supported by NXP Technical Support but nothing special has been found yet.&lt;/P&gt;&lt;P&gt;Regards,&lt;BR /&gt;Khang&lt;/P&gt;</description>
      <pubDate>Wed, 15 Feb 2023 11:16:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8MP-DDR4-Why-or-why-not/m-p/1599552#M201548</guid>
      <dc:creator>khang_letruong</dc:creator>
      <dc:date>2023-02-15T11:16:37Z</dc:date>
    </item>
    <item>
      <title>Re: iMX8MP + DDR4 : Why or why not?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8MP-DDR4-Why-or-why-not/m-p/1600175#M201586</link>
      <description>&lt;P&gt;Dear &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/147542"&gt;@khang_letruong&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Our another engineer is dealing it for you. Any question you can contact him freely.&lt;/P&gt;
&lt;P&gt;Wish you have a nice day&lt;/P&gt;
&lt;P&gt;Best Regards&lt;/P&gt;
&lt;P&gt;Rita&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 16 Feb 2023 04:53:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8MP-DDR4-Why-or-why-not/m-p/1600175#M201586</guid>
      <dc:creator>Rita_Wang</dc:creator>
      <dc:date>2023-02-16T04:53:36Z</dc:date>
    </item>
  </channel>
</rss>