<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: MIMX.RT685 power sequencing</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/MIMX-RT685-power-sequencing/m-p/1593724#M201069</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/210490"&gt;@leduclong&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;Seems fine.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Jing&lt;/P&gt;</description>
    <pubDate>Mon, 06 Feb 2023 07:37:32 GMT</pubDate>
    <dc:creator>jingpan</dc:creator>
    <dc:date>2023-02-06T07:37:32Z</dc:date>
    <item>
      <title>MIMX.RT685 power sequencing</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MIMX-RT685-power-sequencing/m-p/1589463#M200765</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I would like to consult you about the valid power sequencing of iMX.RT685.&lt;/P&gt;&lt;P&gt;From the data sheet:&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Following power-on sequence should be followed when using an external PMIC or external IC to drive the VDDCORE pin (internal LDO is disabled, see timing diagram below):&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;1. VDD_AO1V8, VDD1V8, and VDD1V8_1 pins should be powered first. There is no&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;power sequence requirement between powering the VDD_AO1V8 and VDD1V8 pins.&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;&lt;EM&gt;2. VDDA_ADC1V8 and VREFP can be powered concurrently with VDD_AO1V8 and&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;VDD1V8 or later.&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;&lt;EM&gt;3. VDDIO_x and VDDA_BIAS pins can be powered concurrently with VDD_AO1V8 and&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;VDD1V8 if these pins are 1.8 V range or later if these pins are 3.3 V range. If the&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;VDDIO_x is not powered concurrently with the VDD1V8, the delta voltage between&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;VDDIO_x and VDD1V8 must be 1.89 V or less.&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;&lt;EM&gt;4. Power up the VDDCORE. The external RESETN should be held low until VDDCORE&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;is valid in the timing diagram.VDDCORE should not be ramped up until after all the&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;other supplies have completed ramp up.&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;Will the following power sequence work?&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;1. Power up the VDD1V8, VDD1V8_1, VDDIO_0 and VDDIO_2 (both at 1.8V)&lt;/P&gt;&lt;P&gt;2. Power up VDDAO_1V8&lt;/P&gt;&lt;P&gt;3. Power up VDDIO_1 at 1V8 (later to be changed to 2V8)&lt;/P&gt;&lt;P&gt;4. Power up VDDCORE at 1V0&lt;/P&gt;&lt;P&gt;5. Release the RESETn&lt;/P&gt;&lt;P&gt;Thank you for your support.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 30 Jan 2023 04:39:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MIMX-RT685-power-sequencing/m-p/1589463#M200765</guid>
      <dc:creator>leduclong</dc:creator>
      <dc:date>2023-01-30T04:39:53Z</dc:date>
    </item>
    <item>
      <title>Re: MIMX.RT685 power sequencing</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MIMX-RT685-power-sequencing/m-p/1593724#M201069</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/210490"&gt;@leduclong&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;Seems fine.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Jing&lt;/P&gt;</description>
      <pubDate>Mon, 06 Feb 2023 07:37:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MIMX-RT685-power-sequencing/m-p/1593724#M201069</guid>
      <dc:creator>jingpan</dc:creator>
      <dc:date>2023-02-06T07:37:32Z</dc:date>
    </item>
  </channel>
</rss>