<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic incorrect pin direction using NXPXSPRESSO in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/incorrect-pin-direction-using-NXPXSPRESSO/m-p/1593498#M201053</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;We work on&amp;nbsp;&lt;SPAN class=""&gt;MIMXRT1051CVL5B&lt;/SPAN&gt;&amp;nbsp;using&amp;nbsp;NXPXSPRESSO, and we have issue with some pin directions:&lt;/P&gt;&lt;P&gt;1. PMIC_ON_REQ should be an output pin that enables the main board power once the SNVS voltage is up. The SW seems to consider it as an input signal, and it can't be changed.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="sapirbuz_0-1675605693280.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/209611iA58906EED50D322C/image-size/medium?v=v2&amp;amp;px=400" role="button" title="sapirbuz_0-1675605693280.png" alt="sapirbuz_0-1675605693280.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;2. pin G13 JTAG_TDO should be defined as output, but the SW seems to consider it as an input signal,&amp;nbsp;and it can't be changed.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Can you please help define the correct direction for the pins?&lt;/P&gt;</description>
    <pubDate>Sun, 05 Feb 2023 14:12:52 GMT</pubDate>
    <dc:creator>sapirbuz</dc:creator>
    <dc:date>2023-02-05T14:12:52Z</dc:date>
    <item>
      <title>incorrect pin direction using NXPXSPRESSO</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/incorrect-pin-direction-using-NXPXSPRESSO/m-p/1593498#M201053</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;We work on&amp;nbsp;&lt;SPAN class=""&gt;MIMXRT1051CVL5B&lt;/SPAN&gt;&amp;nbsp;using&amp;nbsp;NXPXSPRESSO, and we have issue with some pin directions:&lt;/P&gt;&lt;P&gt;1. PMIC_ON_REQ should be an output pin that enables the main board power once the SNVS voltage is up. The SW seems to consider it as an input signal, and it can't be changed.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="sapirbuz_0-1675605693280.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/209611iA58906EED50D322C/image-size/medium?v=v2&amp;amp;px=400" role="button" title="sapirbuz_0-1675605693280.png" alt="sapirbuz_0-1675605693280.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;2. pin G13 JTAG_TDO should be defined as output, but the SW seems to consider it as an input signal,&amp;nbsp;and it can't be changed.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Can you please help define the correct direction for the pins?&lt;/P&gt;</description>
      <pubDate>Sun, 05 Feb 2023 14:12:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/incorrect-pin-direction-using-NXPXSPRESSO/m-p/1593498#M201053</guid>
      <dc:creator>sapirbuz</dc:creator>
      <dc:date>2023-02-05T14:12:52Z</dc:date>
    </item>
    <item>
      <title>Re: incorrect pin direction using NXPXSPRESSO</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/incorrect-pin-direction-using-NXPXSPRESSO/m-p/1595089#M201189</link>
      <description>&lt;P&gt;Hello&lt;BR /&gt;Hope you are well.&lt;/P&gt;
&lt;P&gt;1. PMIC_ON_REQ is output and the direction cannot be changed by software:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Omar_Anguiano_0-1675816704886.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/209999i4D1293CC3785A6EF/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Omar_Anguiano_0-1675816704886.png" alt="Omar_Anguiano_0-1675816704886.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;2. The default from the datasheet is an input however as JTAG is the default functionality we can say that it is:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Omar_Anguiano_1-1675816747770.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/210000iB944A68EF63684C5/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Omar_Anguiano_1-1675816747770.png" alt="Omar_Anguiano_1-1675816747770.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Omar&lt;/P&gt;</description>
      <pubDate>Wed, 08 Feb 2023 00:40:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/incorrect-pin-direction-using-NXPXSPRESSO/m-p/1595089#M201189</guid>
      <dc:creator>Omar_Anguiano</dc:creator>
      <dc:date>2023-02-08T00:40:54Z</dc:date>
    </item>
    <item>
      <title>Re: incorrect pin direction using NXPXSPRESSO</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/incorrect-pin-direction-using-NXPXSPRESSO/m-p/1595577#M201247</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;We know the direction of those pins, but our problem is that they are defined incorrectly in the SW&amp;nbsp;NXPXSPRESSO.&lt;/P&gt;&lt;P&gt;We don't know how to change the incorrect pin's direction in the SW&lt;/P&gt;</description>
      <pubDate>Wed, 08 Feb 2023 12:17:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/incorrect-pin-direction-using-NXPXSPRESSO/m-p/1595577#M201247</guid>
      <dc:creator>sapirbuz</dc:creator>
      <dc:date>2023-02-08T12:17:21Z</dc:date>
    </item>
    <item>
      <title>Re: incorrect pin direction using NXPXSPRESSO</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/incorrect-pin-direction-using-NXPXSPRESSO/m-p/1596828#M201339</link>
      <description>&lt;P&gt;This is more a typo of the tool however the direction of those pins is not affected by this. In the case of G13, the direction is given by functionality. Depending on the functionality, the tool can change direction. On the PMIC_ON_REQ pin, the direction cannot be changed.&lt;BR /&gt;It will be helpful to report this typo to avoid further confusion on the direction of the pins.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Omar&lt;/P&gt;</description>
      <pubDate>Thu, 09 Feb 2023 20:06:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/incorrect-pin-direction-using-NXPXSPRESSO/m-p/1596828#M201339</guid>
      <dc:creator>Omar_Anguiano</dc:creator>
      <dc:date>2023-02-09T20:06:11Z</dc:date>
    </item>
  </channel>
</rss>