<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Does IMXRT1176 supports the DoIP protocol ? in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Does-IMXRT1176-supports-the-DoIP-protocol/m-p/1593159#M201021</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;We are using the IMXRT1170-EVK board, we wanted to work on DoIP protocol. Does this controller is capable of supporting the DoIP ? Is this controller meets all the requirements for supporting the DoIP ? requirements like network connectivity, security and memory etc..&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Please suggest.&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;</description>
    <pubDate>Fri, 03 Feb 2023 13:18:28 GMT</pubDate>
    <dc:creator>Shiva-2022</dc:creator>
    <dc:date>2023-02-03T13:18:28Z</dc:date>
    <item>
      <title>Does IMXRT1176 supports the DoIP protocol ?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Does-IMXRT1176-supports-the-DoIP-protocol/m-p/1593159#M201021</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;We are using the IMXRT1170-EVK board, we wanted to work on DoIP protocol. Does this controller is capable of supporting the DoIP ? Is this controller meets all the requirements for supporting the DoIP ? requirements like network connectivity, security and memory etc..&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Please suggest.&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;</description>
      <pubDate>Fri, 03 Feb 2023 13:18:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Does-IMXRT1176-supports-the-DoIP-protocol/m-p/1593159#M201021</guid>
      <dc:creator>Shiva-2022</dc:creator>
      <dc:date>2023-02-03T13:18:28Z</dc:date>
    </item>
    <item>
      <title>Re: Does IMXRT1176 supports the DoIP protocol ?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Does-IMXRT1176-supports-the-DoIP-protocol/m-p/1595927#M201271</link>
      <description>&lt;P&gt;Hello&lt;BR /&gt;I hope you are well.&lt;/P&gt;
&lt;P&gt;I'm not able to confirm if this device is suitable for DoIP since I do not know the specific requirements for that application.&lt;/P&gt;
&lt;P&gt;RT1170 features make possible the use of Ethernet, FlexCAN. It is possible to add external memories but I cannot assure you that these features can fulfill your specific application.&lt;/P&gt;
&lt;P&gt;Unfortunately, we do not have any example of this but if you provide more detail about the specific requirements of your application we could have better criteria to check if this device is suitable.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Omar&lt;/P&gt;</description>
      <pubDate>Wed, 08 Feb 2023 19:20:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Does-IMXRT1176-supports-the-DoIP-protocol/m-p/1595927#M201271</guid>
      <dc:creator>Omar_Anguiano</dc:creator>
      <dc:date>2023-02-08T19:20:55Z</dc:date>
    </item>
    <item>
      <title>Re: Does IMXRT1176 supports the DoIP protocol ?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Does-IMXRT1176-supports-the-DoIP-protocol/m-p/1598120#M201434</link>
      <description>Hello Omar,&lt;BR /&gt;Thanks for the reply.&lt;BR /&gt;Currently we are using FlexCAN for flashing the application via UDS protocol.&lt;BR /&gt;We wanted to the do same using the Ethernet for flashing the application via DoIP.&lt;BR /&gt;&lt;BR /&gt;Please let me know if you need more info.&lt;BR /&gt;</description>
      <pubDate>Mon, 13 Feb 2023 10:45:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Does-IMXRT1176-supports-the-DoIP-protocol/m-p/1598120#M201434</guid>
      <dc:creator>Shiva-2022</dc:creator>
      <dc:date>2023-02-13T10:45:27Z</dc:date>
    </item>
    <item>
      <title>Re: Does IMXRT1176 supports the DoIP protocol ?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Does-IMXRT1176-supports-the-DoIP-protocol/m-p/1601334#M201663</link>
      <description>&lt;P&gt;Thank you for the details. Unfortunately, I cannot confirm if RT1170 is suitable for this end.&lt;BR /&gt;We will need to check if the core/memory/modules are enough to integrate a DoIP application over Ethernet. Do you know the requirements of DoIP?&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Omar&lt;/P&gt;</description>
      <pubDate>Fri, 17 Feb 2023 20:56:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Does-IMXRT1176-supports-the-DoIP-protocol/m-p/1601334#M201663</guid>
      <dc:creator>Omar_Anguiano</dc:creator>
      <dc:date>2023-02-17T20:56:32Z</dc:date>
    </item>
  </channel>
</rss>