<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: CPU1: failed to come online</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/CPU1-failed-to-come-online/m-p/1593061#M201013</link>
    <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/115929"&gt;@raymondman&lt;/a&gt;, did you find a solution to your problem? I'm also having the problem with the 1GB/2GB in U-Boot, I suspect optee to cause the problem at my end. I got my kernel running by adding a kernel-boot-param&amp;nbsp; "mem=1024MB" to circumvent this, perhaps this might help you too.&lt;/P&gt;</description>
    <pubDate>Fri, 03 Feb 2023 10:14:55 GMT</pubDate>
    <dc:creator>dpog</dc:creator>
    <dc:date>2023-02-03T10:14:55Z</dc:date>
    <item>
      <title>CPU1: failed to come online</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/CPU1-failed-to-come-online/m-p/1529496#M195734</link>
      <description>&lt;P&gt;The custom board is using iMX8M Mini processor. We upgrade from Hardknott to Kirkstone and use mender. But after flashing the image, we have two problems.&lt;/P&gt;&lt;P&gt;1) the RAM size has been set to 1GB in imx8mm_evk.h. The devicetree also has the following setting.&lt;/P&gt;&lt;P&gt;memory@40000000 {&lt;BR /&gt;device_type = "memory";&lt;BR /&gt;&amp;nbsp;reg = &amp;lt;0x0 0x40000000 0 0x40000000&amp;gt;;&lt;BR /&gt;};&lt;/P&gt;&lt;P&gt;But U-boot shows it as 2GiB as follow.&lt;/P&gt;&lt;P&gt;U-Boot 2022.04-lf_v2022.04+g1c881f4da8 (Jun 07 2022 - 05:16:02 +0000)&lt;/P&gt;&lt;P&gt;CPU: i.MX8MMQ rev1.0 1800 MHz (running at 1200 MHz)&lt;BR /&gt;CPU: Commercial temperature grade (0C to 95C) at 58C&lt;BR /&gt;Reset cause: POR&lt;BR /&gt;Model: NXP i.MX8MM EVK board&lt;BR /&gt;DRAM: 2 GiB&lt;/P&gt;&lt;P&gt;2) The log also shows that other 3 CPU cannot come online.&lt;/P&gt;&lt;P&gt;[ 0.002781] smp: Bringing up secondary CPUs ...&lt;BR /&gt;[ 5.091634] CPU1: failed to come online&lt;BR /&gt;[ 5.091642] CPU1: failed in unknown state : 0x0&lt;BR /&gt;[ 10.215331] CPU2: failed to come online&lt;BR /&gt;[ 10.215338] CPU2: failed in unknown state : 0x0&lt;BR /&gt;[ 15.339028] CPU3: failed to come online&lt;BR /&gt;[ 15.339035] CPU3: failed in unknown state : 0x0&lt;BR /&gt;[ 15.339079] smp: Brought up 1 node, 1 CPU&lt;/P&gt;&lt;P&gt;In the Hardknott version, all can work perfectly. Does anyone have any advice?&lt;/P&gt;&lt;P&gt;Many thanks!&lt;/P&gt;</description>
      <pubDate>Wed, 28 Sep 2022 11:03:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/CPU1-failed-to-come-online/m-p/1529496#M195734</guid>
      <dc:creator>raymondman</dc:creator>
      <dc:date>2022-09-28T11:03:21Z</dc:date>
    </item>
    <item>
      <title>Re: CPU1: failed to come online</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/CPU1-failed-to-come-online/m-p/1576437#M199414</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I use iMX8QXP, &lt;SPAN&gt;imx-yocto-L5.4.24_2.1.0, also meet the problem.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;[ 0.047913] smp: Bringing up secondary CPUs ...&lt;BR /&gt;[ 5.092627] CPU1: failed to come online&lt;BR /&gt;[ 5.092636] CPU1: failed in unknown state : 0x0&lt;BR /&gt;[ 10.217413] CPU2: failed to come online&lt;BR /&gt;[ 10.217422] CPU2: failed in unknown state : 0x0&lt;BR /&gt;[ 15.342180] CPU3: failed to come online&lt;BR /&gt;[ 15.342189] CPU3: failed in unknown state : 0x0&lt;BR /&gt;[ 15.342237] smp: Brought up 1 node, 1 CPU&lt;BR /&gt;[ 15.342243] SMP: Total of 1 processors activated.&lt;/P&gt;&lt;P&gt;Could you tell me how you solved the problem?&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;</description>
      <pubDate>Tue, 03 Jan 2023 08:49:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/CPU1-failed-to-come-online/m-p/1576437#M199414</guid>
      <dc:creator>Chenyi_Luo</dc:creator>
      <dc:date>2023-01-03T08:49:54Z</dc:date>
    </item>
    <item>
      <title>Re: CPU1: failed to come online</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/CPU1-failed-to-come-online/m-p/1593061#M201013</link>
      <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/115929"&gt;@raymondman&lt;/a&gt;, did you find a solution to your problem? I'm also having the problem with the 1GB/2GB in U-Boot, I suspect optee to cause the problem at my end. I got my kernel running by adding a kernel-boot-param&amp;nbsp; "mem=1024MB" to circumvent this, perhaps this might help you too.&lt;/P&gt;</description>
      <pubDate>Fri, 03 Feb 2023 10:14:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/CPU1-failed-to-come-online/m-p/1593061#M201013</guid>
      <dc:creator>dpog</dc:creator>
      <dc:date>2023-02-03T10:14:55Z</dc:date>
    </item>
  </channel>
</rss>