<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: yocto wic image automatically extend the partition</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/yocto-wic-image-automatically-extend-the-partition/m-p/1591974#M200941</link>
    <description>&lt;P&gt;&lt;SPAN&gt;I had the same problem on S32G2, The default fsl-image-auto.sdcard built by Yocto can not opcuppy the entired 32G eMMc&amp;nbsp;When booting. &amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Can any body help me to solve the problem? And we don't want to&amp;nbsp;manually part the eMMc using fdisk.&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Thu, 02 Feb 2023 06:40:17 GMT</pubDate>
    <dc:creator>Jackie_Zhou</dc:creator>
    <dc:date>2023-02-02T06:40:17Z</dc:date>
    <item>
      <title>yocto wic image automatically extend the partition</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/yocto-wic-image-automatically-extend-the-partition/m-p/1492370#M192762</link>
      <description>&lt;P&gt;hi，&lt;/P&gt;&lt;P&gt;The wic.bz2 image I compiled now is burned into EMMC. The partition used by the system cannot occupy the size of the entire EMMC. Is there any way to automatically expand the root directory partition so that emmc can be fully used?&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
      <pubDate>Wed, 20 Jul 2022 10:00:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/yocto-wic-image-automatically-extend-the-partition/m-p/1492370#M192762</guid>
      <dc:creator>songhongliang</dc:creator>
      <dc:date>2022-07-20T10:00:30Z</dc:date>
    </item>
    <item>
      <title>Re: yocto wic image automatically extend the partition</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/yocto-wic-image-automatically-extend-the-partition/m-p/1495475#M193039</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/158777"&gt;@songhongliang&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;The command fdisk can help partitioning. Please refer to section 4 Booting Linux OS of IMX_LINUX_USER_GUIDE.pdf&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/webapp/Download?colCode=IMX_LINUX_USERS_GUIDE" target="_blank"&gt;https://www.nxp.com/webapp/Download?colCode=IMX_LINUX_USERS_GUIDE&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Best regards&lt;/P&gt;
&lt;P&gt;Harvey&lt;/P&gt;</description>
      <pubDate>Tue, 26 Jul 2022 09:11:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/yocto-wic-image-automatically-extend-the-partition/m-p/1495475#M193039</guid>
      <dc:creator>Harvey021</dc:creator>
      <dc:date>2022-07-26T09:11:48Z</dc:date>
    </item>
    <item>
      <title>Re: yocto wic image automatically extend the partition</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/yocto-wic-image-automatically-extend-the-partition/m-p/1495923#M193064</link>
      <description>&lt;P&gt;HI&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;What I mean is that after flashing the image file, the root directory can be covered with the rest of the entire emmc.&lt;/SPAN&gt; &lt;SPAN class=""&gt;Just like Android, it can automatically expand to maximize the user partition.&lt;/SPAN&gt; &lt;SPAN class=""&gt;Rather than start and then execute the fdisk command to extend the partition.&lt;/SPAN&gt; &lt;SPAN class=""&gt;I want it to be done automatically after the first boot.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;Thanks!&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 27 Jul 2022 02:06:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/yocto-wic-image-automatically-extend-the-partition/m-p/1495923#M193064</guid>
      <dc:creator>songhongliang</dc:creator>
      <dc:date>2022-07-27T02:06:30Z</dc:date>
    </item>
    <item>
      <title>Re: yocto wic image automatically extend the partition</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/yocto-wic-image-automatically-extend-the-partition/m-p/1591974#M200941</link>
      <description>&lt;P&gt;&lt;SPAN&gt;I had the same problem on S32G2, The default fsl-image-auto.sdcard built by Yocto can not opcuppy the entired 32G eMMc&amp;nbsp;When booting. &amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Can any body help me to solve the problem? And we don't want to&amp;nbsp;manually part the eMMc using fdisk.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 02 Feb 2023 06:40:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/yocto-wic-image-automatically-extend-the-partition/m-p/1591974#M200941</guid>
      <dc:creator>Jackie_Zhou</dc:creator>
      <dc:date>2023-02-02T06:40:17Z</dc:date>
    </item>
  </channel>
</rss>