<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: iMX8MP: VPU hangs after playback</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX8MP-VPU-hangs-after-playback/m-p/1591744#M200924</link>
    <description>&lt;P&gt;Hi Joanxie,&lt;/P&gt;&lt;P&gt;As I mentioned before, I am using EVK image to test VPU.&lt;BR /&gt;I am just appending our uboot on top of EVK image and this should replicate EVK behaviour in our board as well.&lt;/P&gt;&lt;P&gt;Could you please share the image that you used for testing VPU in EVK so that i can test here as well to understand the issue.&lt;/P&gt;&lt;P&gt;Also, we are using 4G memory compared to 6G memory used in EVK.&lt;BR /&gt;I find the below cma settings in evk dtb.&lt;/P&gt;&lt;P&gt;linux,cma {&lt;BR /&gt;compatible = "shared-dma-pool";&lt;BR /&gt;reusable;&lt;BR /&gt;size = &amp;lt;0 0x3c000000&amp;gt;;&lt;BR /&gt;alloc-ranges = &amp;lt;0 0x40000000 0 0xC0000000&amp;gt;;&lt;BR /&gt;linux,cma-default;&lt;BR /&gt;};&lt;/P&gt;&lt;P&gt;Do we need to modify CMA node in DTB for 4G memory size?&lt;BR /&gt;Please share your inputs.&lt;BR /&gt;Also please share the evk image used for testing VPU.&lt;/P&gt;&lt;P&gt;Regards,&lt;BR /&gt;Santhana Kumar&lt;/P&gt;</description>
    <pubDate>Wed, 01 Feb 2023 23:35:53 GMT</pubDate>
    <dc:creator>santhanakumar</dc:creator>
    <dc:date>2023-02-01T23:35:53Z</dc:date>
    <item>
      <title>iMX8MP: VPU hangs after playback</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8MP-VPU-hangs-after-playback/m-p/1589287#M200743</link>
      <description>&lt;P&gt;Hi Everyone,&lt;/P&gt;&lt;P&gt;We have a custom board based on imx8mp.&lt;BR /&gt;I tried to build the latest Yocto (Yocto version: Kirkstone, Linux Kernel version: 5.15) following the below document:&lt;BR /&gt;&lt;A href="https://www.nxp.com/docs/en/user-guide/IMX_YOCTO_PROJECT_USERS_GUIDE.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/user-guide/IMX_YOCTO_PROJECT_USERS_GUIDE.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;I configured Yocto with the below parameters:&lt;BR /&gt;Distro:&lt;STRONG&gt; fsl-imx-xwayland&lt;/STRONG&gt;&lt;BR /&gt;Machine: &lt;STRONG&gt;imx8mp-lpddr4-evk&lt;/STRONG&gt;&lt;BR /&gt;Image: &lt;STRONG&gt;imx-image-full&lt;/STRONG&gt;&lt;BR /&gt;I could able to build the image successfully.&lt;/P&gt;&lt;P&gt;I did not make any changes to the SDK and generated default image for imx8mp evk.&lt;BR /&gt;I then tried to evaluate VPU by running gstreamer and able to play 1080p video without issues.&lt;BR /&gt;But system freezes after playback is complete.&lt;BR /&gt;Please find the below logs for the same.&lt;/P&gt;&lt;P&gt;root@imx8mp:~# gst-pl ay -1.0 /sample_video.MOV&lt;BR /&gt;Press 'k' to see a list of keyboard shortcuts.&lt;BR /&gt;Now playing /sample_video.MOV&lt;BR /&gt;Prerolling...&lt;BR /&gt;====== AIUR: 4.7.1 build on Jul 19 2022 06:15:03. ======&lt;BR /&gt;Core: MPEG4PARSER_06.20.06 build on May 7 2022 07:52:31&lt;BR /&gt;file: /usr/lib/imx-mm/parser/lib_mp4_parser_arm_elinux.so.3.2&lt;BR /&gt;------------------------&lt;BR /&gt;Track 00 [audio_0] Enabled&lt;BR /&gt;Duration: 0:00:16.904126000&lt;BR /&gt;Language: und&lt;BR /&gt;Mime:&lt;BR /&gt;audio/mpeg, mpegversion=(int)4, channels=(int)2, rate=(int)44100, bitrate=(int)0, stream-format=(string)raw, codec_data=(buffer)1210&lt;BR /&gt;------------------------&lt;/P&gt;&lt;P&gt;====== BEEP: 4.7.1 build on Jul[ 22.313492] remoteproc remoteproc0: powering up imx-dsp-rproc&lt;BR /&gt;19 2022 06:15:03. ======&lt;BR /&gt;Core: DSP decoder Wrapper build on May 19 2022 08:49:06&lt;BR /&gt;file: /usr/lib/imx-mm/audio-codec/wrap/lib_dsp_wrap_arm_elinux.so&lt;BR /&gt;[ 22.333189] remoteproc remoteproc0: Booting fw image imx/dsp/hifi4.bin, size 804421&lt;BR /&gt;[ 22.344940] remoteproc0#vdev0buffer: assigned reserved memory node vdev0buffer@94300000&lt;BR /&gt;[ 22.353798] virtio_rpmsg_bus virtio0: rpmsg host is online&lt;BR /&gt;[ 22.354296] virtio_rpmsg_bus virtio0: creating channel rpmsg-raw addr 0x1&lt;BR /&gt;[ 22.359491] remoteproc0#vdev0buffer: registered virtio0 (type 7)&lt;BR /&gt;[ 22.366735] virtio_rpmsg_bus virtio0: creating channel rpmsg-raw addr 0x2&lt;BR /&gt;[ 22.372792] remoteproc remoteproc0: remote processor imx-dsp-rproc is now up&lt;BR /&gt;Audio Device Ready&lt;BR /&gt;------------------------&lt;BR /&gt;Track 01 [video_0] Enabled&lt;BR /&gt;Duration: 0:00:16.850000000&lt;BR /&gt;Language: und&lt;BR /&gt;Mime:&lt;BR /&gt;video/x-h264, parsed=(boolean)true, alignment=(string)au, stream-format=(string)avc, width=(int)1920, height=(int)1080, framerate=(fraction)60/1, codec_data=(buffer)0164002affe100102764002aac56c0780227e59a8080808101000428ee3cb0fdf8f800&lt;BR /&gt;------------------------&lt;BR /&gt;Track 02 [subtitle]: Disabled&lt;BR /&gt;Codec: 0, SubCodec: 0&lt;BR /&gt;------------------------&lt;BR /&gt;Track 03 [subtitle]: Disabled&lt;BR /&gt;Codec: 0, SubCodec: 0&lt;BR /&gt;------------------------&lt;BR /&gt;Track 04 [subtitle]: Disabled&lt;BR /&gt;Codec: 0, SubCodec: 0&lt;BR /&gt;------------------------&lt;/P&gt;&lt;P&gt;====== V4L2DEC: 1.20.0 build on Jul 28 2022 06:57:16. ======&lt;BR /&gt;Redistribute latency...&lt;/P&gt;&lt;P&gt;===!!! Current pulsesink device is alsa_output.platform-sound-xcvr.iec958-stereo !!!===&lt;/P&gt;&lt;P&gt;Redistribute latency...&lt;BR /&gt;0:00:00.0 / 0:00:16.8&lt;BR /&gt;0:00:16.9 / 0:00:16.8&lt;BR /&gt;Reached end of play list.&lt;BR /&gt;Total showed frames (1011), playing for (0:00:16.905064000), fps (59.805).&lt;BR /&gt;[ 39.566308] remoteproc remoteproc0: stopped remote processor imx-dsp-rproc&lt;BR /&gt;[ 60.574505] rcu: INFO: rcu_preempt detected stalls on CPUs/tasks:&lt;BR /&gt;[ 60.580627] rcu: 3-...0: (0 ticks this GP) idle=0c1/1/0x4000000000000000 softirq=6730/6732 fqs=2571&lt;BR /&gt;[ 60.589853] (detected by 2, t=5254 jiffies, g=8953, q=5495)&lt;BR /&gt;[ 60.595514] Task dump for CPU 3:&lt;BR /&gt;[ 60.598744] task:vsidaemon state:R running task stack: 0 pid: 836 ppid: 2 flags:0x00000202&lt;BR /&gt;[ 60.608666] Call trace:&lt;BR /&gt;[ 60.611109] __switch_to+0x108/0x160&lt;BR /&gt;[ 60.614698] genpd_runtime_suspend+0x118/0x2c0&lt;BR /&gt;[ 60.619147] __rpm_callback+0x48/0x170&lt;BR /&gt;[ 60.622898] rpm_callback+0x6c/0x80&lt;BR /&gt;[ 60.626388] rpm_suspend+0x100/0x554&lt;BR /&gt;[ 60.629965] rpm_idle+0xf4/0x154&lt;BR /&gt;[ 60.633194] __pm_runtime_idle+0x60/0xb0&lt;BR /&gt;[ 60.637120] hantrodec_release+0x1c8/0x240&lt;BR /&gt;[ 60.641221] __fput+0x70/0x234&lt;BR /&gt;[ 60.644280] ____fput+0x14/0x20&lt;BR /&gt;[ 60.647423] task_work_run+0x84/0x17c&lt;BR /&gt;[ 60.651088] do_notify_resume+0x208/0x12ec&lt;BR /&gt;[ 60.655186] el0_svc+0x6c/0x80&lt;BR /&gt;[ 60.658246] el0t_64_sync_handler+0xa8/0x130&lt;BR /&gt;[ 60.662518] el0t_64_sync+0x1a0/0x1a4&lt;BR /&gt;[ 123.683477] rcu: INFO: rcu_preempt detected stalls on CPUs/tasks:&lt;BR /&gt;[ 123.689590] rcu: 3-...0: (0 ticks this GP) idle=0c1/1/0x4000000000000000 softirq=6730/6732 fqs=10343&lt;BR /&gt;[ 123.698903] (detected by 1, t=21032 jiffies, g=8953, q=20683)&lt;BR /&gt;[ 123.704737] Task dump for CPU 3:&lt;BR /&gt;[ 123.707963] task:vsidaemon state:R running task stack: 0 pid: 836 ppid: 2 flags:0x00000202&lt;BR /&gt;[ 123.717884] Call trace:&lt;BR /&gt;[ 123.720329] __switch_to+0x108/0x160&lt;BR /&gt;[ 123.723916] genpd_runtime_suspend+0x118/0x2c0&lt;BR /&gt;[ 123.728367] __rpm_callback+0x48/0x170&lt;BR /&gt;[ 123.732122] rpm_callback+0x6c/0x80&lt;BR /&gt;[ 123.735613] rpm_suspend+0x100/0x554&lt;BR /&gt;[ 123.739192] rpm_idle+0xf4/0x154&lt;BR /&gt;[ 123.742421] __pm_runtime_idle+0x60/0xb0&lt;BR /&gt;[ 123.746345] hantrodec_release+0x1c8/0x240&lt;BR /&gt;[ 123.750445] __fput+0x70/0x234&lt;BR /&gt;[ 123.753503] ____fput+0x14/0x20&lt;BR /&gt;[ 123.756646] task_work_run+0x84/0x17c&lt;BR /&gt;[ 123.760310] do_notify_resume+0x208/0x12ec&lt;BR /&gt;[ 123.764410] el0_svc+0x6c/0x80&lt;BR /&gt;[ 123.767468] el0t_64_sync_handler+0xa8/0x130&lt;BR /&gt;[ 123.771740] el0t_64_sync+0x1a0/0x1a4&lt;BR /&gt;[ 166.793653] rcu: INFO: rcu_preempt detected expedited stalls on CPUs/tasks: { 3-... } 5581 jiffies s: 157 root: 0x8/.&lt;BR /&gt;[ 166.804366] rcu: blocking rcu_node structures (internal RCU debug):&lt;BR /&gt;[ 166.810666] Task dump for CPU 3:&lt;BR /&gt;[ 166.813912] task:vsidaemon state:R running task stack: 0 pid: 836 ppid: 2 flags:0x00000202&lt;BR /&gt;[ 166.823894] Call trace:&lt;BR /&gt;[ 166.826362] __switch_to+0x108/0x160&lt;BR /&gt;[ 166.829968] genpd_runtime_suspend+0x118/0x2c0&lt;BR /&gt;[ 166.834435] __rpm_callback+0x48/0x170&lt;BR /&gt;[ 166.838205] rpm_callback+0x6c/0x80&lt;BR /&gt;[ 166.841738] rpm_suspend+0x100/0x554&lt;BR /&gt;[ 166.845318] rpm_idle+0xf4/0x154&lt;BR /&gt;[ 166.848599] __pm_runtime_idle+0x60/0xb0&lt;BR /&gt;[ 166.852549] hantrodec_release+0x1c8/0x240&lt;BR /&gt;[ 166.856676] __fput+0x70/0x234&lt;BR /&gt;[ 166.859755] ____fput+0x14/0x20&lt;BR /&gt;[ 166.862917] task_work_run+0x84/0x17c&lt;BR /&gt;[ 166.866630] do_notify_resume+0x208/0x12ec&lt;BR /&gt;[ 166.870752] el0_svc+0x6c/0x80&lt;BR /&gt;[ 166.873828] el0t_64_sync_handler+0xa8/0x130&lt;BR /&gt;[ 166.878119] el0t_64_sync+0x1a0/0x1a4&lt;BR /&gt;[ 186.729335] rcu: INFO: rcu_preempt detected stalls on CPUs/tasks:&lt;BR /&gt;[ 186.735454] rcu: 3-...0: (0 ticks this GP) idle=0c1/1/0x4000000000000000 softirq=6730/6732 fqs=18090&lt;BR /&gt;[ 186.744772] (detected by 1, t=36794 jiffies, g=8953, q=36033)&lt;BR /&gt;[ 186.750608] Task dump for CPU 3:&lt;BR /&gt;[ 186.753835] task:vsidaemon state:R running task stack: 0 pid: 836 ppid: 2 flags:0x00000202&lt;BR /&gt;[ 186.763756] Call trace:&lt;BR /&gt;[ 186.766202] __switch_to+0x108/0x160&lt;BR /&gt;[ 186.769789] genpd_runtime_suspend+0x118/0x2c0&lt;BR /&gt;[ 186.774237] __rpm_callback+0x48/0x170&lt;BR /&gt;[ 186.777989] rpm_callback+0x6c/0x80&lt;BR /&gt;[ 186.781478] rpm_suspend+0x100/0x554&lt;BR /&gt;[ 186.785056] rpm_idle+0xf4/0x154&lt;BR /&gt;[ 186.788284] __pm_runtime_idle+0x60/0xb0&lt;BR /&gt;[ 186.792208] hantrodec_release+0x1c8/0x240&lt;BR /&gt;[ 186.796308] __fput+0x70/0x234&lt;BR /&gt;[ 186.799367] ____fput+0x14/0x20&lt;BR /&gt;[ 186.802510] task_work_run+0x84/0x17c&lt;BR /&gt;[ 186.806174] do_notify_resume+0x208/0x12ec&lt;BR /&gt;[ 186.810273] el0_svc+0x6c/0x80&lt;BR /&gt;[ 186.813330] el0t_64_sync_handler+0xa8/0x130&lt;BR /&gt;[ 186.817602] el0t_64_sync+0x1a0/0x1a4&lt;BR /&gt;[ 230.281056] rcu: INFO: rcu_preempt detected expedited stalls on CPUs/tasks: { 3-... } 21453 jiffies s: 157 root: 0x8/.&lt;BR /&gt;[ 230.291851] rcu: blocking rcu_node structures (internal RCU debug):&lt;BR /&gt;[ 230.298149] Task dump for CPU 3:&lt;BR /&gt;[ 230.301398] task:vsidaemon state:R running task stack: 0 pid: 836 ppid: 2 flags:0x00000202&lt;BR /&gt;[ 230.311338] Call trace:&lt;BR /&gt;[ 230.313830] __switch_to+0x108/0x160&lt;BR /&gt;[ 230.317447] genpd_runtime_suspend+0x118/0x2c0&lt;BR /&gt;[ 230.321916] __rpm_callback+0x48/0x170&lt;BR /&gt;[ 230.325688] rpm_callback+0x6c/0x80&lt;BR /&gt;[ 230.329195] rpm_suspend+0x100/0x554&lt;BR /&gt;[ 230.332776] rpm_idle+0xf4/0x154&lt;BR /&gt;[ 230.336022] __pm_runtime_idle+0x60/0xb0&lt;BR /&gt;[ 230.339992] hantrodec_release+0x1c8/0x240&lt;BR /&gt;[ 230.344122] __fput+0x70/0x234&lt;BR /&gt;[ 230.347203] ____fput+0x14/0x20&lt;BR /&gt;[ 230.350364] task_work_run+0x84/0x17c&lt;BR /&gt;[ 230.354048] do_notify_resume+0x208/0x12ec&lt;BR /&gt;[ 230.358167] el0_svc+0x6c/0x80&lt;BR /&gt;[ 230.361241] el0t_64_sync_handler+0xa8/0x130&lt;BR /&gt;[ 230.365560] el0t_64_sync+0x1a0/0x1a4&lt;/P&gt;&lt;P&gt;The logs are taken from serial console and has both gstramer and kernel logs.&lt;BR /&gt;System hangs and not usable after playback is complete.&lt;/P&gt;&lt;P&gt;Please confirm gstreamer is validated with video playback in the latest SDK.&lt;BR /&gt;I am playing the below video in Gstreamer:&lt;BR /&gt;&lt;A href="https://hq0epm0west0us0storage.blob.core.windows.net/development/Temp/sample_video.MOV" target="_blank"&gt;https://hq0epm0west0us0storage.blob.core.windows.net/development/Temp/sample_video.MOV&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;BR /&gt;Santhana Kumar&lt;/P&gt;</description>
      <pubDate>Sun, 29 Jan 2023 07:28:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8MP-VPU-hangs-after-playback/m-p/1589287#M200743</guid>
      <dc:creator>santhanakumar</dc:creator>
      <dc:date>2023-01-29T07:28:59Z</dc:date>
    </item>
    <item>
      <title>Re: iMX8MP: VPU hangs after playback</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8MP-VPU-hangs-after-playback/m-p/1589315#M200744</link>
      <description>&lt;P&gt;I have tested your sample video on i.mx8mp evk board successfully, pls compare your own code with nxp bsp to debug your own code&lt;/P&gt;</description>
      <pubDate>Sun, 29 Jan 2023 09:51:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8MP-VPU-hangs-after-playback/m-p/1589315#M200744</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2023-01-29T09:51:50Z</dc:date>
    </item>
    <item>
      <title>Re: iMX8MP: VPU hangs after playback</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8MP-VPU-hangs-after-playback/m-p/1591744#M200924</link>
      <description>&lt;P&gt;Hi Joanxie,&lt;/P&gt;&lt;P&gt;As I mentioned before, I am using EVK image to test VPU.&lt;BR /&gt;I am just appending our uboot on top of EVK image and this should replicate EVK behaviour in our board as well.&lt;/P&gt;&lt;P&gt;Could you please share the image that you used for testing VPU in EVK so that i can test here as well to understand the issue.&lt;/P&gt;&lt;P&gt;Also, we are using 4G memory compared to 6G memory used in EVK.&lt;BR /&gt;I find the below cma settings in evk dtb.&lt;/P&gt;&lt;P&gt;linux,cma {&lt;BR /&gt;compatible = "shared-dma-pool";&lt;BR /&gt;reusable;&lt;BR /&gt;size = &amp;lt;0 0x3c000000&amp;gt;;&lt;BR /&gt;alloc-ranges = &amp;lt;0 0x40000000 0 0xC0000000&amp;gt;;&lt;BR /&gt;linux,cma-default;&lt;BR /&gt;};&lt;/P&gt;&lt;P&gt;Do we need to modify CMA node in DTB for 4G memory size?&lt;BR /&gt;Please share your inputs.&lt;BR /&gt;Also please share the evk image used for testing VPU.&lt;/P&gt;&lt;P&gt;Regards,&lt;BR /&gt;Santhana Kumar&lt;/P&gt;</description>
      <pubDate>Wed, 01 Feb 2023 23:35:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8MP-VPU-hangs-after-playback/m-p/1591744#M200924</guid>
      <dc:creator>santhanakumar</dc:creator>
      <dc:date>2023-02-01T23:35:53Z</dc:date>
    </item>
    <item>
      <title>Re: iMX8MP: VPU hangs after playback</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8MP-VPU-hangs-after-playback/m-p/1592786#M200990</link>
      <description>&lt;P&gt;I just use 5.15 demo images from&lt;/P&gt;
&lt;P&gt;"&lt;A href="https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applications-processors:IMXLINUX&amp;quot;" target="_blank"&gt;https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applications-processors:IMXLINUX"&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;since you use new DDR, did you pass the stress test tool? and did you change the uboot according to your new DDR? pls try to pass stress test firsly&lt;/P&gt;
&lt;P&gt;"&lt;A href="https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX-8M-Family-DDR-Tool-Release/ta-p/1104467" target="_blank"&gt;https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX-8M-Family-DDR-Tool-Release/ta-p/1104467&lt;/A&gt;"&lt;/P&gt;</description>
      <pubDate>Fri, 03 Feb 2023 04:31:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8MP-VPU-hangs-after-playback/m-p/1592786#M200990</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2023-02-03T04:31:55Z</dc:date>
    </item>
    <item>
      <title>Re: iMX8MP: VPU hangs after playback</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8MP-VPU-hangs-after-playback/m-p/1620444#M203105</link>
      <description>&lt;P&gt;Hi Kumar,&lt;/P&gt;&lt;P&gt;Its looks like you have issues with Audio DSP. Try to play video without audio output (disable it).&lt;/P&gt;</description>
      <pubDate>Thu, 23 Mar 2023 04:00:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8MP-VPU-hangs-after-playback/m-p/1620444#M203105</guid>
      <dc:creator>artsiomstaliaro</dc:creator>
      <dc:date>2023-03-23T04:00:27Z</dc:date>
    </item>
    <item>
      <title>Re: iMX8MP: VPU hangs after playback</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8MP-VPU-hangs-after-playback/m-p/1620683#M203125</link>
      <description>&lt;P&gt;I could able to fix the issue myself.&lt;BR /&gt;Actually, the problem exists only in 4G memory version of our board and no issues are observed in 2G version.&lt;BR /&gt;I have removed power management routines from hantro decoder; playback now works fine.&lt;/P&gt;</description>
      <pubDate>Thu, 23 Mar 2023 08:42:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8MP-VPU-hangs-after-playback/m-p/1620683#M203125</guid>
      <dc:creator>santhanakumar</dc:creator>
      <dc:date>2023-03-23T08:42:20Z</dc:date>
    </item>
  </channel>
</rss>