<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Using a P&amp;amp;E Micro Universal Multilink probe on the  MIMXRT1010-EVK.</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Using-a-P-amp-E-Micro-Universal-Multilink-probe-on-the/m-p/1588489#M200668</link>
    <description>&lt;P&gt;To use the P&amp;amp;E Multilink on the MIMXRT1010-EVK.:&lt;/P&gt;&lt;P&gt;Connect the 10 pin cable from the probe&amp;nbsp; to connector&amp;nbsp; J55 - red side with pin1&lt;/P&gt;&lt;P&gt;Disconnect the USB connector from J42 and connect to J9, Move the Jump on J1 from 1-2 to 3-4.&lt;/P&gt;&lt;P&gt;SW8 OFF-OFF-ON-OFF ( this is the default)&lt;/P&gt;</description>
    <pubDate>Thu, 26 Jan 2023 18:55:35 GMT</pubDate>
    <dc:creator>JimDon</dc:creator>
    <dc:date>2023-01-26T18:55:35Z</dc:date>
    <item>
      <title>Using a P&amp;E Micro Universal Multilink probe on the  MIMXRT1010-EVK.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Using-a-P-amp-E-Micro-Universal-Multilink-probe-on-the/m-p/1588489#M200668</link>
      <description>&lt;P&gt;To use the P&amp;amp;E Multilink on the MIMXRT1010-EVK.:&lt;/P&gt;&lt;P&gt;Connect the 10 pin cable from the probe&amp;nbsp; to connector&amp;nbsp; J55 - red side with pin1&lt;/P&gt;&lt;P&gt;Disconnect the USB connector from J42 and connect to J9, Move the Jump on J1 from 1-2 to 3-4.&lt;/P&gt;&lt;P&gt;SW8 OFF-OFF-ON-OFF ( this is the default)&lt;/P&gt;</description>
      <pubDate>Thu, 26 Jan 2023 18:55:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Using-a-P-amp-E-Micro-Universal-Multilink-probe-on-the/m-p/1588489#M200668</guid>
      <dc:creator>JimDon</dc:creator>
      <dc:date>2023-01-26T18:55:35Z</dc:date>
    </item>
  </channel>
</rss>