<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックIMX8M Plus - Software update and Boot config</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX8M-Plus-Software-update-and-Boot-config/m-p/1588465#M200667</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;My carrier board for the IMX8MP will contain a memory device (eMMC) and USB3(USB1 ports)&lt;/P&gt;&lt;P&gt;The IMX8MP will be programmed only via USB and the program file will be save at eMMC (boot from eMMC).&lt;/P&gt;&lt;P&gt;Regarding the initial program:&lt;/P&gt;&lt;P&gt;- in which state the boot strap shall be for programming via USB and boot from the eMMC ?&lt;/P&gt;&lt;P&gt;- There is a way to reset the device (internally) for new boot after programming without using button for reset?&lt;/P&gt;&lt;P&gt;Regarding software:&lt;/P&gt;&lt;P&gt;- How can i make a software update (without the USB/JTAG ) ? the idea is to make an option for software update once the our costumer using the product via main FPGA (UART ? SPI ? )&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;thanks&lt;/P&gt;</description>
    <pubDate>Thu, 26 Jan 2023 18:12:45 GMT</pubDate>
    <dc:creator>YoavBenita</dc:creator>
    <dc:date>2023-01-26T18:12:45Z</dc:date>
    <item>
      <title>IMX8M Plus - Software update and Boot config</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8M-Plus-Software-update-and-Boot-config/m-p/1588465#M200667</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;My carrier board for the IMX8MP will contain a memory device (eMMC) and USB3(USB1 ports)&lt;/P&gt;&lt;P&gt;The IMX8MP will be programmed only via USB and the program file will be save at eMMC (boot from eMMC).&lt;/P&gt;&lt;P&gt;Regarding the initial program:&lt;/P&gt;&lt;P&gt;- in which state the boot strap shall be for programming via USB and boot from the eMMC ?&lt;/P&gt;&lt;P&gt;- There is a way to reset the device (internally) for new boot after programming without using button for reset?&lt;/P&gt;&lt;P&gt;Regarding software:&lt;/P&gt;&lt;P&gt;- How can i make a software update (without the USB/JTAG ) ? the idea is to make an option for software update once the our costumer using the product via main FPGA (UART ? SPI ? )&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;thanks&lt;/P&gt;</description>
      <pubDate>Thu, 26 Jan 2023 18:12:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8M-Plus-Software-update-and-Boot-config/m-p/1588465#M200667</guid>
      <dc:creator>YoavBenita</dc:creator>
      <dc:date>2023-01-26T18:12:45Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8M Plus - Software update and Boot config</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8M-Plus-Software-update-and-Boot-config/m-p/1589084#M200728</link>
      <description>&lt;P&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;If eMMC will be in a clean state, you may set it to boot from eMMC since the memory will be clean ROM code will jump to Serial download so you may flash trough USB.&lt;BR /&gt;&lt;BR /&gt;Yes, it may be possible to do so, like using an application for OTA updates like SWUpdate&lt;BR /&gt;&lt;A href="https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/SWUpdate-OTA-i-MX8MM-EVK-i-MX8QXP-MEK/ta-p/1307416" target="_blank"&gt;https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/SWUpdate-OTA-i-MX8MM-EVK-i-MX8QXP-MEK/ta-p/1307416&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;Well, the above is an option using network or from storage, but we do not support using UART or SPI as a medium to download software.&lt;BR /&gt;&lt;BR /&gt;Best regards,&lt;BR /&gt;Aldo.&lt;/P&gt;</description>
      <pubDate>Fri, 27 Jan 2023 21:17:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8M-Plus-Software-update-and-Boot-config/m-p/1589084#M200728</guid>
      <dc:creator>AldoG</dc:creator>
      <dc:date>2023-01-27T21:17:01Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8M Plus - Software update and Boot config</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8M-Plus-Software-update-and-Boot-config/m-p/1590024#M200802</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Which hardware peripheral are required to support the OTA ?&lt;/P&gt;&lt;P&gt;The only storage i have is the eMMC.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 30 Jan 2023 19:52:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8M-Plus-Software-update-and-Boot-config/m-p/1590024#M200802</guid>
      <dc:creator>YoavBenita</dc:creator>
      <dc:date>2023-01-30T19:52:41Z</dc:date>
    </item>
  </channel>
</rss>