<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic PRE_PERIPH MUX in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/PRE-PERIPH-MUX/m-p/241116#M20055</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; font-family: 'Arial','sans-serif';"&gt;Normally the DDR clock are sourced via PLL2 – PFD2 and this source passes the PRE_PERIPH mux. The question is how the sub CCM register CCM_CBCMR are naming this mux. The pre_periph2 seams [22:21] to correspond to PFD2 but the question if it or pre_periph [19:18] should be used instead or both??&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 03 Dec 2013 13:45:22 GMT</pubDate>
    <dc:creator>mrlantz</dc:creator>
    <dc:date>2013-12-03T13:45:22Z</dc:date>
    <item>
      <title>PRE_PERIPH MUX</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/PRE-PERIPH-MUX/m-p/241116#M20055</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; font-family: 'Arial','sans-serif';"&gt;Normally the DDR clock are sourced via PLL2 – PFD2 and this source passes the PRE_PERIPH mux. The question is how the sub CCM register CCM_CBCMR are naming this mux. The pre_periph2 seams [22:21] to correspond to PFD2 but the question if it or pre_periph [19:18] should be used instead or both??&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Dec 2013 13:45:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/PRE-PERIPH-MUX/m-p/241116#M20055</guid>
      <dc:creator>mrlantz</dc:creator>
      <dc:date>2013-12-03T13:45:22Z</dc:date>
    </item>
    <item>
      <title>Re: PRE_PERIPH MUX</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/PRE-PERIPH-MUX/m-p/241117#M20056</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Johan&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; The pre_periph2 in CCM_CBCMR[22:21] is to select clock source for periph2_clk, it is for mmdc_ch1_axi_clk_root, the pre_periph in CCM_CBCMR[19:18] is to select clock source for periph_clk, and mmdc_ch0_axi_clk_root is sourcing from periph_clk, you can refer to the clock tree in i.MX6Q RM Figure 18-5 in CCM chapter. These are two different clock mux for different clock path.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 04 Dec 2013 11:59:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/PRE-PERIPH-MUX/m-p/241117#M20056</guid>
      <dc:creator>AnsonHuang</dc:creator>
      <dc:date>2013-12-04T11:59:21Z</dc:date>
    </item>
  </channel>
</rss>