<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックFlex CAN Driver on iMX8QXP board with Android 12.1.0 OS</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Flex-CAN-Driver-on-iMX8QXP-board-with-Android-12-1-0-OS/m-p/1586657#M200526</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am using imx8qxp with Android 12.1.0 OS , I need use Flex CAN driver but not able to.&lt;/P&gt;&lt;P&gt;Could you please provide detail steps to run Flex CAN imx8qxp with Android 12.1.0 OS?&lt;/P&gt;&lt;P&gt;Thank you in advance for the help.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Prashant&amp;nbsp;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Mon, 23 Jan 2023 14:47:37 GMT</pubDate>
    <dc:creator>prashant_khengale</dc:creator>
    <dc:date>2023-01-23T14:47:37Z</dc:date>
    <item>
      <title>Flex CAN Driver on iMX8QXP board with Android 12.1.0 OS</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Flex-CAN-Driver-on-iMX8QXP-board-with-Android-12-1-0-OS/m-p/1586657#M200526</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am using imx8qxp with Android 12.1.0 OS , I need use Flex CAN driver but not able to.&lt;/P&gt;&lt;P&gt;Could you please provide detail steps to run Flex CAN imx8qxp with Android 12.1.0 OS?&lt;/P&gt;&lt;P&gt;Thank you in advance for the help.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Prashant&amp;nbsp;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 23 Jan 2023 14:47:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Flex-CAN-Driver-on-iMX8QXP-board-with-Android-12-1-0-OS/m-p/1586657#M200526</guid>
      <dc:creator>prashant_khengale</dc:creator>
      <dc:date>2023-01-23T14:47:37Z</dc:date>
    </item>
    <item>
      <title>Re: Flex CAN Driver on iMX8QXP board with Android 12.1.0 OS</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Flex-CAN-Driver-on-iMX8QXP-board-with-Android-12-1-0-OS/m-p/1587154#M200572</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;DIV id="bodyDisplay_4" class="lia-message-body lia-component-message-view-widget-body lia-component-body-signature-highlight-escalation lia-component-message-view-widget-body-signature-highlight-escalation"&gt;
&lt;DIV class="lia-message-body-content"&gt;
&lt;P&gt;Yes, FlexCAN is verified on latest BSP.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;The iMX8QXP defaul driver used CAN fd mode, so we used followed command to test it:&lt;/P&gt;
&lt;P&gt;Rx: ip link set can0 up type can bitrate 1000000 dbitrate 4000000 fd on&lt;/P&gt;
&lt;P&gt;Tx:&amp;nbsp;ip link set can1 up type can bitrate 1000000 dbitrate 4000000 fd on&lt;/P&gt;
&lt;P&gt;Rx: candump can0&lt;/P&gt;
&lt;P&gt;Tx: cangen can1 -m&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;If you want to use the&amp;nbsp;legacy mode iMX6/7 test&amp;nbsp;command such as "ip link set can0 up type can bitrate 1000000", you need disable the&amp;nbsp;fd mode in device tree by added "disable-fd-mode".&lt;/P&gt;
&lt;/DIV&gt;
&lt;/DIV&gt;
&lt;P&gt;The CAN test code can be found.&lt;/P&gt;
&lt;P&gt;MEK-MIMX8QX-SDK\boards\mekmimx8qx\driver_examples\flexcan&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 24 Jan 2023 14:17:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Flex-CAN-Driver-on-iMX8QXP-board-with-Android-12-1-0-OS/m-p/1587154#M200572</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2023-01-24T14:17:52Z</dc:date>
    </item>
    <item>
      <title>Re: Flex CAN Driver on iMX8QXP board with Android 12.1.0 OS</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Flex-CAN-Driver-on-iMX8QXP-board-with-Android-12-1-0-OS/m-p/1587610#M200606</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Thank you for your reply.&lt;/P&gt;&lt;P&gt;we are not able to found path :&amp;nbsp;&lt;SPAN&gt;MEK-MIMX8QX-SDK\boards\mekmimx8qx\driver_examples\flexcan&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;could you please know us where we can find this path? give detail path.&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Prashant&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 25 Jan 2023 11:54:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Flex-CAN-Driver-on-iMX8QXP-board-with-Android-12-1-0-OS/m-p/1587610#M200606</guid>
      <dc:creator>prashant_khengale</dc:creator>
      <dc:date>2023-01-25T11:54:41Z</dc:date>
    </item>
  </channel>
</rss>