<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: imx6ull Custom Board</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx6ull-Custom-Board/m-p/1586087#M200454</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;You have to adapt the driver and its programming to your pcb, check your device tree the locations of all modules.&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
    <pubDate>Fri, 20 Jan 2023 15:02:23 GMT</pubDate>
    <dc:creator>Bio_TICFSL</dc:creator>
    <dc:date>2023-01-20T15:02:23Z</dc:date>
    <item>
      <title>imx6ull Custom Board</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6ull-Custom-Board/m-p/1585318#M200385</link>
      <description>&lt;P&gt;Hi NXP,&lt;/P&gt;&lt;P&gt;I have the okimx6ull-s system on module.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.forlinx.net/product/i.mx6ull-system-on-module-106.html" target="_blank"&gt;https://www.forlinx.net/product/i.mx6ull-system-on-module-106.html&lt;/A&gt;&lt;/P&gt;&lt;P&gt;I'm trying to program emmc but I'm getting an error:&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;                                                                              
U-Boot 2022.04-lf_v2022.04+g16e8414193 (Oct 08 2022 - 13:33:43 +0000)           
                                                                                
CPU:   i.MX6ULL rev1.1 792 MHz (running at 396 MHz)                             
CPU:   Industrial temperature grade (-40C to 105C) at 42C                       
Reset cause: POR                                                                
Model: i.MX6 ULL 14x14 EVK Board                                                
Board: MX6ULL 14x14 EVK                                                         
DRAM:  512 MiB                                                                  
Core:  65 devices, 18 uclasses, devicetree: separate                            
MMC:   FSL_SDHC: 0, FSL_SDHC: 1                                                 
Loading Environment from MMC... *** Warning - bad CRC, using default environment
                                                                                
[*]-Video Link 0 (480 x 272)                                                    
        [0] lcdif@21c8000, video                                                
In:    serial                                                                   
Out:   serial                                                                   
Err:   serial                                                                   
switch to partitions #0, OK                                                     
mmc1(part 0) is current device                                                  
flash target is MMC:1                                                           
Net:   Could not get PHY for FEC1: addr 1                                       
Could not get PHY for FEC1: addr 1                                              
Get shared mii bus on ethernet@2188000       &lt;/LI-CODE&gt;&lt;P&gt;Works in original software :&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;MMC:   FSL_SDHC: 0, FSL_SDHC: 1                               
Display: TFT70AB-1024x600                                                       
Video: 1024x600x24                                                              
Card did not respond to voltage select!                                         
reading logo.bmp                                                                
391736 bytes read in 24 ms (15.6 MiB/s)                                         
In:    serial                                                                   
Out:   serial                                                                   
Err:   serial                                                                   
Time-out: 128s                                                                  
switch to partitions #0, OK                                                     
mmc1(part 0) is current device                                                  
Saving Environment to MMC...                                                    
Writing to MMC(1)... done                                                       
Saving Environment to MMC...                                                    
Writing to MMC(1)... done                                                       
                                                                                
Warning: MAC address is generated using cpuid                                   
Net:   Board Net Initialization Failed                                          
No ethernet found.                                                              
Normal Boot                                                                     
Press SPACE to abort autoboot in 1 seconds                                      
reading boot.scr                      &lt;/LI-CODE&gt;&lt;P&gt;my yocto project file:&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;        $ mkdir imx-yocto-bsp
	$ cd imx-yocto-bsp
	$ repo init -u https://github.com/nxp-imx/imx-manifest -b imx-linux-kirkstone -m imx-5.15.52-2.1.0.xml
	$ repo sync
	$ DISTRO=fsl-imx-wayland MACHINE=imx6ull14x14evk source imx-setup-release.sh -b build
	$ bitbake imx-image-core&lt;/LI-CODE&gt;&lt;P&gt;How do I create my own yocto project for my custom card?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 19 Jan 2023 09:44:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6ull-Custom-Board/m-p/1585318#M200385</guid>
      <dc:creator>ylmzhsn_</dc:creator>
      <dc:date>2023-01-19T09:44:25Z</dc:date>
    </item>
    <item>
      <title>Re: imx6ull Custom Board</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6ull-Custom-Board/m-p/1586087#M200454</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;You have to adapt the driver and its programming to your pcb, check your device tree the locations of all modules.&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Fri, 20 Jan 2023 15:02:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6ull-Custom-Board/m-p/1586087#M200454</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2023-01-20T15:02:23Z</dc:date>
    </item>
  </channel>
</rss>