<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: QDC INDEX Interrupt</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/QDC-INDEX-Interrupt/m-p/1584763#M200351</link>
    <description>&lt;P&gt;My mistake. I am using MIMXRT1166DVM6A&lt;/P&gt;</description>
    <pubDate>Wed, 18 Jan 2023 16:17:15 GMT</pubDate>
    <dc:creator>twjudge</dc:creator>
    <dc:date>2023-01-18T16:17:15Z</dc:date>
    <item>
      <title>QDC INDEX Interrupt</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/QDC-INDEX-Interrupt/m-p/1584230#M200280</link>
      <description>&lt;P&gt;I am using the INDEX signal on an external quadrature encoder to generate an interrupt. I have this working in general however I would like to be able to select whether the interrupt occurs on the rising edge or the following edge of the INDEX signal.&lt;/P&gt;&lt;P&gt;I see this option on the CTRL-&amp;gt;XNE control bit however this is for determining which edge of INDEX resets the position counter. I would like to generate the interrupt on the falling/rising edge of INDEX without resetting the position counter. Is this possible?&lt;/P&gt;</description>
      <pubDate>Wed, 18 Jan 2023 00:11:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/QDC-INDEX-Interrupt/m-p/1584230#M200280</guid>
      <dc:creator>twjudge</dc:creator>
      <dc:date>2023-01-18T00:11:31Z</dc:date>
    </item>
    <item>
      <title>Re: QDC INDEX Interrupt</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/QDC-INDEX-Interrupt/m-p/1584266#M200282</link>
      <description>&lt;P&gt;Which MPU/MCU are you using?&lt;/P&gt;</description>
      <pubDate>Wed, 18 Jan 2023 02:05:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/QDC-INDEX-Interrupt/m-p/1584266#M200282</guid>
      <dc:creator>jimmychan</dc:creator>
      <dc:date>2023-01-18T02:05:18Z</dc:date>
    </item>
    <item>
      <title>Re: QDC INDEX Interrupt</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/QDC-INDEX-Interrupt/m-p/1584763#M200351</link>
      <description>&lt;P&gt;My mistake. I am using MIMXRT1166DVM6A&lt;/P&gt;</description>
      <pubDate>Wed, 18 Jan 2023 16:17:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/QDC-INDEX-Interrupt/m-p/1584763#M200351</guid>
      <dc:creator>twjudge</dc:creator>
      <dc:date>2023-01-18T16:17:15Z</dc:date>
    </item>
    <item>
      <title>Re: QDC INDEX Interrupt</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/QDC-INDEX-Interrupt/m-p/1590837#M200868</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Thank you so much for your interest in our products and for using our community.&lt;/P&gt;
&lt;P&gt;Based on the Control Register (CTRL), I understand that it is possible to generate the interrupt without the INDEX pulse initializes the position counter.&lt;/P&gt;
&lt;P&gt;For this you must configure XIE-&amp;gt;1, XIP-&amp;gt;0, and XNE depending on your choice. With that the INDEX interrupt occurs when XIRQ is set.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="nxf86756_0-1675205297723.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/209027i206C2FFAB4CCD048/image-size/medium?v=v2&amp;amp;px=400" role="button" title="nxf86756_0-1675205297723.png" alt="nxf86756_0-1675205297723.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;nxf86756_0-1675205297723.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Hope it helps you. Please let me know if you have more questions about it.&lt;/P&gt;
&lt;P&gt;Have a nice day!&lt;/P&gt;</description>
      <pubDate>Tue, 31 Jan 2023 22:50:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/QDC-INDEX-Interrupt/m-p/1590837#M200868</guid>
      <dc:creator>_Leo_</dc:creator>
      <dc:date>2023-01-31T22:50:04Z</dc:date>
    </item>
  </channel>
</rss>