<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processorsのトピック回复： XEN Hypervisor DomU Set IP Address</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/XEN-Hypervisor-DomU-Set-IP-Address/m-p/1584551#M200319</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I assigned the ip to DomU using tmux from the terminal of Domain-0 and this is how I solved the problem.&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Efecan&lt;/P&gt;</description>
    <pubDate>Wed, 18 Jan 2023 10:55:41 GMT</pubDate>
    <dc:creator>cbl</dc:creator>
    <dc:date>2023-01-18T10:55:41Z</dc:date>
    <item>
      <title>XEN Hypervisor DomU Set IP Address</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/XEN-Hypervisor-DomU-Set-IP-Address/m-p/1583998#M200254</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am running Yocto image and Android Automotive OS on XEN hypervisor.&lt;/P&gt;&lt;P&gt;Domain-0 Yocto image. DomU is Android Automotive OS.&lt;/P&gt;&lt;P&gt;After creating DomU I want to give IP to DomU. However, I want to run "xl console DomU" command and do it via Domain-0, not from Android Terminal.&lt;/P&gt;&lt;P&gt;But I don't know how to do it. Can you help with this?&lt;/P&gt;&lt;P&gt;What linux command or what XEN configuration do I need to set the IP of DomU@ from Domain-0?&lt;/P&gt;&lt;P&gt;Best regards,&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 17 Jan 2023 13:53:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/XEN-Hypervisor-DomU-Set-IP-Address/m-p/1583998#M200254</guid>
      <dc:creator>cbl</dc:creator>
      <dc:date>2023-01-17T13:53:59Z</dc:date>
    </item>
    <item>
      <title>回复： XEN Hypervisor DomU Set IP Address</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/XEN-Hypervisor-DomU-Set-IP-Address/m-p/1584551#M200319</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I assigned the ip to DomU using tmux from the terminal of Domain-0 and this is how I solved the problem.&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Efecan&lt;/P&gt;</description>
      <pubDate>Wed, 18 Jan 2023 10:55:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/XEN-Hypervisor-DomU-Set-IP-Address/m-p/1584551#M200319</guid>
      <dc:creator>cbl</dc:creator>
      <dc:date>2023-01-18T10:55:41Z</dc:date>
    </item>
    <item>
      <title>回复： XEN Hypervisor DomU Set IP Address</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/XEN-Hypervisor-DomU-Set-IP-Address/m-p/1584686#M200340</link>
      <description>&lt;P&gt;Good!&lt;/P&gt;</description>
      <pubDate>Wed, 18 Jan 2023 14:28:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/XEN-Hypervisor-DomU-Set-IP-Address/m-p/1584686#M200340</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2023-01-18T14:28:49Z</dc:date>
    </item>
  </channel>
</rss>