<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Device Tree for i.MX8M Plus LPDDR4 EVK in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Device-Tree-for-i-MX8M-Plus-LPDDR4-EVK/m-p/1584501#M200309</link>
    <description>&lt;P&gt;For the i.MX8M Plus LPDDR4 EVK will only using &lt;STRONG&gt;imx8mp-evk.dts&lt;/STRONG&gt; ONLY or &lt;STRONG&gt;imx8mp-evk.dts + below .dts&lt;/STRONG&gt; files ?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;U&gt;&lt;STRONG&gt;imx8mp-lpddr4-evk.conf&lt;/STRONG&gt;&lt;/U&gt;&lt;/P&gt;&lt;P&gt;KERNEL_DEVICETREE:append:use-nxp-bsp = " \&lt;BR /&gt;freescale/imx8mp-ab2.dtb \&lt;BR /&gt;freescale/imx8mp-evk-basler.dtb \&lt;BR /&gt;freescale/imx8mp-evk-basler-ov2775.dtb \&lt;BR /&gt;freescale/imx8mp-evk-basler-ov5640.dtb \&lt;BR /&gt;freescale/imx8mp-evk-dual-basler.dtb \&lt;BR /&gt;freescale/imx8mp-evk-dual-ov2775.dtb \&lt;BR /&gt;freescale/imx8mp-evk-ecspi-slave.dtb \&lt;BR /&gt;freescale/imx8mp-evk-flexcan2.dtb \&lt;BR /&gt;freescale/imx8mp-evk-hifiberry-dacplus.dtb \&lt;BR /&gt;freescale/imx8mp-evk-inmate.dtb \&lt;BR /&gt;freescale/imx8mp-evk-iqaudio-dacplus.dtb \&lt;BR /&gt;freescale/imx8mp-evk-iqaudio-dacpro.dtb \&lt;BR /&gt;freescale/imx8mp-evk-it6263-lvds-dual-channel.dtb \&lt;BR /&gt;freescale/imx8mp-evk-jdi-wuxga-lvds-panel.dtb \&lt;BR /&gt;freescale/imx8mp-evk-ndm.dtb \&lt;BR /&gt;freescale/imx8mp-evk-ov2775.dtb \&lt;BR /&gt;freescale/imx8mp-evk-ov2775-ov5640.dtb \&lt;BR /&gt;freescale/imx8mp-evk-pcie-ep.dtb \&lt;BR /&gt;freescale/imx8mp-evk-rm67191.dtb \&lt;BR /&gt;freescale/imx8mp-evk-rm67199.dtb \&lt;BR /&gt;freescale/imx8mp-evk-root.dtb \&lt;BR /&gt;freescale/imx8mp-evk-rpmsg.dtb \&lt;BR /&gt;freescale/imx8mp-evk-sof-wm8960.dtb \&lt;BR /&gt;freescale/imx8mp-evk-spdif-lb.dtb \&lt;BR /&gt;freescale/imx8mp-evk-usdhc1-m2.dtb \&lt;BR /&gt;"&lt;/P&gt;</description>
    <pubDate>Wed, 18 Jan 2023 09:28:54 GMT</pubDate>
    <dc:creator>Jimmychea</dc:creator>
    <dc:date>2023-01-18T09:28:54Z</dc:date>
    <item>
      <title>Device Tree for i.MX8M Plus LPDDR4 EVK</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Device-Tree-for-i-MX8M-Plus-LPDDR4-EVK/m-p/1584501#M200309</link>
      <description>&lt;P&gt;For the i.MX8M Plus LPDDR4 EVK will only using &lt;STRONG&gt;imx8mp-evk.dts&lt;/STRONG&gt; ONLY or &lt;STRONG&gt;imx8mp-evk.dts + below .dts&lt;/STRONG&gt; files ?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;U&gt;&lt;STRONG&gt;imx8mp-lpddr4-evk.conf&lt;/STRONG&gt;&lt;/U&gt;&lt;/P&gt;&lt;P&gt;KERNEL_DEVICETREE:append:use-nxp-bsp = " \&lt;BR /&gt;freescale/imx8mp-ab2.dtb \&lt;BR /&gt;freescale/imx8mp-evk-basler.dtb \&lt;BR /&gt;freescale/imx8mp-evk-basler-ov2775.dtb \&lt;BR /&gt;freescale/imx8mp-evk-basler-ov5640.dtb \&lt;BR /&gt;freescale/imx8mp-evk-dual-basler.dtb \&lt;BR /&gt;freescale/imx8mp-evk-dual-ov2775.dtb \&lt;BR /&gt;freescale/imx8mp-evk-ecspi-slave.dtb \&lt;BR /&gt;freescale/imx8mp-evk-flexcan2.dtb \&lt;BR /&gt;freescale/imx8mp-evk-hifiberry-dacplus.dtb \&lt;BR /&gt;freescale/imx8mp-evk-inmate.dtb \&lt;BR /&gt;freescale/imx8mp-evk-iqaudio-dacplus.dtb \&lt;BR /&gt;freescale/imx8mp-evk-iqaudio-dacpro.dtb \&lt;BR /&gt;freescale/imx8mp-evk-it6263-lvds-dual-channel.dtb \&lt;BR /&gt;freescale/imx8mp-evk-jdi-wuxga-lvds-panel.dtb \&lt;BR /&gt;freescale/imx8mp-evk-ndm.dtb \&lt;BR /&gt;freescale/imx8mp-evk-ov2775.dtb \&lt;BR /&gt;freescale/imx8mp-evk-ov2775-ov5640.dtb \&lt;BR /&gt;freescale/imx8mp-evk-pcie-ep.dtb \&lt;BR /&gt;freescale/imx8mp-evk-rm67191.dtb \&lt;BR /&gt;freescale/imx8mp-evk-rm67199.dtb \&lt;BR /&gt;freescale/imx8mp-evk-root.dtb \&lt;BR /&gt;freescale/imx8mp-evk-rpmsg.dtb \&lt;BR /&gt;freescale/imx8mp-evk-sof-wm8960.dtb \&lt;BR /&gt;freescale/imx8mp-evk-spdif-lb.dtb \&lt;BR /&gt;freescale/imx8mp-evk-usdhc1-m2.dtb \&lt;BR /&gt;"&lt;/P&gt;</description>
      <pubDate>Wed, 18 Jan 2023 09:28:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Device-Tree-for-i-MX8M-Plus-LPDDR4-EVK/m-p/1584501#M200309</guid>
      <dc:creator>Jimmychea</dc:creator>
      <dc:date>2023-01-18T09:28:54Z</dc:date>
    </item>
    <item>
      <title>Re: Device Tree for i.MX8M Plus LPDDR4 EVK</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Device-Tree-for-i-MX8M-Plus-LPDDR4-EVK/m-p/1584646#M200331</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/208450"&gt;@Jimmychea&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;I hope you are doing well.&lt;/P&gt;
&lt;P&gt;The device tree file can be determined by a u-boot environment variable &lt;STRONG&gt;fdtfile&lt;/STRONG&gt;.&lt;BR /&gt;&lt;STRONG&gt;imx8mp-evk.dts&lt;/STRONG&gt; is the base device tree file for i.MX8MP EVK,&lt;/P&gt;
&lt;P&gt;For Example:&lt;/P&gt;
&lt;PRE&gt;&lt;STRONG&gt;setenv fdtfile "imx8mp-evk.dtb"&lt;/STRONG&gt;&lt;/PRE&gt;
&lt;P&gt;Other device tree files are used for specific use cases and they use imx8mp-evk.dts as a base.&lt;/P&gt;
&lt;P&gt;For example, &lt;STRONG&gt;imx8mp-evk-basler-ov5640.dtb&lt;/STRONG&gt; can be set as fdtfile in u-boot cmd if the &lt;STRONG&gt;basler camera&lt;/STRONG&gt; is used&lt;BR /&gt;imx8mp-evk-basler-ov5640.dts contains &lt;STRONG&gt;#include "imx8mp-evk.dts".&lt;/STRONG&gt;&lt;/P&gt;
&lt;P&gt;The same goes for other device tree files.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Thanks &amp;amp; Regards,&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Dhruvit Vasavada&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 18 Jan 2023 13:23:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Device-Tree-for-i-MX8M-Plus-LPDDR4-EVK/m-p/1584646#M200331</guid>
      <dc:creator>Dhruvit</dc:creator>
      <dc:date>2023-01-18T13:23:38Z</dc:date>
    </item>
  </channel>
</rss>