<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic IMXRT1176 PWM Frequency Modulation in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMXRT1176-PWM-Frequency-Modulation/m-p/1584205#M200276</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm working with the IMXRT1176 and would like to implement frequency modulation with the pwm driver. I've had a look at the SDK example and it seems the driver is written with the intention of setting up the frequency on initialization and the performing duty cycle modulation after that. Is it possible to implement frequency modulation with this peripheral?&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
    <pubDate>Tue, 17 Jan 2023 22:21:39 GMT</pubDate>
    <dc:creator>rnicolls</dc:creator>
    <dc:date>2023-01-17T22:21:39Z</dc:date>
    <item>
      <title>IMXRT1176 PWM Frequency Modulation</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMXRT1176-PWM-Frequency-Modulation/m-p/1584205#M200276</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm working with the IMXRT1176 and would like to implement frequency modulation with the pwm driver. I've had a look at the SDK example and it seems the driver is written with the intention of setting up the frequency on initialization and the performing duty cycle modulation after that. Is it possible to implement frequency modulation with this peripheral?&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
      <pubDate>Tue, 17 Jan 2023 22:21:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMXRT1176-PWM-Frequency-Modulation/m-p/1584205#M200276</guid>
      <dc:creator>rnicolls</dc:creator>
      <dc:date>2023-01-17T22:21:39Z</dc:date>
    </item>
    <item>
      <title>Re: IMXRT1176 PWM Frequency Modulation</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMXRT1176-PWM-Frequency-Modulation/m-p/1587359#M200582</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Thank you so much for your interest in our products and for using our community.&lt;/P&gt;
&lt;P&gt;The driver for the PWM only allows updating the PWM signal duty cycle of a particular PWM channel. And I can't find documentation about PFM with this driver, you would be the first person to do it with the eFlexPWM module. If you succeed, I appreciate your comments about it.&lt;/P&gt;
&lt;P&gt;However, the application note &lt;A href="https://www.nxp.com/docs/en/application-note/AN12713.pdf" target="_blank" rel="noopener"&gt;AN12713&lt;/A&gt; &lt;EM&gt;Generating PWM and PFM by Using FlexIO&lt;/EM&gt; illustrates how to do what you are looking for but with the FlexIO module and even comes with its respective associated file &lt;A href="https://www.nxp.com/docs/en/application-note-software/AN12713SW.zip" target="_blank" rel="noopener"&gt;AN12713SW&lt;/A&gt;. It is based on the i.MX RT1010 EVK board but it can easily enable on other i.MX RT Series EVK board.&lt;/P&gt;
&lt;P&gt;Hope it helps you.&lt;/P&gt;
&lt;P&gt;Have a nice day!&lt;/P&gt;</description>
      <pubDate>Tue, 24 Jan 2023 22:15:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMXRT1176-PWM-Frequency-Modulation/m-p/1587359#M200582</guid>
      <dc:creator>_Leo_</dc:creator>
      <dc:date>2023-01-24T22:15:35Z</dc:date>
    </item>
    <item>
      <title>Re: IMXRT1176 PWM Frequency Modulation</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMXRT1176-PWM-Frequency-Modulation/m-p/1588550#M200675</link>
      <description>&lt;P&gt;Hello, it's me, again,&lt;/P&gt;
&lt;P&gt;Perhaps application note &lt;A href="https://www.nxp.com/webapp/Download?colCode=AN12873&amp;amp;location=null" target="_blank" rel="noopener"&gt;AN12873&lt;/A&gt; &lt;EM&gt;Valid update of PWM signals for eFlexPWM&lt;/EM&gt; module will be useful to you. However, it does not come with associated software.&lt;/P&gt;</description>
      <pubDate>Thu, 26 Jan 2023 21:09:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMXRT1176-PWM-Frequency-Modulation/m-p/1588550#M200675</guid>
      <dc:creator>_Leo_</dc:creator>
      <dc:date>2023-01-26T21:09:08Z</dc:date>
    </item>
    <item>
      <title>Re: IMXRT1176 PWM Frequency Modulation</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMXRT1176-PWM-Frequency-Modulation/m-p/1588553#M200676</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Thank you for the reply.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I was able to modulate the frequency by running the PWM edge aligned and then updating the VAL registers with calculated period length and pulse width. To increase resolution, depending on the range, the clock prescaler could be updated. Seeing as the registered were buffered, I didn't encounter any issues when updating them.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;Rory&lt;/P&gt;</description>
      <pubDate>Thu, 26 Jan 2023 21:19:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMXRT1176-PWM-Frequency-Modulation/m-p/1588553#M200676</guid>
      <dc:creator>rnicolls</dc:creator>
      <dc:date>2023-01-26T21:19:17Z</dc:date>
    </item>
  </channel>
</rss>