<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Which python version should be used as &amp;quot;python&amp;quot; command?</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Which-python-version-should-be-used-as-quot-python-quot-command/m-p/1583243#M200184</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;Any version sonce 3.x and up can be use by yocto.&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
    <pubDate>Mon, 16 Jan 2023 14:25:49 GMT</pubDate>
    <dc:creator>Bio_TICFSL</dc:creator>
    <dc:date>2023-01-16T14:25:49Z</dc:date>
    <item>
      <title>Which python version should be used as "python" command?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Which-python-version-should-be-used-as-quot-python-quot-command/m-p/1582782#M200127</link>
      <description>&lt;P&gt;It seems from Ubuntu 20.04, t&lt;SPAN&gt;he default "python" command is deliberately undefined. Actually, all official Ubuntu packages depend explicitly on "python2" or "python3". The&amp;nbsp;IMXLXYOCTOUG recommend Ubuntu versions &amp;gt;= 20.04. But still ask the user to install 'python' package. Then which version should I use as 'python' command when compiling the Yocto project, 2 or 3?&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Thanks.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Sun, 15 Jan 2023 14:12:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Which-python-version-should-be-used-as-quot-python-quot-command/m-p/1582782#M200127</guid>
      <dc:creator>diverger</dc:creator>
      <dc:date>2023-01-15T14:12:30Z</dc:date>
    </item>
    <item>
      <title>Re: Which python version should be used as "python" command?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Which-python-version-should-be-used-as-quot-python-quot-command/m-p/1583202#M200181</link>
      <description>&lt;P&gt;If you are referring to the python &lt;STRONG&gt;host&lt;/STRONG&gt; verison , you can retrieve the infos that you need on the yocto project documentation.&lt;/P&gt;&lt;P&gt;Example&lt;/P&gt;&lt;P&gt;&lt;A href="https://docs.yoctoproject.org/migration-guides/migration-3.1.html" target="_blank"&gt;https://docs.yoctoproject.org/migration-guides/migration-3.1.html&lt;/A&gt;&lt;/P&gt;&lt;P&gt;That's for migrating to the dunfell branch from a previous one , you can see from the screenshot i've taken that python 3.5 is in the requirements .&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="L30_0-1673874626280.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/207469i2520DEA828C8FD80/image-size/medium?v=v2&amp;amp;px=400" role="button" title="L30_0-1673874626280.png" alt="L30_0-1673874626280.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;L30_0-1673874626280.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Hope this will help you &lt;LI-EMOJI id="lia_slightly-smiling-face" title=":slightly_smiling_face:"&gt;&lt;/LI-EMOJI&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 16 Jan 2023 13:12:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Which-python-version-should-be-used-as-quot-python-quot-command/m-p/1583202#M200181</guid>
      <dc:creator>L30</dc:creator>
      <dc:date>2023-01-16T13:12:52Z</dc:date>
    </item>
    <item>
      <title>Re: Which python version should be used as "python" command?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Which-python-version-should-be-used-as-quot-python-quot-command/m-p/1583243#M200184</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;Any version sonce 3.x and up can be use by yocto.&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Mon, 16 Jan 2023 14:25:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Which-python-version-should-be-used-as-quot-python-quot-command/m-p/1583243#M200184</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2023-01-16T14:25:49Z</dc:date>
    </item>
  </channel>
</rss>