<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックLPUART FreeRTOS DRIVER</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/LPUART-FreeRTOS-DRIVER/m-p/1582253#M200062</link>
    <description>&lt;P&gt;I am using IMXRT1062 processor looking for FreeRTOS LPUART driver which can support 9bit and 10bit UART. I followed Resource Manual and got info that I need to manipulate CTRL registers to enable, but my concern is how the data will be handled since the whole FreeRTOS_Lpuart driver is using uint8_t buffer, same goes with ring buffer.&lt;BR /&gt;&lt;BR /&gt;How to proceed now?&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Fri, 13 Jan 2023 07:28:53 GMT</pubDate>
    <dc:creator>pp99</dc:creator>
    <dc:date>2023-01-13T07:28:53Z</dc:date>
    <item>
      <title>LPUART FreeRTOS DRIVER</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/LPUART-FreeRTOS-DRIVER/m-p/1582253#M200062</link>
      <description>&lt;P&gt;I am using IMXRT1062 processor looking for FreeRTOS LPUART driver which can support 9bit and 10bit UART. I followed Resource Manual and got info that I need to manipulate CTRL registers to enable, but my concern is how the data will be handled since the whole FreeRTOS_Lpuart driver is using uint8_t buffer, same goes with ring buffer.&lt;BR /&gt;&lt;BR /&gt;How to proceed now?&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 13 Jan 2023 07:28:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/LPUART-FreeRTOS-DRIVER/m-p/1582253#M200062</guid>
      <dc:creator>pp99</dc:creator>
      <dc:date>2023-01-13T07:28:53Z</dc:date>
    </item>
    <item>
      <title>Re: LPUART FreeRTOS DRIVER</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/LPUART-FreeRTOS-DRIVER/m-p/1584220#M200278</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/211187"&gt;@pp99&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;I'm afraid we don't have any example codes or pre-designed drivers that use 9 or 10bit UART by default. This would have to be changed manually on the provided drivers in order to work. Sorry for the inconvenience.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR,&lt;/P&gt;
&lt;P&gt;Edwin.&lt;/P&gt;</description>
      <pubDate>Tue, 17 Jan 2023 23:55:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/LPUART-FreeRTOS-DRIVER/m-p/1584220#M200278</guid>
      <dc:creator>EdwinHz</dc:creator>
      <dc:date>2023-01-17T23:55:14Z</dc:date>
    </item>
  </channel>
</rss>