<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: Config Tools for i.MX 12.1: Ubuntu cannot locat python</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Config-Tools-for-i-MX-12-1-Ubuntu-cannot-locat-python/m-p/1581191#M199955</link>
    <description>If I ignore the message and try to run the tests It fails with the following message:&lt;BR /&gt;&lt;BR /&gt;/opt/nxp/i.MX_CFG_v12.1/bin/python38/bin/python: Error while finding module specification for 'memtool.s' (ModuleNotFoundError: No module named 'memtool')</description>
    <pubDate>Wed, 11 Jan 2023 22:31:02 GMT</pubDate>
    <dc:creator>don_gunn</dc:creator>
    <dc:date>2023-01-11T22:31:02Z</dc:date>
    <item>
      <title>Config Tools for i.MX 12.1: Ubuntu cannot locat python</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Config-Tools-for-i-MX-12-1-Ubuntu-cannot-locat-python/m-p/1571874#M198938</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am using config tools for i.MX ubuntu version 12.1&amp;nbsp; to calculate RAM timings. I figured out that after creating a new project code preview does not work because python couldn't be found. swtool.log shows that one of following errors "Python path does not exist: /opt/nxp/i.MX_CFG_v12.1/bin/python39" because after installation only "/opt/nxp/i.MX_CFG_v12.1/bin/python38" is available and python version is 3.10.0a2+.&lt;/P&gt;&lt;P&gt;Would you please correct this. Thank you.&lt;/P&gt;&lt;P&gt;Whish you Merry Christmas.&lt;/P&gt;</description>
      <pubDate>Mon, 19 Dec 2022 10:31:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Config-Tools-for-i-MX-12-1-Ubuntu-cannot-locat-python/m-p/1571874#M198938</guid>
      <dc:creator>ad-fsdev</dc:creator>
      <dc:date>2022-12-19T10:31:45Z</dc:date>
    </item>
    <item>
      <title>Re: Config Tools for i.MX 12.1: Ubuntu cannot locat python</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Config-Tools-for-i-MX-12-1-Ubuntu-cannot-locat-python/m-p/1578712#M199702</link>
      <description>&lt;P&gt;I have the same issue.&amp;nbsp; Any update on this?&lt;/P&gt;</description>
      <pubDate>Fri, 06 Jan 2023 20:39:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Config-Tools-for-i-MX-12-1-Ubuntu-cannot-locat-python/m-p/1578712#M199702</guid>
      <dc:creator>don_gunn</dc:creator>
      <dc:date>2023-01-06T20:39:43Z</dc:date>
    </item>
    <item>
      <title>Re: Config Tools for i.MX 12.1: Ubuntu cannot locat python</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Config-Tools-for-i-MX-12-1-Ubuntu-cannot-locat-python/m-p/1579898#M199824</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;you can set your own path in the tool.ini to -Dpython.dir=python39 (/opt/nxp/i.MX_CFG_v12.1/bin) and it should work too. But the failure (maybe copy paste) is available from my understanding.&lt;/P&gt;&lt;P&gt;Happy new year.&lt;/P&gt;</description>
      <pubDate>Tue, 10 Jan 2023 08:54:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Config-Tools-for-i-MX-12-1-Ubuntu-cannot-locat-python/m-p/1579898#M199824</guid>
      <dc:creator>ad-fsdev</dc:creator>
      <dc:date>2023-01-10T08:54:20Z</dc:date>
    </item>
    <item>
      <title>Re: Config Tools for i.MX 12.1: Ubuntu cannot locat python</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Config-Tools-for-i-MX-12-1-Ubuntu-cannot-locat-python/m-p/1581189#M199954</link>
      <description>&lt;P&gt;Thank you, I was able to fix the tools.ini file.&lt;/P&gt;&lt;P&gt;The folder that comes with the install package is called python38 but the ini file is set to python39.&lt;/P&gt;&lt;P&gt;That cleared the python error but then I get another error:&lt;/P&gt;&lt;P&gt;"Error&amp;nbsp; &amp;nbsp; DDRC&amp;nbsp; &amp;nbsp; Failed to generate code due to erroneous values used to configure DDR!"&lt;/P&gt;&lt;P&gt;I have all of the values set to the defaults for the MX8M Mini evk and I still get this error.&amp;nbsp; Every time a try to adjust a value I get a message saying "the specified value is not supported".&lt;/P&gt;&lt;P&gt;The same values work properly when I use the Windows based tool.&lt;/P&gt;&lt;P&gt;Don&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 11 Jan 2023 22:27:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Config-Tools-for-i-MX-12-1-Ubuntu-cannot-locat-python/m-p/1581189#M199954</guid>
      <dc:creator>don_gunn</dc:creator>
      <dc:date>2023-01-11T22:27:52Z</dc:date>
    </item>
    <item>
      <title>Re: Config Tools for i.MX 12.1: Ubuntu cannot locat python</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Config-Tools-for-i-MX-12-1-Ubuntu-cannot-locat-python/m-p/1581191#M199955</link>
      <description>If I ignore the message and try to run the tests It fails with the following message:&lt;BR /&gt;&lt;BR /&gt;/opt/nxp/i.MX_CFG_v12.1/bin/python38/bin/python: Error while finding module specification for 'memtool.s' (ModuleNotFoundError: No module named 'memtool')</description>
      <pubDate>Wed, 11 Jan 2023 22:31:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Config-Tools-for-i-MX-12-1-Ubuntu-cannot-locat-python/m-p/1581191#M199955</guid>
      <dc:creator>don_gunn</dc:creator>
      <dc:date>2023-01-11T22:31:02Z</dc:date>
    </item>
    <item>
      <title>Re: Config Tools for i.MX 12.1: Ubuntu cannot locat python</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Config-Tools-for-i-MX-12-1-Ubuntu-cannot-locat-python/m-p/1581192#M199956</link>
      <description>One thing I just noticed - If I save my configuration the&lt;BR /&gt;"Error DDRC Failed to generate code due to erroneous values used to configure DDR!"&lt;BR /&gt;&lt;BR /&gt;message goes away but when I try to run the tests on my board I get the message about missing memtool.</description>
      <pubDate>Wed, 11 Jan 2023 22:33:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Config-Tools-for-i-MX-12-1-Ubuntu-cannot-locat-python/m-p/1581192#M199956</guid>
      <dc:creator>don_gunn</dc:creator>
      <dc:date>2023-01-11T22:33:23Z</dc:date>
    </item>
    <item>
      <title>Re: Config Tools for i.MX 12.1: Ubuntu cannot locat python</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Config-Tools-for-i-MX-12-1-Ubuntu-cannot-locat-python/m-p/2199121#M241942</link>
      <description>&lt;P&gt;I also got Python related errors when trying to generate the `lpddr4_config.c` file for U-Boot&lt;BR /&gt;with the i.MX config tools version 25.06. It looks like the tool does not ship the&lt;BR /&gt;correct Python version since `python3.13` is symlinked to `python3.12` in the `bin` directory.&lt;BR /&gt;&lt;BR /&gt;I got it working and successfully generate the config file on Debian 13&lt;BR /&gt;which uses Python 3.13 as system wide python by replacing the `python3.13` symlink with a link to&lt;BR /&gt;the system python. This can be done with the following bash command:&lt;BR /&gt;`(cd i.MX_CFG_25.06/bin/python3/bin &amp;amp;&amp;amp; rm python3.13 &amp;amp;&amp;amp; ln -s /usr/bin/python3.13 python3.13)`&lt;BR /&gt;&lt;BR /&gt;Additionally, the `tools` binary has to be executed directly from the `bin` directory, e.g.&lt;BR /&gt;`(cd i.MX_CFG_25.06/bin &amp;amp;&amp;amp; ./tools)&lt;/P&gt;</description>
      <pubDate>Wed, 05 Nov 2025 14:57:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Config-Tools-for-i-MX-12-1-Ubuntu-cannot-locat-python/m-p/2199121#M241942</guid>
      <dc:creator>maximilian-maisel-bl</dc:creator>
      <dc:date>2025-11-05T14:57:05Z</dc:date>
    </item>
  </channel>
</rss>