<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic IMX8MM + AS4C512M16D4-75BCN in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MM-AS4C512M16D4-75BCN/m-p/1580934#M199937</link>
    <description>&lt;P&gt;I use a custom board with i.MX8MM and&amp;nbsp;AS4C512M16D4-75BCN. Electrical control is fine, and an x-ray of soldering is fine. but I have trouble with DDR. RPA file with my setting and schematic attached.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Log from i.MX/Mscale DDR Tool. v3.10&lt;BR /&gt;&lt;BR /&gt;Downloading file 'bin\ddr4_train1d_string.bin' ..Done&lt;/P&gt;&lt;P&gt;Downloading file 'bin\ddr4_train2d_string.bin' ..Done&lt;/P&gt;&lt;P&gt;Downloading file 'bin\ddr4_imem_1d.bin' ..Done&lt;/P&gt;&lt;P&gt;Downloading file 'bin\ddr4_dmem_1d.bin' ..Done&lt;/P&gt;&lt;P&gt;Downloading file 'bin\ddr4_imem_2d.bin' ..Done&lt;/P&gt;&lt;P&gt;Downloading file 'bin\ddr4_dmem_2d.bin' ..Done&lt;/P&gt;&lt;P&gt;Downloading IVT header...Done&lt;BR /&gt;Downloading file 'bin\m845s_ddr_stress_test.bin' ...Done&lt;/P&gt;&lt;P&gt;Download is complete&lt;BR /&gt;Waiting for the target board boot...&lt;BR /&gt;I2C_I2SR(0x30a2000c):0x93&lt;BR /&gt;bus is not ready&lt;BR /&gt;hardware_init exit&lt;/P&gt;&lt;P&gt;*************************************************************************&lt;/P&gt;&lt;P&gt;*************************************************************************&lt;/P&gt;&lt;P&gt;*************************************************************************&lt;BR /&gt;MX8 DDR Stress Test V3.10&lt;BR /&gt;Built on Feb 5 2020 13:04:09&lt;BR /&gt;*************************************************************************&lt;/P&gt;&lt;P&gt;--Set up the MMU and enable I and D cache--&lt;BR /&gt;- This is the Cortex-A53 core&lt;BR /&gt;- Check if I cache is enabled&lt;BR /&gt;- Enabling I cache since it was disabled&lt;BR /&gt;- Push base address of TTB to TTBR0_EL3&lt;BR /&gt;- Config TCR_EL3&lt;BR /&gt;- Config MAIR_EL3&lt;BR /&gt;- Enable MMU&lt;BR /&gt;- Data Cache has been enabled&lt;BR /&gt;- Check system memory register, only for debug&lt;/P&gt;&lt;P&gt;- VMCR Check:&lt;BR /&gt;- ttbr0_el3: 0x93d000&lt;BR /&gt;- tcr_el3: 0x2051c&lt;BR /&gt;- mair_el3: 0x774400&lt;BR /&gt;- sctlr_el3: 0xc01815&lt;BR /&gt;- id_aa64mmfr0_el1: 0x1122&lt;/P&gt;&lt;P&gt;- MMU and cache setup complete&lt;/P&gt;&lt;P&gt;*************************************************************************&lt;BR /&gt;ARM clock(CA53) rate: 1800MHz&lt;BR /&gt;DDR Clock: 1000MHz&lt;/P&gt;&lt;P&gt;============================================&lt;BR /&gt;DDR configuration&lt;BR /&gt;DDR type is DDR4&lt;BR /&gt;Data width: 16, bank num: 8&lt;BR /&gt;For DDR4, bank num is the total of 2 bank groups and 4 banks per group&lt;BR /&gt;Row size: 16, col size: 10&lt;BR /&gt;One chip select is used&lt;BR /&gt;Number of DDR controllers used on the SoC: 1&lt;BR /&gt;Density per chip select: 1024MB&lt;BR /&gt;Density per controller is: 1024MB&lt;BR /&gt;Total density detected on the board is: 1024MB&lt;BR /&gt;============================================&lt;/P&gt;&lt;P&gt;MX8M-mini: Cortex-A53 is found&lt;/P&gt;&lt;P&gt;*************************************************************************&lt;/P&gt;&lt;P&gt;============ Step 1: DDRPHY Training... ============&lt;BR /&gt;---DDR 1D-Training @800Mhz...&lt;BR /&gt;[Process] End of initialization&lt;BR /&gt;[Process] End of read enable training&lt;BR /&gt;[Process] End of fine write leveling&lt;BR /&gt;PMU: Error: dbyte 0 lane 0 failed read deskew&lt;BR /&gt;PMU: ***** Assertion Error - terminating *****&lt;BR /&gt;[Result] FAILED&lt;BR /&gt;&lt;BR /&gt;What does mean that error? Give me any tips, please.&lt;/P&gt;</description>
    <pubDate>Wed, 11 Jan 2023 17:57:26 GMT</pubDate>
    <dc:creator>AlekseyM</dc:creator>
    <dc:date>2023-01-11T17:57:26Z</dc:date>
    <item>
      <title>IMX8MM + AS4C512M16D4-75BCN</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MM-AS4C512M16D4-75BCN/m-p/1580934#M199937</link>
      <description>&lt;P&gt;I use a custom board with i.MX8MM and&amp;nbsp;AS4C512M16D4-75BCN. Electrical control is fine, and an x-ray of soldering is fine. but I have trouble with DDR. RPA file with my setting and schematic attached.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Log from i.MX/Mscale DDR Tool. v3.10&lt;BR /&gt;&lt;BR /&gt;Downloading file 'bin\ddr4_train1d_string.bin' ..Done&lt;/P&gt;&lt;P&gt;Downloading file 'bin\ddr4_train2d_string.bin' ..Done&lt;/P&gt;&lt;P&gt;Downloading file 'bin\ddr4_imem_1d.bin' ..Done&lt;/P&gt;&lt;P&gt;Downloading file 'bin\ddr4_dmem_1d.bin' ..Done&lt;/P&gt;&lt;P&gt;Downloading file 'bin\ddr4_imem_2d.bin' ..Done&lt;/P&gt;&lt;P&gt;Downloading file 'bin\ddr4_dmem_2d.bin' ..Done&lt;/P&gt;&lt;P&gt;Downloading IVT header...Done&lt;BR /&gt;Downloading file 'bin\m845s_ddr_stress_test.bin' ...Done&lt;/P&gt;&lt;P&gt;Download is complete&lt;BR /&gt;Waiting for the target board boot...&lt;BR /&gt;I2C_I2SR(0x30a2000c):0x93&lt;BR /&gt;bus is not ready&lt;BR /&gt;hardware_init exit&lt;/P&gt;&lt;P&gt;*************************************************************************&lt;/P&gt;&lt;P&gt;*************************************************************************&lt;/P&gt;&lt;P&gt;*************************************************************************&lt;BR /&gt;MX8 DDR Stress Test V3.10&lt;BR /&gt;Built on Feb 5 2020 13:04:09&lt;BR /&gt;*************************************************************************&lt;/P&gt;&lt;P&gt;--Set up the MMU and enable I and D cache--&lt;BR /&gt;- This is the Cortex-A53 core&lt;BR /&gt;- Check if I cache is enabled&lt;BR /&gt;- Enabling I cache since it was disabled&lt;BR /&gt;- Push base address of TTB to TTBR0_EL3&lt;BR /&gt;- Config TCR_EL3&lt;BR /&gt;- Config MAIR_EL3&lt;BR /&gt;- Enable MMU&lt;BR /&gt;- Data Cache has been enabled&lt;BR /&gt;- Check system memory register, only for debug&lt;/P&gt;&lt;P&gt;- VMCR Check:&lt;BR /&gt;- ttbr0_el3: 0x93d000&lt;BR /&gt;- tcr_el3: 0x2051c&lt;BR /&gt;- mair_el3: 0x774400&lt;BR /&gt;- sctlr_el3: 0xc01815&lt;BR /&gt;- id_aa64mmfr0_el1: 0x1122&lt;/P&gt;&lt;P&gt;- MMU and cache setup complete&lt;/P&gt;&lt;P&gt;*************************************************************************&lt;BR /&gt;ARM clock(CA53) rate: 1800MHz&lt;BR /&gt;DDR Clock: 1000MHz&lt;/P&gt;&lt;P&gt;============================================&lt;BR /&gt;DDR configuration&lt;BR /&gt;DDR type is DDR4&lt;BR /&gt;Data width: 16, bank num: 8&lt;BR /&gt;For DDR4, bank num is the total of 2 bank groups and 4 banks per group&lt;BR /&gt;Row size: 16, col size: 10&lt;BR /&gt;One chip select is used&lt;BR /&gt;Number of DDR controllers used on the SoC: 1&lt;BR /&gt;Density per chip select: 1024MB&lt;BR /&gt;Density per controller is: 1024MB&lt;BR /&gt;Total density detected on the board is: 1024MB&lt;BR /&gt;============================================&lt;/P&gt;&lt;P&gt;MX8M-mini: Cortex-A53 is found&lt;/P&gt;&lt;P&gt;*************************************************************************&lt;/P&gt;&lt;P&gt;============ Step 1: DDRPHY Training... ============&lt;BR /&gt;---DDR 1D-Training @800Mhz...&lt;BR /&gt;[Process] End of initialization&lt;BR /&gt;[Process] End of read enable training&lt;BR /&gt;[Process] End of fine write leveling&lt;BR /&gt;PMU: Error: dbyte 0 lane 0 failed read deskew&lt;BR /&gt;PMU: ***** Assertion Error - terminating *****&lt;BR /&gt;[Result] FAILED&lt;BR /&gt;&lt;BR /&gt;What does mean that error? Give me any tips, please.&lt;/P&gt;</description>
      <pubDate>Wed, 11 Jan 2023 17:57:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8MM-AS4C512M16D4-75BCN/m-p/1580934#M199937</guid>
      <dc:creator>AlekseyM</dc:creator>
      <dc:date>2023-01-11T17:57:26Z</dc:date>
    </item>
    <item>
      <title>回复： IMX8MM + AS4C512M16D4-75BCN</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MM-AS4C512M16D4-75BCN/m-p/1949883#M228186</link>
      <description>&lt;P&gt;I had the same problem. Have you solved it yet？&lt;/P&gt;</description>
      <pubDate>Mon, 09 Sep 2024 08:04:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8MM-AS4C512M16D4-75BCN/m-p/1949883#M228186</guid>
      <dc:creator>ruirui</dc:creator>
      <dc:date>2024-09-09T08:04:38Z</dc:date>
    </item>
    <item>
      <title>回复： IMX8MM + AS4C512M16D4-75BCN</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MM-AS4C512M16D4-75BCN/m-p/1950031#M228191</link>
      <description>&lt;P&gt;Yes, it was a mistake with diffpair connections.&lt;/P&gt;</description>
      <pubDate>Mon, 09 Sep 2024 11:01:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8MM-AS4C512M16D4-75BCN/m-p/1950031#M228191</guid>
      <dc:creator>AlekseyM</dc:creator>
      <dc:date>2024-09-09T11:01:43Z</dc:date>
    </item>
    <item>
      <title>回复： IMX8MM + AS4C512M16D4-75BCN</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MM-AS4C512M16D4-75BCN/m-p/1950708#M228235</link>
      <description>&lt;P&gt;Can you tell me more about it? I have no idea about the same problem now,thanks a lot.&lt;/P&gt;</description>
      <pubDate>Tue, 10 Sep 2024 06:44:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8MM-AS4C512M16D4-75BCN/m-p/1950708#M228235</guid>
      <dc:creator>ruirui</dc:creator>
      <dc:date>2024-09-10T06:44:50Z</dc:date>
    </item>
  </channel>
</rss>