<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: Using FFT on iMXRT-685-aud-evk DSP</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Using-FFT-on-iMXRT-685-aud-evk-DSP/m-p/1580608#M199897</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/209911"&gt;@MrRv&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;Please refer to the Naturedsp example at SDK_2_12_0_EVK-MIMXRT685\boards\evkmimxrt685\dsp_examples\naturedsp\dsp.&lt;/P&gt;
&lt;P&gt;It shows how to use DSP to perform FFT and other calculations.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Jing&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 11 Jan 2023 07:19:27 GMT</pubDate>
    <dc:creator>jingpan</dc:creator>
    <dc:date>2023-01-11T07:19:27Z</dc:date>
    <item>
      <title>Using FFT on iMXRT-685-aud-evk DSP</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Using-FFT-on-iMXRT-685-aud-evk-DSP/m-p/1579365#M199778</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I'm working on the iMX RT685-aud-evk board, and I'm interested in performing FFT in a library for the DSP.&lt;BR /&gt;However, the only examples I could find regarding using FFT are using the CMSIS libraries, which, as I understand, are used from the CPU side.&lt;/P&gt;&lt;P&gt;Are there resources regarding usage of FFT functionality (and other mathematical functions) on the DSP alone?&lt;/P&gt;&lt;P&gt;Thanks in advance!&lt;/P&gt;</description>
      <pubDate>Mon, 09 Jan 2023 14:30:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Using-FFT-on-iMXRT-685-aud-evk-DSP/m-p/1579365#M199778</guid>
      <dc:creator>MrRv</dc:creator>
      <dc:date>2023-01-09T14:30:31Z</dc:date>
    </item>
    <item>
      <title>Re: Using FFT on iMXRT-685-aud-evk DSP</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Using-FFT-on-iMXRT-685-aud-evk-DSP/m-p/1580608#M199897</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/209911"&gt;@MrRv&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;Please refer to the Naturedsp example at SDK_2_12_0_EVK-MIMXRT685\boards\evkmimxrt685\dsp_examples\naturedsp\dsp.&lt;/P&gt;
&lt;P&gt;It shows how to use DSP to perform FFT and other calculations.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Jing&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 11 Jan 2023 07:19:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Using-FFT-on-iMXRT-685-aud-evk-DSP/m-p/1580608#M199897</guid>
      <dc:creator>jingpan</dc:creator>
      <dc:date>2023-01-11T07:19:27Z</dc:date>
    </item>
  </channel>
</rss>