<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Where are the NatureDSP unit tests? in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Where-are-the-NatureDSP-unit-tests/m-p/1578817#M199714</link>
    <description>&lt;P&gt;Hi,&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;Although I have the i.mxrt board, I am running HIFI4 DSP examples using simulation.&lt;BR /&gt;&lt;BR /&gt;This question is independent of the specific NXP board, I posted the question in this i.MX forum because the document refers to the DSP unit_test which I don't see present in the downloads mentioned.&lt;BR /&gt;&lt;BR /&gt;I would appreciate it if I get any pointers to locate the unit tests.&lt;BR /&gt;&lt;BR /&gt;Thanks,&lt;BR /&gt;Abdo&lt;/P&gt;</description>
    <pubDate>Sun, 08 Jan 2023 05:26:11 GMT</pubDate>
    <dc:creator>abdob</dc:creator>
    <dc:date>2023-01-08T05:26:11Z</dc:date>
    <item>
      <title>Where are the NatureDSP unit tests?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Where-are-the-NatureDSP-unit-tests/m-p/1577475#M199529</link>
      <description>&lt;P&gt;Hi,&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;This DSP User's guide:&lt;BR /&gt;&lt;BR /&gt;&lt;A href="https://www.nxp.com/docs/en/user-guide/IMX_DSP_USERS_GUIDE.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/user-guide/IMX_DSP_USERS_GUIDE.pdf&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;refers to the unit_tests in this location:&lt;BR /&gt;&lt;BR /&gt;Unit test location: rootfs: /unit_tests/DSP/naturedsp_test&lt;BR /&gt;&lt;BR /&gt;Where can I find the unit tests? I've tried downloading and extracting the packages in the user guide, but I don't see the unit_tests directory anywhere.&lt;BR /&gt;&lt;BR /&gt;Thanks,&lt;BR /&gt;Abdo&lt;/P&gt;</description>
      <pubDate>Wed, 04 Jan 2023 22:09:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Where-are-the-NatureDSP-unit-tests/m-p/1577475#M199529</guid>
      <dc:creator>abdob</dc:creator>
      <dc:date>2023-01-04T22:09:44Z</dc:date>
    </item>
    <item>
      <title>Re: Where are the NatureDSP unit tests?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Where-are-the-NatureDSP-unit-tests/m-p/1577679#M199558</link>
      <description>&lt;P&gt;firstly download images to your board, then you can find this when board boot up&lt;/P&gt;
&lt;P&gt;"&lt;A href="https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applications-processors:IMXLINUX" target="_blank"&gt;https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applications-processors:IMXLINUX&lt;/A&gt;"&lt;/P&gt;</description>
      <pubDate>Thu, 05 Jan 2023 05:57:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Where-are-the-NatureDSP-unit-tests/m-p/1577679#M199558</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2023-01-05T05:57:34Z</dc:date>
    </item>
    <item>
      <title>Re: Where are the NatureDSP unit tests?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Where-are-the-NatureDSP-unit-tests/m-p/1578165#M199630</link>
      <description>&lt;P&gt;I was able to extract the rootfs from the I.MX 8M Plus EVK and I.MX 8QuadMax MEK images, I see /unit_tests/DSP directory however it only contains&amp;nbsp;dsp_rend_test.out and dsp_test.out.&lt;BR /&gt;&lt;BR /&gt;I don't have the actual boards but I am attempting to reuse the test vectors for the MIMRT685 EVK which includes the HIFI4 DSP but is not a linux-based board.&lt;BR /&gt;&lt;BR /&gt;Is the content inside naturedsp_test accessible without having the linux-based boards?&lt;/P&gt;</description>
      <pubDate>Thu, 05 Jan 2023 20:49:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Where-are-the-NatureDSP-unit-tests/m-p/1578165#M199630</guid>
      <dc:creator>abdob</dc:creator>
      <dc:date>2023-01-05T20:49:45Z</dc:date>
    </item>
    <item>
      <title>Re: Where are the NatureDSP unit tests?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Where-are-the-NatureDSP-unit-tests/m-p/1578246#M199638</link>
      <description>&lt;P&gt;the user guide you refer to is for i.mx processor, if you are interested with IMXRT, pls create a new thread and put it in the i.mxRT community, the IMXRT engineer would check this for you, I'm not sure this package is available for imxRT or not&lt;/P&gt;</description>
      <pubDate>Fri, 06 Jan 2023 02:03:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Where-are-the-NatureDSP-unit-tests/m-p/1578246#M199638</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2023-01-06T02:03:39Z</dc:date>
    </item>
    <item>
      <title>Re: Where are the NatureDSP unit tests?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Where-are-the-NatureDSP-unit-tests/m-p/1578817#M199714</link>
      <description>&lt;P&gt;Hi,&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;Although I have the i.mxrt board, I am running HIFI4 DSP examples using simulation.&lt;BR /&gt;&lt;BR /&gt;This question is independent of the specific NXP board, I posted the question in this i.MX forum because the document refers to the DSP unit_test which I don't see present in the downloads mentioned.&lt;BR /&gt;&lt;BR /&gt;I would appreciate it if I get any pointers to locate the unit tests.&lt;BR /&gt;&lt;BR /&gt;Thanks,&lt;BR /&gt;Abdo&lt;/P&gt;</description>
      <pubDate>Sun, 08 Jan 2023 05:26:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Where-are-the-NatureDSP-unit-tests/m-p/1578817#M199714</guid>
      <dc:creator>abdob</dc:creator>
      <dc:date>2023-01-08T05:26:11Z</dc:date>
    </item>
    <item>
      <title>Re: Where are the NatureDSP unit tests?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Where-are-the-NatureDSP-unit-tests/m-p/1578820#M199715</link>
      <description>&lt;P&gt;refer to the user guide,&lt;/P&gt;
&lt;P&gt;"NatureDSP Library package is license restricted on the i.MX platform. License authorization is required from the NXP marketing for the users to access the source code."&lt;/P&gt;
&lt;P&gt;this package is under NDA, so pls contact local representative to get further help, we couldn't share any license restricted packages on the public community&lt;/P&gt;</description>
      <pubDate>Sun, 08 Jan 2023 09:09:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Where-are-the-NatureDSP-unit-tests/m-p/1578820#M199715</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2023-01-08T09:09:03Z</dc:date>
    </item>
  </channel>
</rss>