<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: Using libcamera on the i.MX6 ULL</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Using-libcamera-on-the-i-MX6-ULL/m-p/1577581#M199541</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/210753"&gt;@oneil&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;If you are using NXP yocto project and NXP demo images, you can check if there is gstreamer libcamera libray in /usr.&lt;/P&gt;</description>
    <pubDate>Thu, 05 Jan 2023 02:33:13 GMT</pubDate>
    <dc:creator>Zhiming_Liu</dc:creator>
    <dc:date>2023-01-05T02:33:13Z</dc:date>
    <item>
      <title>Using libcamera on the i.MX6 ULL</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Using-libcamera-on-the-i-MX6-ULL/m-p/1577461#M199527</link>
      <description>&lt;DIV&gt;&lt;DIV&gt;&lt;DIV&gt;&lt;P&gt;I was wondering if anyone has experience using libcamera on the i.MX6 ULL and could give some tips on configuring it to work on this device. I'm new to the i.MX6 ULL family as well as libcamera so am not sure where to start.&lt;/P&gt;&lt;P&gt;Per the libcamera FAQs, there is not official support for the i.MX6 ULL. However, &lt;A href="https://community.nxp.com/t5/i-MX-Processors/i-MX6-and-libcamera/m-p/1394403" target="_blank" rel="noopener"&gt;this post&lt;/A&gt; on NXP Community suggests that it is possible to use it.&lt;/P&gt;&lt;P&gt;Any help is appreciated.&lt;/P&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;</description>
      <pubDate>Wed, 04 Jan 2023 21:26:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Using-libcamera-on-the-i-MX6-ULL/m-p/1577461#M199527</guid>
      <dc:creator>oneil</dc:creator>
      <dc:date>2023-01-04T21:26:36Z</dc:date>
    </item>
    <item>
      <title>Re: Using libcamera on the i.MX6 ULL</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Using-libcamera-on-the-i-MX6-ULL/m-p/1577581#M199541</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/210753"&gt;@oneil&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;If you are using NXP yocto project and NXP demo images, you can check if there is gstreamer libcamera libray in /usr.&lt;/P&gt;</description>
      <pubDate>Thu, 05 Jan 2023 02:33:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Using-libcamera-on-the-i-MX6-ULL/m-p/1577581#M199541</guid>
      <dc:creator>Zhiming_Liu</dc:creator>
      <dc:date>2023-01-05T02:33:13Z</dc:date>
    </item>
  </channel>
</rss>