<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックYocto kernel module folder name change when config is changed</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Yocto-kernel-module-folder-name-change-when-config-is-changed/m-p/1576326#M199399</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Currently I'm facing an issue where when I add any additional kernel module or remove a module the folder name of the kernel modules also changes, so during upgrade I have to upgrade both kernel and rootfs. But the intended solution is to only update the rootfs and not the kernel module.&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;/lib/modules/5.10.9-1.0.0&lt;STRONG&gt;+g170b779cb1ba, &lt;/STRONG&gt;I've added an example path for the kernel module in my yocto build where the characters in bold after the &lt;STRONG&gt;"+" &lt;/STRONG&gt;sign changes when a new module is added or removed. Is there any way to have the path as a constant so that only rootfs upgrade can be done without the kernel upgrade.&lt;BR /&gt;&lt;BR /&gt;&lt;/SPAN&gt;Thanks in advance.&lt;/P&gt;</description>
    <pubDate>Tue, 03 Jan 2023 05:56:23 GMT</pubDate>
    <dc:creator>rvignesh496</dc:creator>
    <dc:date>2023-01-03T05:56:23Z</dc:date>
    <item>
      <title>Yocto kernel module folder name change when config is changed</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Yocto-kernel-module-folder-name-change-when-config-is-changed/m-p/1576326#M199399</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Currently I'm facing an issue where when I add any additional kernel module or remove a module the folder name of the kernel modules also changes, so during upgrade I have to upgrade both kernel and rootfs. But the intended solution is to only update the rootfs and not the kernel module.&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;/lib/modules/5.10.9-1.0.0&lt;STRONG&gt;+g170b779cb1ba, &lt;/STRONG&gt;I've added an example path for the kernel module in my yocto build where the characters in bold after the &lt;STRONG&gt;"+" &lt;/STRONG&gt;sign changes when a new module is added or removed. Is there any way to have the path as a constant so that only rootfs upgrade can be done without the kernel upgrade.&lt;BR /&gt;&lt;BR /&gt;&lt;/SPAN&gt;Thanks in advance.&lt;/P&gt;</description>
      <pubDate>Tue, 03 Jan 2023 05:56:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Yocto-kernel-module-folder-name-change-when-config-is-changed/m-p/1576326#M199399</guid>
      <dc:creator>rvignesh496</dc:creator>
      <dc:date>2023-01-03T05:56:23Z</dc:date>
    </item>
    <item>
      <title>Re: Yocto kernel module folder name change when config is changed</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Yocto-kernel-module-folder-name-change-when-config-is-changed/m-p/1577535#M199537</link>
      <description>&lt;P&gt;You should handle this change in kernel module side.&lt;/P&gt;</description>
      <pubDate>Thu, 05 Jan 2023 01:24:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Yocto-kernel-module-folder-name-change-when-config-is-changed/m-p/1577535#M199537</guid>
      <dc:creator>Zhiming_Liu</dc:creator>
      <dc:date>2023-01-05T01:24:30Z</dc:date>
    </item>
  </channel>
</rss>