<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic DFU using USB Mass Storage in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/DFU-using-USB-Mass-Storage/m-p/1576011#M199374</link>
    <description>&lt;P&gt;We have a development board custom PCB. In addition, in development NXP INMX 1173 Controller, need to develop DFU which works on USB Flash Drive. If I plug the USB Drive (Pen Drive) It has to upload the firmware . Using KEIL and FreeRTOS.&lt;/P&gt;&lt;P&gt;Is there is any sample code and application note to evaluate this.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;BR /&gt;Swetha&lt;/P&gt;</description>
    <pubDate>Mon, 02 Jan 2023 09:36:03 GMT</pubDate>
    <dc:creator>Swethakrishnaraj</dc:creator>
    <dc:date>2023-01-02T09:36:03Z</dc:date>
    <item>
      <title>DFU using USB Mass Storage</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/DFU-using-USB-Mass-Storage/m-p/1576011#M199374</link>
      <description>&lt;P&gt;We have a development board custom PCB. In addition, in development NXP INMX 1173 Controller, need to develop DFU which works on USB Flash Drive. If I plug the USB Drive (Pen Drive) It has to upload the firmware . Using KEIL and FreeRTOS.&lt;/P&gt;&lt;P&gt;Is there is any sample code and application note to evaluate this.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;BR /&gt;Swetha&lt;/P&gt;</description>
      <pubDate>Mon, 02 Jan 2023 09:36:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/DFU-using-USB-Mass-Storage/m-p/1576011#M199374</guid>
      <dc:creator>Swethakrishnaraj</dc:creator>
      <dc:date>2023-01-02T09:36:03Z</dc:date>
    </item>
    <item>
      <title>Re: DFU using USB Mass Storage</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/DFU-using-USB-Mass-Storage/m-p/1576197#M199386</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/210522"&gt;@Swethakrishnaraj&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;I'm afraid we don't currently provide any documentation or example code that assimilates what you are looking for. Sorry for the inconvenience this may cause.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR,&lt;/P&gt;
&lt;P&gt;Edwin.&lt;/P&gt;</description>
      <pubDate>Mon, 02 Jan 2023 21:41:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/DFU-using-USB-Mass-Storage/m-p/1576197#M199386</guid>
      <dc:creator>EdwinHz</dc:creator>
      <dc:date>2023-01-02T21:41:15Z</dc:date>
    </item>
  </channel>
</rss>