<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Boot mode in MIMXRT1024CAG4B</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Boot-mode-in-MIMXRT1024CAG4B/m-p/1572562#M199029</link>
    <description>&lt;P&gt;1. Of course, you can use &lt;SPAN&gt;Internal&lt;/SPAN&gt;&amp;nbsp;flash for booting&lt;/P&gt;
&lt;P&gt;2. Set&amp;nbsp;&lt;SPAN&gt;BOOT_MODE[1:0] = 10b to enter device boot mode, and also make sure the BT_CFG pins/eFuse 0x450 points to internal NOR Flash, as internal flash is not the only device for booting.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;3. Yes, you can load Program image by HW debugger.&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Tue, 20 Dec 2022 13:36:07 GMT</pubDate>
    <dc:creator>jay_heng</dc:creator>
    <dc:date>2022-12-20T13:36:07Z</dc:date>
    <item>
      <title>Boot mode in MIMXRT1024CAG4B</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Boot-mode-in-MIMXRT1024CAG4B/m-p/1571524#M198902</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Boot Mode:&lt;/P&gt;&lt;P&gt;We are using MIMXRT1024CAG4B Microcontroller for our design and planned to use the On-Chip Flash for booting by setting the Internal Boot Mode (BOOT_MODE[1:0] = 10b).&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Is there any issue in using the Internal Flash for booting?&lt;/LI&gt;&lt;LI&gt;What is the precaution to be taken care in using the Internal Flash from HW and SW perspective?&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;After first Power On, can we use the JTAG Port or Serial Wire Debug Interface for loading the Program Image into the On-Chip memory?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="sowmiya_a_0-1671334133193.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/204794i6AC7197194369C42/image-size/medium?v=v2&amp;amp;px=400" role="button" title="sowmiya_a_0-1671334133193.png" alt="sowmiya_a_0-1671334133193.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Sun, 18 Dec 2022 03:31:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Boot-mode-in-MIMXRT1024CAG4B/m-p/1571524#M198902</guid>
      <dc:creator>sowmiya_a</dc:creator>
      <dc:date>2022-12-18T03:31:05Z</dc:date>
    </item>
    <item>
      <title>Re: Boot mode in MIMXRT1024CAG4B</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Boot-mode-in-MIMXRT1024CAG4B/m-p/1572562#M199029</link>
      <description>&lt;P&gt;1. Of course, you can use &lt;SPAN&gt;Internal&lt;/SPAN&gt;&amp;nbsp;flash for booting&lt;/P&gt;
&lt;P&gt;2. Set&amp;nbsp;&lt;SPAN&gt;BOOT_MODE[1:0] = 10b to enter device boot mode, and also make sure the BT_CFG pins/eFuse 0x450 points to internal NOR Flash, as internal flash is not the only device for booting.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;3. Yes, you can load Program image by HW debugger.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 20 Dec 2022 13:36:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Boot-mode-in-MIMXRT1024CAG4B/m-p/1572562#M199029</guid>
      <dc:creator>jay_heng</dc:creator>
      <dc:date>2022-12-20T13:36:07Z</dc:date>
    </item>
  </channel>
</rss>