<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: i.MX6UL GPIO Pad Configuration &amp;amp; OpenOCD Signal Issues in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6UL-GPIO-Pad-Configuration-amp-OpenOCD-Signal-Issues/m-p/1571754#M198930</link>
    <description>&lt;P&gt;Which pad are you using?&lt;/P&gt;
&lt;P&gt;For example: You could check the pad control setting in the RM.&lt;/P&gt;
&lt;P&gt;IOMUXC_SW_PAD_CTL_PAD_GPIO1_IO00&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;You could try to set the speed and the SRE of the PAD.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Mon, 19 Dec 2022 08:01:53 GMT</pubDate>
    <dc:creator>jimmychan</dc:creator>
    <dc:date>2022-12-19T08:01:53Z</dc:date>
    <item>
      <title>i.MX6UL GPIO Pad Configuration &amp; OpenOCD Signal Issues</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6UL-GPIO-Pad-Configuration-amp-OpenOCD-Signal-Issues/m-p/1568652#M198645</link>
      <description>&lt;P&gt;I am attempting to use an IMX6UL as a JTAG interface utilizing OpenOCD's native bitbang support for the IMX's GPIO.&lt;/P&gt;&lt;P&gt;I have successfully connected to the target at lower speeds such as 100KHz. However, to successfully perform flash functions, I need to set the adapter to speed to at least 500KHz, preferably closer to 1500KHz, and have not yet been able to connect to the target at these higher speeds. I have tried a host of GPIO Pad Control Configurations to optimize the signal output but have yet to find one that can properly handle these high speeds.&lt;/P&gt;&lt;P&gt;Therefore, I have the following two questions:&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;What is the best possible GPIO pad configuration to reach these high speeds?&lt;/LI&gt;&lt;LI&gt;Is it possible to toggle the GPIO registers using the IMX6UL at these higher speeds(500KHz,1500KHz,etc)?&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 13 Dec 2022 00:51:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6UL-GPIO-Pad-Configuration-amp-OpenOCD-Signal-Issues/m-p/1568652#M198645</guid>
      <dc:creator>dev_imx</dc:creator>
      <dc:date>2022-12-13T00:51:39Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6UL GPIO Pad Configuration &amp; OpenOCD Signal Issues</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6UL-GPIO-Pad-Configuration-amp-OpenOCD-Signal-Issues/m-p/1571754#M198930</link>
      <description>&lt;P&gt;Which pad are you using?&lt;/P&gt;
&lt;P&gt;For example: You could check the pad control setting in the RM.&lt;/P&gt;
&lt;P&gt;IOMUXC_SW_PAD_CTL_PAD_GPIO1_IO00&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;You could try to set the speed and the SRE of the PAD.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 19 Dec 2022 08:01:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6UL-GPIO-Pad-Configuration-amp-OpenOCD-Signal-Issues/m-p/1571754#M198930</guid>
      <dc:creator>jimmychan</dc:creator>
      <dc:date>2022-12-19T08:01:53Z</dc:date>
    </item>
  </channel>
</rss>