<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックPWM trigger in imxrt1176</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/PWM-trigger-in-imxrt1176/m-p/1570346#M198806</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I have used PWM example, given in SDK. The code has been modified so that 50Hz signal will generate from PWM_Submodule0 (both from PWMA &amp;amp; PWMB pins). The code is working fine.&lt;/P&gt;&lt;P&gt;Now, I want to count the number of rising edges in the signal. Can anyone help in how exactly this can be done?&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Devaharsha&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 15 Dec 2022 09:48:23 GMT</pubDate>
    <dc:creator>Devaharsha</dc:creator>
    <dc:date>2022-12-15T09:48:23Z</dc:date>
    <item>
      <title>PWM trigger in imxrt1176</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/PWM-trigger-in-imxrt1176/m-p/1570346#M198806</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I have used PWM example, given in SDK. The code has been modified so that 50Hz signal will generate from PWM_Submodule0 (both from PWMA &amp;amp; PWMB pins). The code is working fine.&lt;/P&gt;&lt;P&gt;Now, I want to count the number of rising edges in the signal. Can anyone help in how exactly this can be done?&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Devaharsha&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 15 Dec 2022 09:48:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/PWM-trigger-in-imxrt1176/m-p/1570346#M198806</guid>
      <dc:creator>Devaharsha</dc:creator>
      <dc:date>2022-12-15T09:48:23Z</dc:date>
    </item>
    <item>
      <title>Re: PWM trigger in imxrt1176</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/PWM-trigger-in-imxrt1176/m-p/1572186#M198975</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;Could you elaborate further? or could you give an explanation about the solution you want to achieve?&lt;/P&gt;&lt;P&gt;Best regards,&lt;BR /&gt;Pavel&lt;/P&gt;</description>
      <pubDate>Tue, 20 Dec 2022 02:27:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/PWM-trigger-in-imxrt1176/m-p/1572186#M198975</guid>
      <dc:creator>Pavel_Hernandez</dc:creator>
      <dc:date>2022-12-20T02:27:37Z</dc:date>
    </item>
    <item>
      <title>Re: PWM trigger in imxrt1176</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/PWM-trigger-in-imxrt1176/m-p/1572246#M198980</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;For generating PWM signal, I am using modified SDK example such that the signal will be of 50 Hz.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am using this signal as the input to stepper motor. What I understood is, the stepper motor steps every time a rise edge signal is detected. So, if I want lets say 50 degrees that corresponds to 200 steps, there should be 200 rising edges as the input.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Can you help with this issue on how to count number of rising edges in the PWM signal?&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Devaharsha&amp;nbsp; &amp;nbsp;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 20 Dec 2022 04:26:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/PWM-trigger-in-imxrt1176/m-p/1572246#M198980</guid>
      <dc:creator>Devaharsha</dc:creator>
      <dc:date>2022-12-20T04:26:26Z</dc:date>
    </item>
    <item>
      <title>Re: PWM trigger in imxrt1176</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/PWM-trigger-in-imxrt1176/m-p/1572746#M199043</link>
      <description>&lt;P&gt;Hello,&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thanks for being clear, I suggest using the FTM input capture to detect the rising edge and count, to do that there is no example available for that solution in the SDK.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I recommend reviewing this app note this is for LPC but using the same module of eflexPWM maybe could help you to get more details to implement in your application.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/docs/en/application-note/AN13724.pdf" target="_blank"&gt;Stepper Motor Control on LPC55S3x (nxp.com)&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Pavel&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 20 Dec 2022 22:34:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/PWM-trigger-in-imxrt1176/m-p/1572746#M199043</guid>
      <dc:creator>Pavel_Hernandez</dc:creator>
      <dc:date>2022-12-20T22:34:15Z</dc:date>
    </item>
  </channel>
</rss>