<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Unable to Flash NAND using Windows or over commandline in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Unable-to-Flash-NAND-using-Windows-or-over-commandline/m-p/154797#M1988</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp; in continuation i have also seen multiple failures using the nandtest utility. is there a corellation?. How could i make sure that i can boot from SD and transfer to NAND?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;regards,&lt;/P&gt;&lt;P&gt;Vikram.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 13 May 2011 11:22:25 GMT</pubDate>
    <dc:creator>VikramU_ng</dc:creator>
    <dc:date>2011-05-13T11:22:25Z</dc:date>
    <item>
      <title>Unable to Flash NAND using Windows or over commandline</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Unable-to-Flash-NAND-using-Windows-or-over-commandline/m-p/154796#M1987</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear all,&lt;/P&gt;&lt;P&gt;&amp;nbsp; On a iMX233 EVK, i have run into a problem booting from SD that i am unable to transfer contents to the NAND.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;SPAN&gt;From the commandline... &lt;/SPAN&gt;&lt;STRONG&gt;kobs-ng&lt;/STRONG&gt;&lt;SPAN&gt; fails to complete and reports a failed to commit structures error.&lt;/SPAN&gt;&lt;P&gt;With the &lt;STRONG&gt;Mfgtool,&lt;/STRONG&gt; on Windows, it fails to complete NAND update in USB mode(0000 switch setting).&lt;/P&gt;&lt;P&gt;Is there something wrong with the EVK?. How do i confirm the NAND.&lt;/P&gt;&lt;P&gt;Attached are the screenshots from Winows for Mfgtool and from the device terminal.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Kindly help regards possible solutions.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 May 2011 04:10:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Unable-to-Flash-NAND-using-Windows-or-over-commandline/m-p/154796#M1987</guid>
      <dc:creator>VikramU_ng</dc:creator>
      <dc:date>2011-05-12T04:10:51Z</dc:date>
    </item>
    <item>
      <title>Re: Unable to Flash NAND using Windows or over commandline</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Unable-to-Flash-NAND-using-Windows-or-over-commandline/m-p/154797#M1988</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp; in continuation i have also seen multiple failures using the nandtest utility. is there a corellation?. How could i make sure that i can boot from SD and transfer to NAND?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;regards,&lt;/P&gt;&lt;P&gt;Vikram.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 13 May 2011 11:22:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Unable-to-Flash-NAND-using-Windows-or-over-commandline/m-p/154797#M1988</guid>
      <dc:creator>VikramU_ng</dc:creator>
      <dc:date>2011-05-13T11:22:25Z</dc:date>
    </item>
    <item>
      <title>Re: Unable to Flash NAND using Windows or over commandline</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Unable-to-Flash-NAND-using-Windows-or-over-commandline/m-p/154798#M1989</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi All,&lt;/P&gt;&lt;P&gt;&amp;nbsp; I followed the advice of another colleague and have used the sb_loader utility on Windows. still am unable to flash the Image to the EVK. Could someone confirm if the sb_loader works?.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;EVK switch settings are detailed:&lt;/P&gt;&lt;P&gt;S12(Battery Supply) in Left Switch/ External power&lt;/P&gt;&lt;P&gt;S1 Hold in in OFF&lt;/P&gt;&lt;P&gt;S22(Debug) in Lower(off Mode)&lt;/P&gt;&lt;P&gt;S14(USB) in USB 5V UP Position&lt;/P&gt;&lt;P&gt;Boot Switches in 0000 -USB Mode.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;as described i have failed to burn using Mfgtool versions mfgtool version 1.6.2.032 and 1.6.2.006&amp;nbsp; earlier. Nand is Fine since on SD Boot up the Toshiba Nand Information is intact. Could someone confirm and help please.&lt;/P&gt;&lt;P&gt;Attached is the screenshot from using commandline tool&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;regards.&lt;/P&gt;&lt;P&gt;Vikram.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 11 Jun 2011 08:06:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Unable-to-Flash-NAND-using-Windows-or-over-commandline/m-p/154798#M1989</guid>
      <dc:creator>VikramU_ng</dc:creator>
      <dc:date>2011-06-11T08:06:04Z</dc:date>
    </item>
  </channel>
</rss>