<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックUsing Function Pointers with Position Independent Code.</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Using-Function-Pointers-with-Position-Independent-Code/m-p/1570031#M198774</link>
    <description>&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;We're currently trying to implement two separate slots to store the our application in. The application is supposed to be position independent, so that it can run from either slot.&amp;nbsp;&lt;/P&gt;&lt;P&gt;We've encountered an issue where function pointers that are initialized before runtime point to the incorrect address, as they do not have the added offset for slot two.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Can we configure the compiler so that function pointers will use the GOT table to call the function? That way we can add the correct offset to the address in the startup code?&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
    <pubDate>Thu, 15 Dec 2022 00:02:31 GMT</pubDate>
    <dc:creator>rnicolls</dc:creator>
    <dc:date>2022-12-15T00:02:31Z</dc:date>
    <item>
      <title>Using Function Pointers with Position Independent Code.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Using-Function-Pointers-with-Position-Independent-Code/m-p/1570031#M198774</link>
      <description>&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;We're currently trying to implement two separate slots to store the our application in. The application is supposed to be position independent, so that it can run from either slot.&amp;nbsp;&lt;/P&gt;&lt;P&gt;We've encountered an issue where function pointers that are initialized before runtime point to the incorrect address, as they do not have the added offset for slot two.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Can we configure the compiler so that function pointers will use the GOT table to call the function? That way we can add the correct offset to the address in the startup code?&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
      <pubDate>Thu, 15 Dec 2022 00:02:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Using-Function-Pointers-with-Position-Independent-Code/m-p/1570031#M198774</guid>
      <dc:creator>rnicolls</dc:creator>
      <dc:date>2022-12-15T00:02:31Z</dc:date>
    </item>
    <item>
      <title>Re: Using Function Pointers with Position Independent Code.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Using-Function-Pointers-with-Position-Independent-Code/m-p/1572047#M198966</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/206323"&gt;@rnicolls&lt;/a&gt;&amp;nbsp;,&lt;BR /&gt;&lt;BR /&gt;I hope you're having a great day. Could you let us know the board you're using to review in more detail your case?&lt;BR /&gt;&lt;BR /&gt;Thank you in advance.&lt;BR /&gt;&lt;BR /&gt;Best regards,&lt;BR /&gt;Hector.&lt;/P&gt;</description>
      <pubDate>Mon, 19 Dec 2022 18:55:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Using-Function-Pointers-with-Position-Independent-Code/m-p/1572047#M198966</guid>
      <dc:creator>hector_delgado</dc:creator>
      <dc:date>2022-12-19T18:55:21Z</dc:date>
    </item>
    <item>
      <title>Re: Using Function Pointers with Position Independent Code.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Using-Function-Pointers-with-Position-Independent-Code/m-p/1573327#M199096</link>
      <description>&lt;P&gt;Hi Hector,&lt;/P&gt;&lt;P&gt;I'm using this board from Embedded Artists:&amp;nbsp;&lt;A href="https://www.embeddedartists.com/products/imx-rt1176-developers-kit/" target="_blank"&gt;https://www.embeddedartists.com/products/imx-rt1176-developers-kit/&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Thank you.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 21 Dec 2022 22:03:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Using-Function-Pointers-with-Position-Independent-Code/m-p/1573327#M199096</guid>
      <dc:creator>rnicolls</dc:creator>
      <dc:date>2022-12-21T22:03:50Z</dc:date>
    </item>
  </channel>
</rss>