<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Poor ping performance - i.MX 8M Plus</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Poor-ping-performance-i-MX-8M-Plus/m-p/1569477#M198735</link>
    <description>&lt;P&gt;Hi Qmiller,&lt;/P&gt;&lt;P&gt;Thanks for your reply. I understand that ENET_QoS is attached to eth1, but my question regards eth0.&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I did some ping tests on the NXP i.mx8m-plus EVK with realtime edge 2.2.0.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;ETH0 - 1.162ms&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;ETH1 - 0.312ms&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;These numbers are similar on any i.MX8M Plus device that I could test. Custom boards and NXP's own EVK, running NXP's realtime edge.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Why is eth0 ping time double than eth1?&lt;/P&gt;&lt;P&gt;What can I do in order to achieve better performance with eth0?&lt;/P&gt;&lt;P&gt;Thanks a lot,&lt;/P&gt;&lt;P&gt;Nir.&lt;/P&gt;</description>
    <pubDate>Wed, 14 Dec 2022 07:59:16 GMT</pubDate>
    <dc:creator>NG_R3</dc:creator>
    <dc:date>2022-12-14T07:59:16Z</dc:date>
    <item>
      <title>Poor ping performance - i.MX 8M Plus</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Poor-ping-performance-i-MX-8M-Plus/m-p/1562838#M198245</link>
      <description>&lt;P&gt;Hi there,&lt;/P&gt;&lt;P&gt;I'm running imx-kernel 5.15.32 on a&amp;nbsp;i.MX 8M Plus based custom board.&lt;BR /&gt;I have 2 nics:&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;# ethtool -i eth0
driver: fec
version: 5.15.60-tq+g03954e24f9ca-rt49-t
firmware-version:
expansion-rom-version:
bus-info: eth0
supports-statistics: yes
supports-test: yes
supports-eeprom-access: no
supports-register-dump: yes
supports-priv-flags: no


# ethtool -i eth1
driver: st_gmac
version: Jan_2016
firmware-version:
expansion-rom-version:
bus-info:
supports-statistics: yes
supports-test: no
supports-eeprom-access: no
supports-register-dump: yes
supports-priv-flags: no&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm experiencing poor results (average, and mdev) when sending ping to eth0, and better results when pinging eth1:&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;ping eth0 results:
...
...
64 bytes from 90.0.0.2: icmp_seq=34463 ttl=63 time=1.02 ms
64 bytes from 90.0.0.2: icmp_seq=34464 ttl=63 time=0.949 ms

--- 90.0.0.2 ping statistics ---
100000 packets transmitted, 99999 received, 0.001% packet loss, time 107149ms
rtt min/avg/max/mdev = 0.131/0.852/12.708/0.388 ms, pipe 2

ping eth1 results
...
...
64 bytes from 90.0.0.2: icmp_seq=34463 ttl=63 time=0.447 ms
64 bytes from 90.0.0.2: icmp_seq=34464 ttl=63 time=0.401 ms

--- 90.0.0.2 ping statistics ---
100000 packets transmitted, 100000 received, 0% packet loss, time 100018ms
rtt min/avg/max/mdev = 0.205/0.411/8.626/0.045 ms&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Why is eth0 ping time double than eth1?&lt;/P&gt;&lt;P&gt;What can I do in order to achieve better performance with eth0?&lt;/P&gt;&lt;P&gt;Thanks a lot,&lt;/P&gt;&lt;P&gt;Nir.&lt;/P&gt;</description>
      <pubDate>Thu, 01 Dec 2022 13:03:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Poor-ping-performance-i-MX-8M-Plus/m-p/1562838#M198245</guid>
      <dc:creator>NG_R3</dc:creator>
      <dc:date>2022-12-01T13:03:39Z</dc:date>
    </item>
    <item>
      <title>Re: Poor ping performance - i.MX 8M Plus</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Poor-ping-performance-i-MX-8M-Plus/m-p/1568846#M198672</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I did some ping tests on the NXP i.mx8m-plus EVK with realtime edge 2.2.0. Numbers are average over 500 pings&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;ETH0 - 1.162ms&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;ETH1 - 0.312ms&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Any comment on this issue would be great.&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Nir.&lt;/P&gt;</description>
      <pubDate>Tue, 13 Dec 2022 11:14:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Poor-ping-performance-i-MX-8M-Plus/m-p/1568846#M198672</guid>
      <dc:creator>NG_R3</dc:creator>
      <dc:date>2022-12-13T11:14:53Z</dc:date>
    </item>
    <item>
      <title>Re: Poor ping performance - i.MX 8M Plus</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Poor-ping-performance-i-MX-8M-Plus/m-p/1569265#M198718</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/204193"&gt;@NG_R3&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;The ENTE_QoS is assigned to eth1 instance. O&lt;/SPAN&gt;nly eth1 support TSN feature, you can refer this knowledge base:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/AVB-TSN-demo-on-i-MX8MP/ta-p/1123791" target="_blank"&gt;https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/AVB-TSN-demo-on-i-MX8MP/ta-p/1123791&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;The&amp;nbsp;&lt;SPAN&gt;ENET_QoS IP about eth1 support hardware&amp;nbsp;multi-queue and&amp;nbsp;traffic control&amp;nbsp;.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 14 Dec 2022 01:26:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Poor-ping-performance-i-MX-8M-Plus/m-p/1569265#M198718</guid>
      <dc:creator>Zhiming_Liu</dc:creator>
      <dc:date>2022-12-14T01:26:03Z</dc:date>
    </item>
    <item>
      <title>Re: Poor ping performance - i.MX 8M Plus</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Poor-ping-performance-i-MX-8M-Plus/m-p/1569477#M198735</link>
      <description>&lt;P&gt;Hi Qmiller,&lt;/P&gt;&lt;P&gt;Thanks for your reply. I understand that ENET_QoS is attached to eth1, but my question regards eth0.&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I did some ping tests on the NXP i.mx8m-plus EVK with realtime edge 2.2.0.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;ETH0 - 1.162ms&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;ETH1 - 0.312ms&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;These numbers are similar on any i.MX8M Plus device that I could test. Custom boards and NXP's own EVK, running NXP's realtime edge.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Why is eth0 ping time double than eth1?&lt;/P&gt;&lt;P&gt;What can I do in order to achieve better performance with eth0?&lt;/P&gt;&lt;P&gt;Thanks a lot,&lt;/P&gt;&lt;P&gt;Nir.&lt;/P&gt;</description>
      <pubDate>Wed, 14 Dec 2022 07:59:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Poor-ping-performance-i-MX-8M-Plus/m-p/1569477#M198735</guid>
      <dc:creator>NG_R3</dc:creator>
      <dc:date>2022-12-14T07:59:16Z</dc:date>
    </item>
  </channel>
</rss>