<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic i.MX8QXP C0 MEK; 'USB Root Hub' device does not appear in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8QXP-C0-MEK-USB-Root-Hub-device-does-not-appear/m-p/1567941#M198609</link>
    <description>&lt;P&gt;I bought a i.MX8QXP MEK evaluation board from NXP.&lt;BR /&gt;I fused the image provided by NXP and am testing USB related functions.&lt;BR /&gt;It is using the kernel, DTB, and root filesystem as provided by NXP, but there are a few problems:&lt;/P&gt;&lt;H3&gt;A. The 'USB Root Hub' device does not appear&lt;/H3&gt;&lt;P&gt;On my i.MX8M Mini Board, with no USB device connected, I get this message:&lt;/P&gt;&lt;PRE&gt;# lsusb&lt;BR /&gt;Bus 001 Device 001: ID 1d6b:0002 Linux Foundation 2.0 root hub&lt;/PRE&gt;&lt;P&gt;However, no message is displayed on the MEK board.&lt;/P&gt;&lt;H3&gt;B. modprobe g_ether&lt;/H3&gt;&lt;P&gt;An error message appears when loading the USB Gadget driver.&lt;BR /&gt;Modules are loaded, but Ethernet devices such as usb0 do not appear.&lt;/P&gt;&lt;PRE&gt;root@imx8qxpc0mek:~# modprobe g_ether&lt;BR /&gt;[ 1929.547702] udc-core: couldn't find an available UDC - added [g_ether] to list of pending drivers&lt;/PRE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;H3&gt;Environment:&lt;/H3&gt;&lt;P&gt;-Linux Kernel 5.15.52+g36363d8623ba&lt;BR /&gt;-imx8qxp-mek.dtb&lt;/P&gt;&lt;P&gt;root@imx8qxpc0mek:~# uname -a&lt;BR /&gt;Linux imx8qxpc0mek 5.15.52+g36363d8623ba #1 SMP PREEMPT Tue Sep 6 09:50:50 UTC 2022 aarch64 GNU/Linux&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;We really need your help.&lt;/P&gt;</description>
    <pubDate>Mon, 12 Dec 2022 05:43:33 GMT</pubDate>
    <dc:creator>ellabyoon</dc:creator>
    <dc:date>2022-12-12T05:43:33Z</dc:date>
    <item>
      <title>i.MX8QXP C0 MEK; 'USB Root Hub' device does not appear</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8QXP-C0-MEK-USB-Root-Hub-device-does-not-appear/m-p/1567941#M198609</link>
      <description>&lt;P&gt;I bought a i.MX8QXP MEK evaluation board from NXP.&lt;BR /&gt;I fused the image provided by NXP and am testing USB related functions.&lt;BR /&gt;It is using the kernel, DTB, and root filesystem as provided by NXP, but there are a few problems:&lt;/P&gt;&lt;H3&gt;A. The 'USB Root Hub' device does not appear&lt;/H3&gt;&lt;P&gt;On my i.MX8M Mini Board, with no USB device connected, I get this message:&lt;/P&gt;&lt;PRE&gt;# lsusb&lt;BR /&gt;Bus 001 Device 001: ID 1d6b:0002 Linux Foundation 2.0 root hub&lt;/PRE&gt;&lt;P&gt;However, no message is displayed on the MEK board.&lt;/P&gt;&lt;H3&gt;B. modprobe g_ether&lt;/H3&gt;&lt;P&gt;An error message appears when loading the USB Gadget driver.&lt;BR /&gt;Modules are loaded, but Ethernet devices such as usb0 do not appear.&lt;/P&gt;&lt;PRE&gt;root@imx8qxpc0mek:~# modprobe g_ether&lt;BR /&gt;[ 1929.547702] udc-core: couldn't find an available UDC - added [g_ether] to list of pending drivers&lt;/PRE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;H3&gt;Environment:&lt;/H3&gt;&lt;P&gt;-Linux Kernel 5.15.52+g36363d8623ba&lt;BR /&gt;-imx8qxp-mek.dtb&lt;/P&gt;&lt;P&gt;root@imx8qxpc0mek:~# uname -a&lt;BR /&gt;Linux imx8qxpc0mek 5.15.52+g36363d8623ba #1 SMP PREEMPT Tue Sep 6 09:50:50 UTC 2022 aarch64 GNU/Linux&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;We really need your help.&lt;/P&gt;</description>
      <pubDate>Mon, 12 Dec 2022 05:43:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8QXP-C0-MEK-USB-Root-Hub-device-does-not-appear/m-p/1567941#M198609</guid>
      <dc:creator>ellabyoon</dc:creator>
      <dc:date>2022-12-12T05:43:33Z</dc:date>
    </item>
  </channel>
</rss>