<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Error when building yocto image on docker container in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Error-when-building-yocto-image-on-docker-container/m-p/1567078#M198532</link>
    <description>&lt;P&gt;I set up a docker container following the &lt;A href="https://github.com/crops/docker-win-mac-docs/wiki/Windows-Instructions-%28Docker-Toolbox%29" target="_self"&gt;Yocto project instructions&lt;/A&gt;. This environment has Ubuntu 18.04 bionic, which should work for image generation (unlike 20.04), it worked perfectly for the basic poky image building.&lt;BR /&gt;Then, following &lt;A href="https://www.nxp.com/docs/en/user-guide/IMX_YOCTO_PROJECT_USERS_GUIDE.pdf" target="_self"&gt;i.MX's BSP instructions&lt;/A&gt;&amp;nbsp;I am trying to build the imx-image-full for the i.MX7ULP board.&lt;BR /&gt;But, when I am doing the build I get this error after 1753 tasks:&lt;BR /&gt;&lt;BR /&gt;&lt;EM&gt;ERROR: Task (virtual:native:/workdir/imx-yocto-bsp/sources/meta-qt6/recipes-qt/qt6/qtbase_git.bb:do_compile) failed with exit code '1'&lt;/EM&gt;&lt;BR /&gt;&lt;BR /&gt;I do not understand the error, and even less how to solve it. I downloaded their required host build packages and set up the .sh file correctly...&lt;BR /&gt;&lt;BR /&gt;I have not found any entry on this error either, and I would like to know if there is a way to work around this error or if I should give up on using that environment and I should set up a&amp;nbsp;&lt;A href="https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/Create-an-Ubuntu-VM-environment-to-build-Yocto-BSP/ta-p/1103589" target="_self"&gt;VM&lt;/A&gt;&amp;nbsp;or a &lt;A href="https://github.com/nxp-imx/imx-docker" target="_self"&gt;different environment using Docker&lt;/A&gt;&amp;nbsp;(which I would like to avoid).&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
    <pubDate>Thu, 08 Dec 2022 21:20:52 GMT</pubDate>
    <dc:creator>alvmarti</dc:creator>
    <dc:date>2022-12-08T21:20:52Z</dc:date>
    <item>
      <title>Error when building yocto image on docker container</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Error-when-building-yocto-image-on-docker-container/m-p/1567078#M198532</link>
      <description>&lt;P&gt;I set up a docker container following the &lt;A href="https://github.com/crops/docker-win-mac-docs/wiki/Windows-Instructions-%28Docker-Toolbox%29" target="_self"&gt;Yocto project instructions&lt;/A&gt;. This environment has Ubuntu 18.04 bionic, which should work for image generation (unlike 20.04), it worked perfectly for the basic poky image building.&lt;BR /&gt;Then, following &lt;A href="https://www.nxp.com/docs/en/user-guide/IMX_YOCTO_PROJECT_USERS_GUIDE.pdf" target="_self"&gt;i.MX's BSP instructions&lt;/A&gt;&amp;nbsp;I am trying to build the imx-image-full for the i.MX7ULP board.&lt;BR /&gt;But, when I am doing the build I get this error after 1753 tasks:&lt;BR /&gt;&lt;BR /&gt;&lt;EM&gt;ERROR: Task (virtual:native:/workdir/imx-yocto-bsp/sources/meta-qt6/recipes-qt/qt6/qtbase_git.bb:do_compile) failed with exit code '1'&lt;/EM&gt;&lt;BR /&gt;&lt;BR /&gt;I do not understand the error, and even less how to solve it. I downloaded their required host build packages and set up the .sh file correctly...&lt;BR /&gt;&lt;BR /&gt;I have not found any entry on this error either, and I would like to know if there is a way to work around this error or if I should give up on using that environment and I should set up a&amp;nbsp;&lt;A href="https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/Create-an-Ubuntu-VM-environment-to-build-Yocto-BSP/ta-p/1103589" target="_self"&gt;VM&lt;/A&gt;&amp;nbsp;or a &lt;A href="https://github.com/nxp-imx/imx-docker" target="_self"&gt;different environment using Docker&lt;/A&gt;&amp;nbsp;(which I would like to avoid).&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 08 Dec 2022 21:20:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Error-when-building-yocto-image-on-docker-container/m-p/1567078#M198532</guid>
      <dc:creator>alvmarti</dc:creator>
      <dc:date>2022-12-08T21:20:52Z</dc:date>
    </item>
    <item>
      <title>Re: Error when building yocto image on docker container</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Error-when-building-yocto-image-on-docker-container/m-p/1567533#M198575</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;The yocto bsp doesn't include qt6 for MX7, at least you are using L5.15.52 BSP.&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 09 Dec 2022 13:41:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Error-when-building-yocto-image-on-docker-container/m-p/1567533#M198575</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2022-12-09T13:41:01Z</dc:date>
    </item>
    <item>
      <title>Re: Error when building yocto image on docker container</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Error-when-building-yocto-image-on-docker-container/m-p/1567561#M198579</link>
      <description>So, if I am using "imx-5.15.52-2.1.0.xml" as BSP from the manifest, is it normal that I do not have QT6 for the IMX7ULP?&lt;BR /&gt;In the i.mx's yocto project user guide it says that imx-image-full doesn't work for IMX7DUAL but it doesn't say anything about IMX7ULP.&lt;BR /&gt;</description>
      <pubDate>Fri, 09 Dec 2022 14:40:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Error-when-building-yocto-image-on-docker-container/m-p/1567561#M198579</guid>
      <dc:creator>alvmarti</dc:creator>
      <dc:date>2022-12-09T14:40:43Z</dc:date>
    </item>
  </channel>
</rss>