<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Not able to get HDMI interface while booting through TFTP/NFS or SD card boot procedure</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Not-able-to-get-HDMI-interface-while-booting-through-TFTP-NFS-or/m-p/1566495#M198482</link>
    <description>&lt;P&gt;could you reproduce this on nxp imx6 board? I can get HDMI interface from sd card boot on nxp imx6q sdb baord before, since you used the third party board, pls contact them to get further help&lt;/P&gt;</description>
    <pubDate>Thu, 08 Dec 2022 03:19:41 GMT</pubDate>
    <dc:creator>joanxie</dc:creator>
    <dc:date>2022-12-08T03:19:41Z</dc:date>
    <item>
      <title>Not able to get HDMI interface while booting through TFTP/NFS or SD card boot procedure</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Not-able-to-get-HDMI-interface-while-booting-through-TFTP-NFS-or/m-p/1564171#M198317</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am working on Apalis 1.1v IMX 6 board which is placed on Ixora carrier board with Embedded linux BSP version 5 , initially&amp;nbsp; I tried booting board using Toradex easy installer here I am able to get HDMI interface by default, but when i tried to boot from TFTP/NFS or SD card boot procedures I am not able to get HDMI interface, tried copying overlays folder and overlays.txt file along with kernel and dtb files, though I am not able to get&amp;nbsp; HDMI interface,I am not able to find HDMI interface dmesg logs also.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Please suggest me the procedure to bring up HDMI interface with TFTP/NFS or SD card boot procedures,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;With Regards,&lt;/P&gt;&lt;P&gt;-Vamsi.&lt;/P&gt;</description>
      <pubDate>Mon, 05 Dec 2022 07:15:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Not-able-to-get-HDMI-interface-while-booting-through-TFTP-NFS-or/m-p/1564171#M198317</guid>
      <dc:creator>vamsi92</dc:creator>
      <dc:date>2022-12-05T07:15:24Z</dc:date>
    </item>
    <item>
      <title>Re: Not able to get HDMI interface while booting through TFTP/NFS or SD card boot procedure</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Not-able-to-get-HDMI-interface-while-booting-through-TFTP-NFS-or/m-p/1566495#M198482</link>
      <description>&lt;P&gt;could you reproduce this on nxp imx6 board? I can get HDMI interface from sd card boot on nxp imx6q sdb baord before, since you used the third party board, pls contact them to get further help&lt;/P&gt;</description>
      <pubDate>Thu, 08 Dec 2022 03:19:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Not-able-to-get-HDMI-interface-while-booting-through-TFTP-NFS-or/m-p/1566495#M198482</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2022-12-08T03:19:41Z</dc:date>
    </item>
  </channel>
</rss>