<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Driving LEDs with iMXRT1064 in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Driving-LEDs-with-iMXRT1064/m-p/1565994#M198461</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I want to connect 8 LEDs (4mA each, 32mA total) directly to GPIO pins.&lt;BR /&gt;Is it possible?&lt;BR /&gt;or it should be necessary to add a driver?&lt;/P&gt;&lt;P&gt;I couldn't find the total maximum current in the datasheet. The only information is the maximum current of a pin, +/-4mA depending on the&amp;nbsp;ipp_dse value.&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 07 Dec 2022 15:06:43 GMT</pubDate>
    <dc:creator>etronic_arg</dc:creator>
    <dc:date>2022-12-07T15:06:43Z</dc:date>
    <item>
      <title>Driving LEDs with iMXRT1064</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Driving-LEDs-with-iMXRT1064/m-p/1565994#M198461</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I want to connect 8 LEDs (4mA each, 32mA total) directly to GPIO pins.&lt;BR /&gt;Is it possible?&lt;BR /&gt;or it should be necessary to add a driver?&lt;/P&gt;&lt;P&gt;I couldn't find the total maximum current in the datasheet. The only information is the maximum current of a pin, +/-4mA depending on the&amp;nbsp;ipp_dse value.&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 07 Dec 2022 15:06:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Driving-LEDs-with-iMXRT1064/m-p/1565994#M198461</guid>
      <dc:creator>etronic_arg</dc:creator>
      <dc:date>2022-12-07T15:06:43Z</dc:date>
    </item>
    <item>
      <title>Re: Driving LEDs with iMXRT1064</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Driving-LEDs-with-iMXRT1064/m-p/1566650#M198503</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Pls refer to table 22 in the data sheet of i.mxrt1060, the current of each I/O cell in push/pull output mode is +/-1mA(sink/source current), so you have to connect a transistor or mosfet to drive led if it requires 4mA current.&lt;/P&gt;
&lt;P&gt;Hope it can help you&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="xiangjun_rong_0-1670484942313.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/203582i0E88471AC0F4DB63/image-size/medium?v=v2&amp;amp;px=400" role="button" title="xiangjun_rong_0-1670484942313.png" alt="xiangjun_rong_0-1670484942313.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;xiangjun_rong_0-1670484942313.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 08 Dec 2022 07:40:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Driving-LEDs-with-iMXRT1064/m-p/1566650#M198503</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2022-12-08T07:40:38Z</dc:date>
    </item>
  </channel>
</rss>