<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: iMX6 SPI SS difference in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX6-SPI-SS-difference/m-p/240104#M19843</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Can you share the IOMUX setting about pins of SPI3? Such as:&lt;/P&gt;&lt;P&gt;/* ECSPI1 */&lt;/P&gt;&lt;P&gt;        MX6Q_PAD_KEY_COL0__ECSPI1_SCLK,&lt;/P&gt;&lt;P&gt;        MX6Q_PAD_KEY_ROW0__ECSPI1_MOSI,&lt;/P&gt;&lt;P&gt;        MX6Q_PAD_KEY_COL1__ECSPI1_MISO,&lt;/P&gt;&lt;P&gt;        MX6Q_PAD_KEY_ROW1__GPIO_4_9,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 03 Jul 2013 08:31:17 GMT</pubDate>
    <dc:creator>RobinGong</dc:creator>
    <dc:date>2013-07-03T08:31:17Z</dc:date>
    <item>
      <title>iMX6 SPI SS difference</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6-SPI-SS-difference/m-p/240101#M19840</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;BR /&gt;We have 2 ECSPI interfaces configured on our iMX6 quad core SPI2 and SPI3. We want to read&amp;nbsp; 96 bytes in on the MISO line. This works fine on SPI2 - the SS stays low for the duration of the read. On SPI3 SS goes high between each byte. Our SPI drivers are identical, as far as we can tell. Is there any difference between the SPI interfaces on the chip?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 26 Jun 2013 12:30:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6-SPI-SS-difference/m-p/240101#M19840</guid>
      <dc:creator>cliverolston</dc:creator>
      <dc:date>2013-06-26T12:30:28Z</dc:date>
    </item>
    <item>
      <title>Re: iMX6 SPI SS difference</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6-SPI-SS-difference/m-p/240102#M19841</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Please take care of that SS pin should be configured GPIO output(arch/arm/mach-mx6/board-mx6q_sabresd.h). And should tell the GPIO number to SPI driver in board file , such as below code in arch/arm/mach-mx6/board-mx6q_sabresd.c&lt;/P&gt;&lt;P&gt;static int mx6q_sabresd_spi_cs[] = {&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; SABRESD_ECSPI1_CS0,&lt;/P&gt;&lt;P&gt;};&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;static const struct spi_imx_master mx6q_sabresd_spi_data __initconst = {&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; .chipselect&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; = mx6q_sabresd_spi_cs,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; .num_chipselect = ARRAY_SIZE(mx6q_sabresd_spi_cs),&lt;/P&gt;&lt;P&gt;};&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 03 Jul 2013 04:48:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6-SPI-SS-difference/m-p/240102#M19841</guid>
      <dc:creator>RobinGong</dc:creator>
      <dc:date>2013-07-03T04:48:19Z</dc:date>
    </item>
    <item>
      <title>Re: iMX6 SPI SS difference</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6-SPI-SS-difference/m-p/240103#M19842</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks Yibin,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We've tried this already but we're still having problems with SPI3.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Cheers,&lt;/P&gt;&lt;P&gt;Clive&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 03 Jul 2013 08:20:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6-SPI-SS-difference/m-p/240103#M19842</guid>
      <dc:creator>cliverolston</dc:creator>
      <dc:date>2013-07-03T08:20:35Z</dc:date>
    </item>
    <item>
      <title>Re: iMX6 SPI SS difference</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6-SPI-SS-difference/m-p/240104#M19843</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Can you share the IOMUX setting about pins of SPI3? Such as:&lt;/P&gt;&lt;P&gt;/* ECSPI1 */&lt;/P&gt;&lt;P&gt;        MX6Q_PAD_KEY_COL0__ECSPI1_SCLK,&lt;/P&gt;&lt;P&gt;        MX6Q_PAD_KEY_ROW0__ECSPI1_MOSI,&lt;/P&gt;&lt;P&gt;        MX6Q_PAD_KEY_COL1__ECSPI1_MISO,&lt;/P&gt;&lt;P&gt;        MX6Q_PAD_KEY_ROW1__GPIO_4_9,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 03 Jul 2013 08:31:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6-SPI-SS-difference/m-p/240104#M19843</guid>
      <dc:creator>RobinGong</dc:creator>
      <dc:date>2013-07-03T08:31:17Z</dc:date>
    </item>
  </channel>
</rss>