<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: How to make hyperram connected with flexspi2 work like SDRAM in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/How-to-make-hyperram-connected-with-flexspi2-work-like-SDRAM/m-p/1565486#M198421</link>
    <description>&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/169053"&gt;@Omar_Anguiano&lt;/a&gt; Thanks for reply. So I should use the AHB bus memory space access: 0x6000_0000 – 0x6FFF_FFFF for hyperram with flexspi2, is it right? Thanks.</description>
    <pubDate>Wed, 07 Dec 2022 01:21:50 GMT</pubDate>
    <dc:creator>yalin</dc:creator>
    <dc:date>2022-12-07T01:21:50Z</dc:date>
    <item>
      <title>How to make hyperram connected with flexspi2 work like SDRAM</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-make-hyperram-connected-with-flexspi2-work-like-SDRAM/m-p/1562732#M198241</link>
      <description>&lt;P&gt;We'd like to use hyperram&amp;nbsp;S27KS0642GA to replace SDRAM on RT1176, I researched some cases in this community and found AN12239.pdf, which showed how to read and write hyperram, I think it is a way using hyperram like a external device driver, such as an I2C device.&lt;/P&gt;&lt;P&gt;However, I'd like to use it by adding it into the MCU settings list in IDE just like SDRAM, is it possible? How can I do that? Is there a whole document or reference for configuring and using it?&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;</description>
      <pubDate>Thu, 01 Dec 2022 09:43:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-make-hyperram-connected-with-flexspi2-work-like-SDRAM/m-p/1562732#M198241</guid>
      <dc:creator>yalin</dc:creator>
      <dc:date>2022-12-01T09:43:11Z</dc:date>
    </item>
    <item>
      <title>Re: How to make hyperram connected with flexspi2 work like SDRAM</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-make-hyperram-connected-with-flexspi2-work-like-SDRAM/m-p/1565475#M198420</link>
      <description>&lt;P&gt;Hello&lt;BR /&gt;Hope you are well.&lt;/P&gt;
&lt;P&gt;Yes, it can be done in the same. You need to specify in the MCU settings the address where your HyperRAM is located so it becomes available.&lt;BR /&gt;I believe that what you want to do is access that HyperRAM through AHB bus so it is important to verify where it is mapped.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Omar_Anguiano_0-1670374011847.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/203265i74781587CFA45A34/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Omar_Anguiano_0-1670374011847.png" alt="Omar_Anguiano_0-1670374011847.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Omar&lt;/P&gt;</description>
      <pubDate>Wed, 07 Dec 2022 00:47:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-make-hyperram-connected-with-flexspi2-work-like-SDRAM/m-p/1565475#M198420</guid>
      <dc:creator>Omar_Anguiano</dc:creator>
      <dc:date>2022-12-07T00:47:09Z</dc:date>
    </item>
    <item>
      <title>Re: How to make hyperram connected with flexspi2 work like SDRAM</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-make-hyperram-connected-with-flexspi2-work-like-SDRAM/m-p/1565486#M198421</link>
      <description>&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/169053"&gt;@Omar_Anguiano&lt;/a&gt; Thanks for reply. So I should use the AHB bus memory space access: 0x6000_0000 – 0x6FFF_FFFF for hyperram with flexspi2, is it right? Thanks.</description>
      <pubDate>Wed, 07 Dec 2022 01:21:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-make-hyperram-connected-with-flexspi2-work-like-SDRAM/m-p/1565486#M198421</guid>
      <dc:creator>yalin</dc:creator>
      <dc:date>2022-12-07T01:21:50Z</dc:date>
    </item>
    <item>
      <title>Re: How to make hyperram connected with flexspi2 work like SDRAM</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-make-hyperram-connected-with-flexspi2-work-like-SDRAM/m-p/1566092#M198467</link>
      <description>&lt;P&gt;You're correct, that space address needs to be used. &lt;BR /&gt;Once you have it on memory settings it is also important to first initialize it before using it.&lt;BR /&gt;One example that might be helpful is the PSRAM example on the RT600, although it is a different device it can be helpful since it accesses the FlexSPI RAM through AHB bus.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Omar&lt;/P&gt;</description>
      <pubDate>Wed, 07 Dec 2022 17:29:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-make-hyperram-connected-with-flexspi2-work-like-SDRAM/m-p/1566092#M198467</guid>
      <dc:creator>Omar_Anguiano</dc:creator>
      <dc:date>2022-12-07T17:29:07Z</dc:date>
    </item>
  </channel>
</rss>