<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic HOW TO ACTIVE PWM AT RT1050 in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/HOW-TO-ACTIVE-PWM-AT-RT1050/m-p/1560840#M198116</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;Im using a SDK example called evkbmimxrt1050_pwm, so i get the 3 signals that the example made but when i want to add another pin , i does not work. I configured my pin firts in the configtools in the part called Pins, then in the code i add some lines like which PWM i want to use in my case is the number 2,then i also add some code to active the sub module number 3. I used the same things that the example use just i modified the number of sub module that i want to use and the channel. the output at the pin does not work but in the others is works well.&lt;/P&gt;&lt;P&gt;thanks for all.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 01 Dec 2022 16:42:49 GMT</pubDate>
    <dc:creator>Jimmywder03</dc:creator>
    <dc:date>2022-12-01T16:42:49Z</dc:date>
    <item>
      <title>HOW TO ACTIVE PWM AT RT1050</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/HOW-TO-ACTIVE-PWM-AT-RT1050/m-p/1560840#M198116</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;Im using a SDK example called evkbmimxrt1050_pwm, so i get the 3 signals that the example made but when i want to add another pin , i does not work. I configured my pin firts in the configtools in the part called Pins, then in the code i add some lines like which PWM i want to use in my case is the number 2,then i also add some code to active the sub module number 3. I used the same things that the example use just i modified the number of sub module that i want to use and the channel. the output at the pin does not work but in the others is works well.&lt;/P&gt;&lt;P&gt;thanks for all.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 01 Dec 2022 16:42:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/HOW-TO-ACTIVE-PWM-AT-RT1050/m-p/1560840#M198116</guid>
      <dc:creator>Jimmywder03</dc:creator>
      <dc:date>2022-12-01T16:42:49Z</dc:date>
    </item>
    <item>
      <title>Re: HOW TO ACTIVE PWM AT RT1050</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/HOW-TO-ACTIVE-PWM-AT-RT1050/m-p/1561573#M198158</link>
      <description>&lt;P&gt;There is most likely an error with the configuration code you add for the 4th signal.&lt;/P&gt;
&lt;P&gt;Instead of using Pins tool and adding the extra code manually, I recommend you to use the Peripherals tool, under ConfigTools, to set up the configuration of the PWM module as a whole with all of the signals you require. You should be able to do the setup of each submodule in a more straightforward manner, and make sure the setup of each submodule is the same. Here I added all 4 submodules by simply clicking the "+" button beside the "Submodules" section, and set up each as PWM.&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="EdwinHz_0-1669762028255.png" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/202166i6B9347C130548A4D/image-size/large?v=v2&amp;amp;px=999" role="button" title="EdwinHz_0-1669762028255.png" alt="EdwinHz_0-1669762028255.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;EdwinHz_0-1669762028255.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR,&lt;/P&gt;
&lt;P&gt;Edwin.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 29 Nov 2022 22:49:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/HOW-TO-ACTIVE-PWM-AT-RT1050/m-p/1561573#M198158</guid>
      <dc:creator>EdwinHz</dc:creator>
      <dc:date>2022-11-29T22:49:03Z</dc:date>
    </item>
    <item>
      <title>Re: HOW TO ACTIVE PWM AT RT1050</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/HOW-TO-ACTIVE-PWM-AT-RT1050/m-p/1562939#M198255</link>
      <description>&lt;P&gt;Hello Edwin,&lt;/P&gt;&lt;P&gt;I have tried that way and it does not work.&lt;/P&gt;&lt;P&gt;Look, first I created a new project and I add the PWM driver then I went to &lt;SPAN&gt;Peripherals tool and I actived it. After that at&amp;nbsp;Peripherals tool I choose PWM2 to use it, then I used the same configuration that you showed me in the picture just I have different the pin that I want to test. I confirm that the pin that i want support PWM2 and it is Channel A submodule 3 (You will see in the picture that I set well that configuration). Then I load that project to my IMXRT1052 EVK I looked that pin to see the signal in the osciloscope and it does not work.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Thank you for you attandance.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 01 Dec 2022 16:42:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/HOW-TO-ACTIVE-PWM-AT-RT1050/m-p/1562939#M198255</guid>
      <dc:creator>Jimmywder03</dc:creator>
      <dc:date>2022-12-01T16:42:31Z</dc:date>
    </item>
    <item>
      <title>Re: HOW TO ACTIVE PWM AT RT1050</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/HOW-TO-ACTIVE-PWM-AT-RT1050/m-p/1562943#M198256</link>
      <description>&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="pwm1.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/202467iA1B288BD8F66FE34/image-size/medium?v=v2&amp;amp;px=400" role="button" title="pwm1.png" alt="pwm1.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;pwm1.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="pwm2.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/202468iBE419602DB2943CE/image-size/medium?v=v2&amp;amp;px=400" role="button" title="pwm2.png" alt="pwm2.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;pwm2.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt; &lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="pwm3.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/202469iCF04C13CC89A2A09/image-size/medium?v=v2&amp;amp;px=400" role="button" title="pwm3.png" alt="pwm3.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;pwm3.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;  &lt;/P&gt;</description>
      <pubDate>Thu, 01 Dec 2022 16:41:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/HOW-TO-ACTIVE-PWM-AT-RT1050/m-p/1562943#M198256</guid>
      <dc:creator>Jimmywder03</dc:creator>
      <dc:date>2022-12-01T16:41:01Z</dc:date>
    </item>
  </channel>
</rss>