<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックWhen I add sd peripheral and freeRtos, the generated code not compile.</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/When-I-add-sd-peripheral-and-freeRtos-the-generated-code-not/m-p/1557367#M197786</link>
    <description>&lt;P&gt;I'm using i.MXRT1052 mcu with Expresso IDE.&amp;nbsp;&lt;BR /&gt;SDK version is 2.12.0.&lt;BR /&gt;&lt;BR /&gt;When I add sd peripheral and freeRtos, the generated code not compile.&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;It's because the os abstraction doens't merge with freeRTOS abstraction, so thats files come into conflict.&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;Check the image&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
    <pubDate>Mon, 21 Nov 2022 22:26:31 GMT</pubDate>
    <dc:creator>Yerih</dc:creator>
    <dc:date>2022-11-21T22:26:31Z</dc:date>
    <item>
      <title>When I add sd peripheral and freeRtos, the generated code not compile.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/When-I-add-sd-peripheral-and-freeRtos-the-generated-code-not/m-p/1557367#M197786</link>
      <description>&lt;P&gt;I'm using i.MXRT1052 mcu with Expresso IDE.&amp;nbsp;&lt;BR /&gt;SDK version is 2.12.0.&lt;BR /&gt;&lt;BR /&gt;When I add sd peripheral and freeRtos, the generated code not compile.&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;It's because the os abstraction doens't merge with freeRTOS abstraction, so thats files come into conflict.&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;Check the image&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 21 Nov 2022 22:26:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/When-I-add-sd-peripheral-and-freeRtos-the-generated-code-not/m-p/1557367#M197786</guid>
      <dc:creator>Yerih</dc:creator>
      <dc:date>2022-11-21T22:26:31Z</dc:date>
    </item>
    <item>
      <title>Re: When I add sd peripheral and freeRtos, the generated code not compile.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/When-I-add-sd-peripheral-and-freeRtos-the-generated-code-not/m-p/1558392#M197892</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/205729"&gt;@Yerih&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;There is&amp;nbsp; sdio_freertos example in&amp;nbsp;SDK_2_12_0_MIMXRT1050-EVK\boards\evkmimxrt1050\driver\sdio. You can refer to it.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Jing&lt;/P&gt;</description>
      <pubDate>Wed, 23 Nov 2022 09:38:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/When-I-add-sd-peripheral-and-freeRtos-the-generated-code-not/m-p/1558392#M197892</guid>
      <dc:creator>jingpan</dc:creator>
      <dc:date>2022-11-23T09:38:29Z</dc:date>
    </item>
  </channel>
</rss>