<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic SNVS Coin cell voltage read in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/SNVS-Coin-cell-voltage-read/m-p/1554059#M197576</link>
    <description>&lt;P&gt;Hi NXP Team,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;We are using the iMX6sX processor which have SNVS functionality enabled and everything is up and running,&lt;/P&gt;&lt;P&gt;But we have one requirement to read the coin cell voltage if it is low,&lt;/P&gt;&lt;P&gt;Is there any registers or method available to read the voltage or generate trigger so user may aware about to change the coin cell battery.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
    <pubDate>Tue, 15 Nov 2022 12:02:17 GMT</pubDate>
    <dc:creator>kevi49</dc:creator>
    <dc:date>2022-11-15T12:02:17Z</dc:date>
    <item>
      <title>SNVS Coin cell voltage read</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SNVS-Coin-cell-voltage-read/m-p/1554059#M197576</link>
      <description>&lt;P&gt;Hi NXP Team,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;We are using the iMX6sX processor which have SNVS functionality enabled and everything is up and running,&lt;/P&gt;&lt;P&gt;But we have one requirement to read the coin cell voltage if it is low,&lt;/P&gt;&lt;P&gt;Is there any registers or method available to read the voltage or generate trigger so user may aware about to change the coin cell battery.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
      <pubDate>Tue, 15 Nov 2022 12:02:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SNVS-Coin-cell-voltage-read/m-p/1554059#M197576</guid>
      <dc:creator>kevi49</dc:creator>
      <dc:date>2022-11-15T12:02:17Z</dc:date>
    </item>
    <item>
      <title>Re: SNVS Coin cell voltage read</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SNVS-Coin-cell-voltage-read/m-p/1556979#M197750</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/201491"&gt;@kevi49&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;As far as I know that you can u&lt;SPAN&gt;se a voltmeter to measure.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Best regards&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Harvey&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 21 Nov 2022 07:31:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SNVS-Coin-cell-voltage-read/m-p/1556979#M197750</guid>
      <dc:creator>Harvey021</dc:creator>
      <dc:date>2022-11-21T07:31:00Z</dc:date>
    </item>
    <item>
      <title>Re: SNVS Coin cell voltage read</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SNVS-Coin-cell-voltage-read/m-p/1557112#M197762</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/201491"&gt;@kevi49&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;You could use an ADC input and put together a small program or script that polls the ADC line. After a bit of conversion to get what the ADC is reading in volts or millivolts then you can set a trigger point to alert the user etc. Depending what you hardware is i.e if you're on a dev board you may have some preconfigured ADC inputs, if not see if you can find a suitable spare pin on your board. Do the normal device tree, and kernel configs and then a simple 'cat /sys/bus/iio/devices/iio:device0/in_voltage1_raw' (or similar) will show it's working. Connect it to your battery line somehow with suitable resistive dividers etc and you might be in business!&lt;/P&gt;&lt;P&gt;Hope it helps.&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 21 Nov 2022 10:47:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SNVS-Coin-cell-voltage-read/m-p/1557112#M197762</guid>
      <dc:creator>edwardtyrrell</dc:creator>
      <dc:date>2022-11-21T10:47:01Z</dc:date>
    </item>
  </channel>
</rss>