<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Xen Hypervisor Multiple Images loading is not working</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Xen-Hypervisor-Multiple-Images-loading-is-not-working/m-p/1553374#M197530</link>
    <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/189361"&gt;@mallibeerala&lt;/a&gt;,&lt;/P&gt;&lt;P&gt;I am also trying to bring up similar thing.&lt;/P&gt;&lt;P&gt;Can you let me know from where do you get "L_VIRT_4.14.98_2.0.0_4.11_0.10_ga_images_MX8QMMEK.zip"? I am unable to locate it.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Ranadip&lt;/P&gt;</description>
    <pubDate>Mon, 14 Nov 2022 14:57:01 GMT</pubDate>
    <dc:creator>Ranadip</dc:creator>
    <dc:date>2022-11-14T14:57:01Z</dc:date>
    <item>
      <title>Xen Hypervisor Multiple Images loading is not working</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Xen-Hypervisor-Multiple-Images-loading-is-not-working/m-p/1340654#M180148</link>
      <description>&lt;P&gt;Dear NXP Team,&lt;/P&gt;&lt;P&gt;I am working on xen hypervisor, for that I downloaded "L_VIRT_4.14.98_2.0.0_4.11_0.10_ga_images_MX8QMMEK" Image from NXP site, and it is working fine and I am able connect to &lt;STRONG&gt;DomU&lt;/STRONG&gt; console by using &lt;STRONG&gt;xl console DomU.&lt;/STRONG&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Now I loaded &lt;STRONG&gt;LF_v5.10_2.0.0_images_IMX8QMMEK &lt;/STRONG&gt;Image in partition 5 and partition 6(extended partition) of same SD card and I am trying to connect&amp;nbsp; to LF_v5.10_2.0.0_images_IMX8QMMEK Image using command &lt;STRONG&gt;xl console Domu&lt;/STRONG&gt;, now bootup is happening but Image not loaded fully, Please find the attached document for Issue.&lt;/P&gt;&lt;P&gt;Please help me to resolve this Issue.&lt;/P&gt;&lt;P&gt;Thanks &amp;amp; Regards,&lt;/P&gt;&lt;P&gt;Mallikarjuna B.&lt;/P&gt;</description>
      <pubDate>Wed, 15 Sep 2021 13:45:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Xen-Hypervisor-Multiple-Images-loading-is-not-working/m-p/1340654#M180148</guid>
      <dc:creator>mallibeerala</dc:creator>
      <dc:date>2021-09-15T13:45:17Z</dc:date>
    </item>
    <item>
      <title>Re: Xen Hypervisor Multiple Images loading is not working</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Xen-Hypervisor-Multiple-Images-loading-is-not-working/m-p/1343280#M180407</link>
      <description>&lt;P&gt;Hello malibeerala,&lt;/P&gt;
&lt;P&gt;The issue is not with XEN is in fact with the OS that you have At boot, the kernel waits for mouse movements to initialize the random number generator.&lt;BR /&gt;Kernel messages on boot: crng init generator, you can burn again the SD for see if this happens, if happens try to fix for the external processor with installing the haveged and enable the systemctl enable haveged.&lt;/P&gt;
&lt;P&gt;Regards&lt;BR /&gt;&amp;nbsp; &lt;/P&gt;</description>
      <pubDate>Tue, 21 Sep 2021 13:03:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Xen-Hypervisor-Multiple-Images-loading-is-not-working/m-p/1343280#M180407</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2021-09-21T13:03:21Z</dc:date>
    </item>
    <item>
      <title>Re: Xen Hypervisor Multiple Images loading is not working</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Xen-Hypervisor-Multiple-Images-loading-is-not-working/m-p/1343659#M180435</link>
      <description>&lt;P&gt;Hi Bio_TICFSL,&lt;/P&gt;&lt;P&gt;I think question is misunderstood.&lt;/P&gt;&lt;P&gt;1. I want to use &lt;FONT color="#FF0000"&gt;&lt;STRONG&gt;DOM0&lt;/STRONG&gt;&lt;/FONT&gt; as L_VIRT_4.14.98_2.0.0_4.11_0.10_ga_images_MX8QMMEK and &lt;FONT color="#FF0000"&gt;&lt;STRONG&gt;DOMU&lt;/STRONG&gt;&lt;/FONT&gt; as LF_v5.10_2.0.0_images_IMX8QMMEK.&lt;/P&gt;&lt;P&gt;2. SD card have 6 partitions, DOM0 kernel, DTB files available in partition 0 and rootfs is available in partition 2.&lt;/P&gt;&lt;P&gt;DOMU kernel, DTB files available in partition 5 and rootfs is available in partition 6.&lt;/P&gt;&lt;P&gt;3. We are using common uboot of "L_VIRT_4.14.98_2.0.0_4.11_0.10_ga_images_MX8QMMEK" for loading DOMU.&lt;/P&gt;&lt;P&gt;4. We have separately tested L_VIRT_4.14.98_2.0.0_4.11_0.10_ga_images_MX8QMMEK, LF_v5.10_2.0.0_images_IMX8QMMEK then it is working fine.&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Query:&lt;/STRONG&gt;&amp;nbsp;To create multiple OS partition using xen, we are using to different kernel to replicate the same and we used uboot belongs to L_VIRT_4.14.98_2.0.0_4.11_0.10_ga_images_MX8QMMEK.&lt;/P&gt;&lt;P&gt;DOM0 is up and running, created DOMU guest but DOM0 is failing to load DOMU, please suggest how to load DOMU from DOM0. Is there any boot parameters required to load DOMU.&lt;/P&gt;&lt;P&gt;we are not using any mouse or monitor.&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Please find the attached log file.&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;Thanks &amp;amp; Regards,&lt;BR /&gt;Mallikarjuna B&lt;/P&gt;</description>
      <pubDate>Thu, 23 Sep 2021 13:49:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Xen-Hypervisor-Multiple-Images-loading-is-not-working/m-p/1343659#M180435</guid>
      <dc:creator>mallibeerala</dc:creator>
      <dc:date>2021-09-23T13:49:42Z</dc:date>
    </item>
    <item>
      <title>Re: Xen Hypervisor Multiple Images loading is not working</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Xen-Hypervisor-Multiple-Images-loading-is-not-working/m-p/1345546#M180568</link>
      <description>&lt;P&gt;Hi Bio_TICFSL,&lt;/P&gt;&lt;P&gt;Is there any other way to try loading of multiple OS Images using xen, then I will try that procedure. Please help us we are stuck here.&lt;/P&gt;</description>
      <pubDate>Fri, 24 Sep 2021 05:15:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Xen-Hypervisor-Multiple-Images-loading-is-not-working/m-p/1345546#M180568</guid>
      <dc:creator>mallibeerala</dc:creator>
      <dc:date>2021-09-24T05:15:47Z</dc:date>
    </item>
    <item>
      <title>Re: Xen Hypervisor Multiple Images loading is not working</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Xen-Hypervisor-Multiple-Images-loading-is-not-working/m-p/1553374#M197530</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/189361"&gt;@mallibeerala&lt;/a&gt;,&lt;/P&gt;&lt;P&gt;I am also trying to bring up similar thing.&lt;/P&gt;&lt;P&gt;Can you let me know from where do you get "L_VIRT_4.14.98_2.0.0_4.11_0.10_ga_images_MX8QMMEK.zip"? I am unable to locate it.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Ranadip&lt;/P&gt;</description>
      <pubDate>Mon, 14 Nov 2022 14:57:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Xen-Hypervisor-Multiple-Images-loading-is-not-working/m-p/1553374#M197530</guid>
      <dc:creator>Ranadip</dc:creator>
      <dc:date>2022-11-14T14:57:01Z</dc:date>
    </item>
    <item>
      <title>Re: Xen Hypervisor Multiple Images loading is not working</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Xen-Hypervisor-Multiple-Images-loading-is-not-working/m-p/1555499#M197648</link>
      <description>Hi Ranadip,&lt;BR /&gt;&lt;BR /&gt;You can find Image at "&lt;A href="https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applications-processors:IMXLINUX" target="_blank"&gt;https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applications-processors:IMXLINUX&lt;/A&gt;".&lt;BR /&gt;&lt;BR /&gt;Regards,&lt;BR /&gt;Mallikarjuna B.</description>
      <pubDate>Thu, 17 Nov 2022 05:14:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Xen-Hypervisor-Multiple-Images-loading-is-not-working/m-p/1555499#M197648</guid>
      <dc:creator>mallibeerala</dc:creator>
      <dc:date>2022-11-17T05:14:31Z</dc:date>
    </item>
  </channel>
</rss>