<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: camera module for MIMXRT1160-EVK</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/camera-module-for-MIMXRT1160-EVK/m-p/1552248#M197444</link>
    <description>&lt;P&gt;Hello&lt;/P&gt;
&lt;P&gt;Hope you are well.&lt;BR /&gt;Yes, you can use MT9M114 or OV5640 as a camera. The MT9M114 is included in the RT1064-EVK. And OV5640 is on RT1170-EVK. Unfortunately, we do not sell these camera modules separately.&lt;/P&gt;
&lt;P&gt;The camera compatible out of the box with the MIMXRT1160-EVK is the same as the one included in the MIMXRT1170-EVK. The manufacturer for this module is Suzhou Real Electronics Technology Co., LTD, with the manufacturing part number R5640AA.&lt;/P&gt;
&lt;P&gt;If you have more questions do not hesitate to ask me.&lt;BR /&gt;Best regards,&lt;BR /&gt;Omar&lt;/P&gt;</description>
    <pubDate>Thu, 10 Nov 2022 21:48:58 GMT</pubDate>
    <dc:creator>Omar_Anguiano</dc:creator>
    <dc:date>2022-11-10T21:48:58Z</dc:date>
    <item>
      <title>camera module for MIMXRT1160-EVK</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/camera-module-for-MIMXRT1160-EVK/m-p/1549840#M197296</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am currently evaluating&amp;nbsp;MIMXRT1160-EVK, which has a MIPI-CSI camera interface. The user guide said it could be used with&amp;nbsp;MT9M114, a SOC image sensor chip. Is there a particular evaluation board for&amp;nbsp;MT9M114 that I can purchase, so it plugs directly into MIMXRT1160-EVK?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you!&lt;/P&gt;&lt;P&gt;Ken&lt;/P&gt;</description>
      <pubDate>Tue, 08 Nov 2022 01:17:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/camera-module-for-MIMXRT1160-EVK/m-p/1549840#M197296</guid>
      <dc:creator>kenthesis</dc:creator>
      <dc:date>2022-11-08T01:17:33Z</dc:date>
    </item>
    <item>
      <title>Re: camera module for MIMXRT1160-EVK</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/camera-module-for-MIMXRT1160-EVK/m-p/1552248#M197444</link>
      <description>&lt;P&gt;Hello&lt;/P&gt;
&lt;P&gt;Hope you are well.&lt;BR /&gt;Yes, you can use MT9M114 or OV5640 as a camera. The MT9M114 is included in the RT1064-EVK. And OV5640 is on RT1170-EVK. Unfortunately, we do not sell these camera modules separately.&lt;/P&gt;
&lt;P&gt;The camera compatible out of the box with the MIMXRT1160-EVK is the same as the one included in the MIMXRT1170-EVK. The manufacturer for this module is Suzhou Real Electronics Technology Co., LTD, with the manufacturing part number R5640AA.&lt;/P&gt;
&lt;P&gt;If you have more questions do not hesitate to ask me.&lt;BR /&gt;Best regards,&lt;BR /&gt;Omar&lt;/P&gt;</description>
      <pubDate>Thu, 10 Nov 2022 21:48:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/camera-module-for-MIMXRT1160-EVK/m-p/1552248#M197444</guid>
      <dc:creator>Omar_Anguiano</dc:creator>
      <dc:date>2022-11-10T21:48:58Z</dc:date>
    </item>
    <item>
      <title>Re: camera module for MIMXRT1160-EVK</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/camera-module-for-MIMXRT1160-EVK/m-p/1556938#M197741</link>
      <description>&lt;P&gt;Hi Omar,&lt;/P&gt;&lt;P&gt;Thank you for sharing. Great to hear that&amp;nbsp;&lt;SPAN&gt;RT1170-EVK has a camera module. I will purchase this evk to test then.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Kenneth&lt;/P&gt;</description>
      <pubDate>Mon, 21 Nov 2022 06:34:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/camera-module-for-MIMXRT1160-EVK/m-p/1556938#M197741</guid>
      <dc:creator>kenthesis</dc:creator>
      <dc:date>2022-11-21T06:34:22Z</dc:date>
    </item>
  </channel>
</rss>