<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Android 12 EVK_8MM uboot failed to load kernel in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Android-12-EVK-8MM-uboot-failed-to-load-kernel/m-p/1552202#M197441</link>
    <description>&lt;P&gt;I fetched aosp-android-12.0.0_2.0.0 and built for &amp;nbsp;evk_8mm-userdebug.&lt;/P&gt;&lt;P&gt;There are no source code changes from me.&lt;/P&gt;&lt;P&gt;However, 8M Mini EVK Board failed to bootup.&lt;/P&gt;&lt;P&gt;There is a reboot loop after “Starting kernel ...”&lt;/P&gt;&lt;P&gt;What is it about "Moving Image from 0x40480000 to 0x40600000, end=435f0000" ?&lt;/P&gt;&lt;P&gt;Is anything else I'm missing?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;U-Boot SPL 2022.04 (Oct 24 2022 - 14:48:44 -0700)&lt;BR /&gt;Can't find PMIC:PCA9450&lt;BR /&gt;DDRINFO: start DRAM init&lt;BR /&gt;DDRINFO: DRAM rate 3000MTS&lt;BR /&gt;DDRINFO:ddrphy calibration done&lt;BR /&gt;DDRINFO: ddrmix config done&lt;BR /&gt;SEC0: RNG instantiated&lt;BR /&gt;Normal Boot&lt;BR /&gt;Trying to boot from MMC2&lt;BR /&gt;NOTICE: BL31: v2.6(release):android-12.0.0_2.0.0-0-gca6eff3c5&lt;BR /&gt;NOTICE: BL31: Built : 14:49:02, Oct 24 2022&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;U-Boot 2022.04 (Oct 24 2022 - 14:48:44 -0700)&lt;/P&gt;&lt;P&gt;CPU: i.MX8MMQ rev1.0 1800 MHz (running at 1200 MHz)&lt;BR /&gt;CPU: Commercial temperature grade (0C to 95C) at 35C&lt;BR /&gt;Reset cause: POR&lt;BR /&gt;Model: NXP i.MX8MM EVK board&lt;BR /&gt;DRAM: 2 GiB&lt;BR /&gt;TCPC: Vendor ID [0x1fc9], Product ID [0x5110], Addr [I2C1 0x52]&lt;BR /&gt;Power supply on USB2&lt;BR /&gt;TCPC: Vendor ID [0x1fc9], Product ID [0x5110], Addr [I2C1 0x50]&lt;BR /&gt;Core: 167 devices, 28 uclasses, devicetree: separate&lt;BR /&gt;MMC: FSL_SDHC: 1, FSL_SDHC: 2&lt;BR /&gt;Loading Environment from MMC... *** Warning - bad CRC, using default environment&lt;/P&gt;&lt;P&gt;[*]-Video Link 0 (1920 x 1080)&lt;BR /&gt;[0] lcdif@32e00000, video&lt;BR /&gt;[1] mipi_dsi@32e10000, video_bridge&lt;BR /&gt;[2] adv7535@3d, panel&lt;BR /&gt;In: serial&lt;BR /&gt;Out: serial&lt;BR /&gt;Err: serial&lt;/P&gt;&lt;P&gt;BuildInfo:&lt;BR /&gt;- ATF ca6eff3&lt;/P&gt;&lt;P&gt;flash target is MMC:2&lt;BR /&gt;Net: eth0: ethernet@30be0000&lt;BR /&gt;Fastboot: Normal&lt;BR /&gt;Normal Boot&lt;BR /&gt;Hit any key to stop autoboot: 0&lt;BR /&gt;In boota get fastboot lock status error. Set lock status&lt;BR /&gt;Magic is incorrect.&lt;BR /&gt;Error validating A/B metadata from disk. Resetting and writing new A/B metadata to disk.&lt;BR /&gt;Writing A/B metadata to disk.&lt;BR /&gt;verify OK, boot 'boot_a'&lt;BR /&gt;Kernel load addr 0x40480000 size 48455 KiB&lt;BR /&gt;kernel @ 40480000 (50266112)&lt;BR /&gt;ramdisk @ 44680000 (14864469)&lt;BR /&gt;fdt @ 435f0400 (50398)&lt;BR /&gt;Moving Image from 0x40480000 to 0x40600000, end=435f0000&lt;BR /&gt;## Flattened Device Tree blob at 435f0400&lt;BR /&gt;Booting using the fdt blob at 0x435f0400&lt;BR /&gt;Using Device Tree in place at 00000000435f0400, end 00000000435ff8dd&lt;/P&gt;&lt;P&gt;Starting kernel ...&lt;/P&gt;</description>
    <pubDate>Thu, 10 Nov 2022 19:26:10 GMT</pubDate>
    <dc:creator>dmitry_abdulov</dc:creator>
    <dc:date>2022-11-10T19:26:10Z</dc:date>
    <item>
      <title>Android 12 EVK_8MM uboot failed to load kernel</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Android-12-EVK-8MM-uboot-failed-to-load-kernel/m-p/1552202#M197441</link>
      <description>&lt;P&gt;I fetched aosp-android-12.0.0_2.0.0 and built for &amp;nbsp;evk_8mm-userdebug.&lt;/P&gt;&lt;P&gt;There are no source code changes from me.&lt;/P&gt;&lt;P&gt;However, 8M Mini EVK Board failed to bootup.&lt;/P&gt;&lt;P&gt;There is a reboot loop after “Starting kernel ...”&lt;/P&gt;&lt;P&gt;What is it about "Moving Image from 0x40480000 to 0x40600000, end=435f0000" ?&lt;/P&gt;&lt;P&gt;Is anything else I'm missing?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;U-Boot SPL 2022.04 (Oct 24 2022 - 14:48:44 -0700)&lt;BR /&gt;Can't find PMIC:PCA9450&lt;BR /&gt;DDRINFO: start DRAM init&lt;BR /&gt;DDRINFO: DRAM rate 3000MTS&lt;BR /&gt;DDRINFO:ddrphy calibration done&lt;BR /&gt;DDRINFO: ddrmix config done&lt;BR /&gt;SEC0: RNG instantiated&lt;BR /&gt;Normal Boot&lt;BR /&gt;Trying to boot from MMC2&lt;BR /&gt;NOTICE: BL31: v2.6(release):android-12.0.0_2.0.0-0-gca6eff3c5&lt;BR /&gt;NOTICE: BL31: Built : 14:49:02, Oct 24 2022&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;U-Boot 2022.04 (Oct 24 2022 - 14:48:44 -0700)&lt;/P&gt;&lt;P&gt;CPU: i.MX8MMQ rev1.0 1800 MHz (running at 1200 MHz)&lt;BR /&gt;CPU: Commercial temperature grade (0C to 95C) at 35C&lt;BR /&gt;Reset cause: POR&lt;BR /&gt;Model: NXP i.MX8MM EVK board&lt;BR /&gt;DRAM: 2 GiB&lt;BR /&gt;TCPC: Vendor ID [0x1fc9], Product ID [0x5110], Addr [I2C1 0x52]&lt;BR /&gt;Power supply on USB2&lt;BR /&gt;TCPC: Vendor ID [0x1fc9], Product ID [0x5110], Addr [I2C1 0x50]&lt;BR /&gt;Core: 167 devices, 28 uclasses, devicetree: separate&lt;BR /&gt;MMC: FSL_SDHC: 1, FSL_SDHC: 2&lt;BR /&gt;Loading Environment from MMC... *** Warning - bad CRC, using default environment&lt;/P&gt;&lt;P&gt;[*]-Video Link 0 (1920 x 1080)&lt;BR /&gt;[0] lcdif@32e00000, video&lt;BR /&gt;[1] mipi_dsi@32e10000, video_bridge&lt;BR /&gt;[2] adv7535@3d, panel&lt;BR /&gt;In: serial&lt;BR /&gt;Out: serial&lt;BR /&gt;Err: serial&lt;/P&gt;&lt;P&gt;BuildInfo:&lt;BR /&gt;- ATF ca6eff3&lt;/P&gt;&lt;P&gt;flash target is MMC:2&lt;BR /&gt;Net: eth0: ethernet@30be0000&lt;BR /&gt;Fastboot: Normal&lt;BR /&gt;Normal Boot&lt;BR /&gt;Hit any key to stop autoboot: 0&lt;BR /&gt;In boota get fastboot lock status error. Set lock status&lt;BR /&gt;Magic is incorrect.&lt;BR /&gt;Error validating A/B metadata from disk. Resetting and writing new A/B metadata to disk.&lt;BR /&gt;Writing A/B metadata to disk.&lt;BR /&gt;verify OK, boot 'boot_a'&lt;BR /&gt;Kernel load addr 0x40480000 size 48455 KiB&lt;BR /&gt;kernel @ 40480000 (50266112)&lt;BR /&gt;ramdisk @ 44680000 (14864469)&lt;BR /&gt;fdt @ 435f0400 (50398)&lt;BR /&gt;Moving Image from 0x40480000 to 0x40600000, end=435f0000&lt;BR /&gt;## Flattened Device Tree blob at 435f0400&lt;BR /&gt;Booting using the fdt blob at 0x435f0400&lt;BR /&gt;Using Device Tree in place at 00000000435f0400, end 00000000435ff8dd&lt;/P&gt;&lt;P&gt;Starting kernel ...&lt;/P&gt;</description>
      <pubDate>Thu, 10 Nov 2022 19:26:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Android-12-EVK-8MM-uboot-failed-to-load-kernel/m-p/1552202#M197441</guid>
      <dc:creator>dmitry_abdulov</dc:creator>
      <dc:date>2022-11-10T19:26:10Z</dc:date>
    </item>
    <item>
      <title>Re: Android 12 EVK_8MM uboot failed to load kernel</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Android-12-EVK-8MM-uboot-failed-to-load-kernel/m-p/1553598#M197543</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/182079"&gt;@dmitry_abdulov&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Have you tried the demo image on EVK?&lt;/P&gt;
&lt;P&gt;Regads&lt;/P&gt;
&lt;P&gt;Qmiller&lt;/P&gt;</description>
      <pubDate>Tue, 15 Nov 2022 02:34:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Android-12-EVK-8MM-uboot-failed-to-load-kernel/m-p/1553598#M197543</guid>
      <dc:creator>Zhiming_Liu</dc:creator>
      <dc:date>2022-11-15T02:34:43Z</dc:date>
    </item>
    <item>
      <title>Re: Android 12 EVK_8MM uboot failed to load kernel</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Android-12-EVK-8MM-uboot-failed-to-load-kernel/m-p/1554346#M197594</link>
      <description>&lt;P&gt;Hi &lt;A href="https://community.nxp.com/t5/user/viewprofilepage/user-id/151788" target="_blank"&gt;&lt;STRONG&gt;Qmiller&lt;/STRONG&gt;&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Yes, I tried demo image and it works just fine.&lt;/P&gt;&lt;P&gt;I found, that I applied one change in the source code.&lt;/P&gt;&lt;P&gt;I disabled “IMX8MM_USES_GKI”.&lt;/P&gt;&lt;P&gt;Apparently, I can run the build when “IMX8MM_USES_GKI” is enabled, but if I disable it I meet the problem I mentioned above.&lt;/P&gt;&lt;P&gt;Is anything else I need to do to run the image without GKI?&lt;/P&gt;</description>
      <pubDate>Wed, 16 Nov 2022 01:29:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Android-12-EVK-8MM-uboot-failed-to-load-kernel/m-p/1554346#M197594</guid>
      <dc:creator>dmitry_abdulov</dc:creator>
      <dc:date>2022-11-16T01:29:33Z</dc:date>
    </item>
    <item>
      <title>Re: Android 12 EVK_8MM uboot failed to load kernel</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Android-12-EVK-8MM-uboot-failed-to-load-kernel/m-p/1555498#M197647</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/182079"&gt;@dmitry_abdulov&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Please try to open all&amp;nbsp;CONFIG_XXXX in&amp;nbsp;SharedBoardConfig.mk&lt;/P&gt;</description>
      <pubDate>Thu, 17 Nov 2022 05:13:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Android-12-EVK-8MM-uboot-failed-to-load-kernel/m-p/1555498#M197647</guid>
      <dc:creator>Zhiming_Liu</dc:creator>
      <dc:date>2022-11-17T05:13:19Z</dc:date>
    </item>
    <item>
      <title>Re: Android 12 EVK_8MM uboot failed to load kernel</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Android-12-EVK-8MM-uboot-failed-to-load-kernel/m-p/1555850#M197683</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;A href="https://community.nxp.com/t5/user/viewprofilepage/user-id/151788" target="_self"&gt;&lt;SPAN class=""&gt;Qmiller&lt;/SPAN&gt;&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;There are plenty "# CONFIG_XXX" commented out in "SharedBoardConfig.mk".&lt;/P&gt;&lt;P&gt;Do you mean they have to be defined as "y" in kernel config in that case?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 17 Nov 2022 14:11:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Android-12-EVK-8MM-uboot-failed-to-load-kernel/m-p/1555850#M197683</guid>
      <dc:creator>dmitry_abdulov</dc:creator>
      <dc:date>2022-11-17T14:11:39Z</dc:date>
    </item>
    <item>
      <title>Re: Android 12 EVK_8MM uboot failed to load kernel</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Android-12-EVK-8MM-uboot-failed-to-load-kernel/m-p/1556825#M197731</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;A href="https://community.nxp.com/t5/user/viewprofilepage/user-id/151788" target="_self"&gt;&lt;SPAN class=""&gt;Qmiller&lt;/SPAN&gt;&lt;/A&gt;,&amp;nbsp;&lt;/P&gt;&lt;P&gt;I opened all of them and it didn't help, I still had the same issue.&lt;/P&gt;&lt;P&gt;Is anything else I can do?&lt;/P&gt;</description>
      <pubDate>Mon, 21 Nov 2022 03:04:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Android-12-EVK-8MM-uboot-failed-to-load-kernel/m-p/1556825#M197731</guid>
      <dc:creator>dmitry_abdulov</dc:creator>
      <dc:date>2022-11-21T03:04:37Z</dc:date>
    </item>
    <item>
      <title>Re: Android 12 EVK_8MM uboot failed to load kernel</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Android-12-EVK-8MM-uboot-failed-to-load-kernel/m-p/1556828#M197732</link>
      <description>&lt;P&gt;I am compiling this BSP, will reply you when i solve this .&lt;/P&gt;</description>
      <pubDate>Mon, 21 Nov 2022 03:06:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Android-12-EVK-8MM-uboot-failed-to-load-kernel/m-p/1556828#M197732</guid>
      <dc:creator>Zhiming_Liu</dc:creator>
      <dc:date>2022-11-21T03:06:52Z</dc:date>
    </item>
    <item>
      <title>Re: Android 12 EVK_8MM uboot failed to load kernel</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Android-12-EVK-8MM-uboot-failed-to-load-kernel/m-p/1558181#M197870</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/182079"&gt;@dmitry_abdulov&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;The compile system of Android 11/12 will generate boot.img and boot-imx.img,&amp;nbsp;boot.img includes gki kernel,&amp;nbsp;boot-imx.img doesn't includes gki.&lt;/P&gt;
&lt;P&gt;So you can change uuu_imx_android_flash.bat like below.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Qmiller_0-1669266619033.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/201551i3E5BB6A26998EC34/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Qmiller_0-1669266619033.png" alt="Qmiller_0-1669266619033.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Qmiller_0-1669266619033.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;The version of kernel_imx in Android is same as GKI kernel version, so you will see same version after using boot-imx.img&lt;/P&gt;</description>
      <pubDate>Thu, 24 Nov 2022 05:13:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Android-12-EVK-8MM-uboot-failed-to-load-kernel/m-p/1558181#M197870</guid>
      <dc:creator>Zhiming_Liu</dc:creator>
      <dc:date>2022-11-24T05:13:11Z</dc:date>
    </item>
    <item>
      <title>Re: Android 12 EVK_8MM uboot failed to load kernel</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Android-12-EVK-8MM-uboot-failed-to-load-kernel/m-p/1558796#M197925</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;A href="https://community.nxp.com/t5/user/viewprofilepage/user-id/151788" target="_blank" rel="noopener"&gt;&lt;STRONG&gt;Qmiller&lt;/STRONG&gt;&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;Thank you very much!!&lt;/P&gt;</description>
      <pubDate>Wed, 23 Nov 2022 18:23:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Android-12-EVK-8MM-uboot-failed-to-load-kernel/m-p/1558796#M197925</guid>
      <dc:creator>dmitry_abdulov</dc:creator>
      <dc:date>2022-11-23T18:23:14Z</dc:date>
    </item>
    <item>
      <title>Re: Android 12 EVK_8MM uboot failed to load kernel</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Android-12-EVK-8MM-uboot-failed-to-load-kernel/m-p/1559107#M197934</link>
      <description>&lt;P&gt;Update previous reply.&lt;/P&gt;</description>
      <pubDate>Thu, 24 Nov 2022 05:11:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Android-12-EVK-8MM-uboot-failed-to-load-kernel/m-p/1559107#M197934</guid>
      <dc:creator>Zhiming_Liu</dc:creator>
      <dc:date>2022-11-24T05:11:36Z</dc:date>
    </item>
  </channel>
</rss>