<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic i.MX8QXP maximum RAM size in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8QXP-maximum-RAM-size/m-p/1551063#M197361</link>
    <description>&lt;P&gt;What is the maximum RAM size which can be used with the i.MX8QXP? MEK uses 3GB. Is 4GB possible?&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 09 Nov 2022 12:55:28 GMT</pubDate>
    <dc:creator>mod42</dc:creator>
    <dc:date>2022-11-09T12:55:28Z</dc:date>
    <item>
      <title>i.MX8QXP maximum RAM size</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8QXP-maximum-RAM-size/m-p/1551063#M197361</link>
      <description>&lt;P&gt;What is the maximum RAM size which can be used with the i.MX8QXP? MEK uses 3GB. Is 4GB possible?&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 09 Nov 2022 12:55:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8QXP-maximum-RAM-size/m-p/1551063#M197361</guid>
      <dc:creator>mod42</dc:creator>
      <dc:date>2022-11-09T12:55:28Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX8QXP maximum RAM size</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8QXP-maximum-RAM-size/m-p/1551990#M197427</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/52006"&gt;@mod42&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;i.MX8QXP does support up to 4GB density.&lt;/P&gt;
&lt;P&gt;Thanks &amp;amp; Regards,&lt;BR /&gt;Ritesh M Patel&lt;/P&gt;</description>
      <pubDate>Thu, 10 Nov 2022 13:26:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8QXP-maximum-RAM-size/m-p/1551990#M197427</guid>
      <dc:creator>riteshmpatel</dc:creator>
      <dc:date>2022-11-10T13:26:15Z</dc:date>
    </item>
  </channel>
</rss>