<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic PWM module with settings using Config Tools in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/PWM-module-with-settings-using-Config-Tools/m-p/1549459#M197263</link>
    <description>&lt;P&gt;Hi All,&lt;/P&gt;&lt;P&gt;I want to use PWM module with settings using Config Tools(Peripherals). I have the pin set as output for PWM and the eFlexPWM module. I still don't see a signal on the output pin(G13, GPIO_AD_B0_10). Can anyone tell me where I am going wrong in the ConfigTools settings?&lt;/P&gt;&lt;P&gt;I am attaching a simple project for EVK. Used MCUXpresso 11.5.0.7232 and SDK_2.x_MIMXRT1060-EVKB(v2.110).&lt;/P&gt;&lt;P&gt;Thank you for answer.&lt;/P&gt;&lt;P&gt;Jaroslav C.&lt;/P&gt;</description>
    <pubDate>Mon, 07 Nov 2022 07:56:52 GMT</pubDate>
    <dc:creator>cerma</dc:creator>
    <dc:date>2022-11-07T07:56:52Z</dc:date>
    <item>
      <title>PWM module with settings using Config Tools</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/PWM-module-with-settings-using-Config-Tools/m-p/1549459#M197263</link>
      <description>&lt;P&gt;Hi All,&lt;/P&gt;&lt;P&gt;I want to use PWM module with settings using Config Tools(Peripherals). I have the pin set as output for PWM and the eFlexPWM module. I still don't see a signal on the output pin(G13, GPIO_AD_B0_10). Can anyone tell me where I am going wrong in the ConfigTools settings?&lt;/P&gt;&lt;P&gt;I am attaching a simple project for EVK. Used MCUXpresso 11.5.0.7232 and SDK_2.x_MIMXRT1060-EVKB(v2.110).&lt;/P&gt;&lt;P&gt;Thank you for answer.&lt;/P&gt;&lt;P&gt;Jaroslav C.&lt;/P&gt;</description>
      <pubDate>Mon, 07 Nov 2022 07:56:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/PWM-module-with-settings-using-Config-Tools/m-p/1549459#M197263</guid>
      <dc:creator>cerma</dc:creator>
      <dc:date>2022-11-07T07:56:52Z</dc:date>
    </item>
    <item>
      <title>Re: PWM module with settings using Config Tools</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/PWM-module-with-settings-using-Config-Tools/m-p/1550967#M197354</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/8010"&gt;@cerma&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;The pin setting seems correct. You can see there is a newline appear in pin_mux.c&lt;/P&gt;
&lt;P&gt;IOMUXC_SetPinMux(IOMUXC_GPIO_AD_B0_10_FLEXPWM1_PWMA03, 0U); &lt;/P&gt;
&lt;P&gt;You can compare the generated code with the pwm example in SDK to search what is not set correctly.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Jing&lt;/P&gt;</description>
      <pubDate>Wed, 09 Nov 2022 09:59:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/PWM-module-with-settings-using-Config-Tools/m-p/1550967#M197354</guid>
      <dc:creator>jingpan</dc:creator>
      <dc:date>2022-11-09T09:59:25Z</dc:date>
    </item>
  </channel>
</rss>