<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: lwip pppos error while communication in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/lwip-pppos-error-while-communication/m-p/1548593#M197194</link>
    <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/191058"&gt;@Sanjay1993&lt;/a&gt;&amp;nbsp;，&lt;BR /&gt;Thanks for your reply.&lt;BR /&gt;I think I need more information, I was wondering if you can introduce the testing environment, such as the board, demo code, etc.&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;
&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Fri, 04 Nov 2022 02:16:18 GMT</pubDate>
    <dc:creator>jeremyzhou</dc:creator>
    <dc:date>2022-11-04T02:16:18Z</dc:date>
    <item>
      <title>lwip pppos error while communication</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/lwip-pppos-error-while-communication/m-p/1539980#M196537</link>
      <description>&lt;P&gt;Hi,&lt;BR /&gt;I am working on a Quectel EG21 GSM module. This is the following output showing.&lt;BR /&gt;GSM initialization start…&lt;BR /&gt;AT COMMAND: [AT…]&lt;BR /&gt;AT RESPONSE: […OK…]&lt;BR /&gt;AT COMMAND: [ATZ…]&lt;BR /&gt;AT RESPONSE: […OK…]&lt;BR /&gt;AT COMMAND: [ATE0…]&lt;BR /&gt;AT RESPONSE: […OK…]&lt;BR /&gt;AT COMMAND: [AT+CFUN=1.]&lt;BR /&gt;AT RESPONSE: […OK…]&lt;BR /&gt;AT COMMAND: [AT+CNMI=0,0,0,0,0…]&lt;BR /&gt;AT RESPONSE: […OK…]&lt;BR /&gt;AT COMMAND: [AT+CPIN?..]&lt;BR /&gt;AT RESPONSE: […+CPIN: READY…OK…]&lt;BR /&gt;AT COMMAND: [AT+CREG?..]&lt;BR /&gt;AT RESPONSE: […+CREG: 0,1…OK…]&lt;BR /&gt;AT COMMAND: [AT+CGDCONT=1,“IP”,“internet”…]&lt;BR /&gt;AT RESPONSE: […OK…]&lt;BR /&gt;AT COMMAND: [AT+CGDATA=“PPP”,1…]&lt;BR /&gt;AT RESPONSE: […CONNECT 150000000…]&lt;BR /&gt;GSM initialized…&lt;BR /&gt;Error code : 6&lt;BR /&gt;status_cb: Connection lost&lt;BR /&gt;Disconnected, trying again…&lt;BR /&gt;Error code : 5&lt;BR /&gt;status_cb: User interrupt (disconnected)&lt;/P&gt;&lt;P&gt;Showing PPP connection is lost.&lt;BR /&gt;Expect receiving ip address back as follows.&lt;/P&gt;&lt;P&gt;I (19277) [PPPOS CLIENT]: AT COMMAND: [AT+CGDATA=“PPP”,1…]&lt;BR /&gt;I (19297) [PPPOS CLIENT]: AT RESPONSE: […CONNECT…]&lt;BR /&gt;I (20297) [PPPOS CLIENT]: GSM initialized.&lt;BR /&gt;I (21077) [PPPOS CLIENT]: status_cb: Connected&lt;BR /&gt;I (21077) [PPPOS CLIENT]: ipaddr = 10.229.68.97&lt;BR /&gt;I (21077) [PPPOS CLIENT]: gateway = 10.64.64.64&lt;BR /&gt;I (21077) [PPPOS CLIENT]: netmask = 255.255.255.255&lt;BR /&gt;I (21087) [PPPOS CLIENT]: ip6addr = ::&lt;/P&gt;&lt;P&gt;Is there any way that i can troubleshoot this error.&lt;BR /&gt;Thanks and Regards&lt;BR /&gt;Sanjay&lt;/P&gt;</description>
      <pubDate>Wed, 19 Oct 2022 09:25:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/lwip-pppos-error-while-communication/m-p/1539980#M196537</guid>
      <dc:creator>Sanjay1993</dc:creator>
      <dc:date>2022-10-19T09:25:08Z</dc:date>
    </item>
    <item>
      <title>Re: lwip pppos error while communication</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/lwip-pppos-error-while-communication/m-p/1547203#M197076</link>
      <description>&lt;P&gt;Hello&lt;BR /&gt;Hope you are well.&lt;/P&gt;
&lt;P&gt;Could you tell me the NXP part number you are working with?&lt;BR /&gt;&lt;BR /&gt;Best regards,&lt;BR /&gt;Omar&lt;/P&gt;</description>
      <pubDate>Tue, 01 Nov 2022 21:24:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/lwip-pppos-error-while-communication/m-p/1547203#M197076</guid>
      <dc:creator>Omar_Anguiano</dc:creator>
      <dc:date>2022-11-01T21:24:23Z</dc:date>
    </item>
    <item>
      <title>Re: lwip pppos error while communication</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/lwip-pppos-error-while-communication/m-p/1548593#M197194</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/191058"&gt;@Sanjay1993&lt;/a&gt;&amp;nbsp;，&lt;BR /&gt;Thanks for your reply.&lt;BR /&gt;I think I need more information, I was wondering if you can introduce the testing environment, such as the board, demo code, etc.&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;
&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 04 Nov 2022 02:16:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/lwip-pppos-error-while-communication/m-p/1548593#M197194</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2022-11-04T02:16:18Z</dc:date>
    </item>
  </channel>
</rss>